<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>ColdFire/68K Microcontrollers and ProcessorsのトピックRe: Motorola MC68332GCFC16 ID 0J30C replacement problem</title>
    <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/Motorola-MC68332GCFC16-ID-0J30C-replacement-problem/m-p/2090742#M14698</link>
    <description>&lt;P&gt;SOLVED&lt;/P&gt;&lt;P&gt;I found the problem The G mask does not have DIO, I need the A mask&lt;/P&gt;</description>
    <pubDate>Thu, 01 May 2025 20:57:12 GMT</pubDate>
    <dc:creator>Micronetwork</dc:creator>
    <dc:date>2025-05-01T20:57:12Z</dc:date>
    <item>
      <title>Motorola MC68332GCFC16 ID 0J30C replacement problem</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/Motorola-MC68332GCFC16-ID-0J30C-replacement-problem/m-p/2090653#M14697</link>
      <description>&lt;P&gt;Hi,&lt;BR /&gt;I have a controller board with an old Motorola MC68332GCFC16 ID 0J30C&lt;BR /&gt;The MCU have damaged IO on one channel.&lt;/P&gt;&lt;P&gt;The board itself is not damaged.&lt;BR /&gt;The original Motorola MC68332GCFC16 ID 0J30C had damaged TPUCH11 (giving output 1.9V, not 5V)&lt;/P&gt;&lt;P&gt;I replace MCU with Freescale MC68332GCFC16 ID 1J66A&lt;BR /&gt;Now , all TPU Channels are NOT working. (no voltage on any channels)&lt;/P&gt;&lt;P&gt;I replace back the Motorola MC68332GCFC16 ID 0J30C&lt;BR /&gt;Now all TPU Channels are working except TPU Channel 11 (giving output 1.9V, not 5V)&lt;/P&gt;&lt;P&gt;I found another Motorola MC68332GCFC16 ID 0J30C and this works&lt;BR /&gt;I also tried 4 other Freescale MC68332GCFC16 ID 1J66A and they all failed.&lt;/P&gt;&lt;P&gt;So problem is incompatible Freescale MCU with original firmware.&lt;/P&gt;&lt;P&gt;After decompiling firmware, I see that firmware expect TPU microcode to be already present&lt;BR /&gt;it does not load microcode, it assumes the Motorola version (with built-in TPU ROM)&lt;/P&gt;&lt;P&gt;So I think I need to integrate the DIO microcode into firmware by loading it into the TPURAM at addresses $YF000–$YF3FF&lt;/P&gt;&lt;P&gt;If this is the case, I'm looking for the TPU microcode block.&lt;/P&gt;&lt;P&gt;Any insight and suggestions would be highly appreciated. Thanks in advance.&lt;/P&gt;&lt;P&gt;Best,&lt;BR /&gt;Tom&lt;/P&gt;</description>
      <pubDate>Thu, 01 May 2025 14:05:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/Motorola-MC68332GCFC16-ID-0J30C-replacement-problem/m-p/2090653#M14697</guid>
      <dc:creator>Micronetwork</dc:creator>
      <dc:date>2025-05-01T14:05:10Z</dc:date>
    </item>
    <item>
      <title>Re: Motorola MC68332GCFC16 ID 0J30C replacement problem</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/Motorola-MC68332GCFC16-ID-0J30C-replacement-problem/m-p/2090742#M14698</link>
      <description>&lt;P&gt;SOLVED&lt;/P&gt;&lt;P&gt;I found the problem The G mask does not have DIO, I need the A mask&lt;/P&gt;</description>
      <pubDate>Thu, 01 May 2025 20:57:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/Motorola-MC68332GCFC16-ID-0J30C-replacement-problem/m-p/2090742#M14698</guid>
      <dc:creator>Micronetwork</dc:creator>
      <dc:date>2025-05-01T20:57:12Z</dc:date>
    </item>
  </channel>
</rss>