<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: TCP/IP stack for MCF5222x family in ColdFire/68K Microcontrollers and Processors</title>
    <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/TCP-IP-stack-for-MCF5222x-family/m-p/134487#M1463</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;Hi lntsenthil&lt;BR /&gt;&lt;BR /&gt;The MCF5222x has USB on-the-go but no Ethernet interface. Therefore it is not normally used together with a TCP/IP stack.&lt;BR /&gt;&lt;BR /&gt;The MCF5223X family with integrated EMAC and EPHY allow single chip embedded IP applications.&lt;BR /&gt;&lt;BR /&gt;Look at the uTasker operating system with integrated TCP/IP stack (www.uTasker.com) which is free (including support) for non-commercial use. There is a demo online at &lt;A href="http://212.254.22.36" target="test_blank"&gt;http://212.254.22.36&lt;/A&gt; requiring about 50k code, 12k SRAM and 32K File system as reference.&lt;BR /&gt;&lt;BR /&gt;Regards&lt;BR /&gt;&lt;BR /&gt;Mark Butcher&lt;BR /&gt;&lt;BR /&gt;&lt;A href="https://community.nxp.com/www.mjbc.ch" target="test_blank"&gt;www.mjbc.ch&lt;/A&gt; / &lt;A href="https://community.nxp.com/www.uTasker.com" target="test_blank"&gt;www.uTasker.com&lt;/A&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Sat, 28 Oct 2006 06:04:58 GMT</pubDate>
    <dc:creator>mjbcswitzerland</dc:creator>
    <dc:date>2006-10-28T06:04:58Z</dc:date>
    <item>
      <title>TCP/IP stack for MCF5222x family</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/TCP-IP-stack-for-MCF5222x-family/m-p/134486#M1462</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;SPAN&gt;Hi all,&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Is there any TCP/IP stack available for MCF5222x family ?&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Can TCP/IP Lite stack by InterNiche be used for MCF5222x family also?&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;If so what is the memory size it occupies?&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Looking for your answers.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;lntsenthil&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 27 Oct 2006 12:07:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/TCP-IP-stack-for-MCF5222x-family/m-p/134486#M1462</guid>
      <dc:creator>senthil</dc:creator>
      <dc:date>2006-10-27T12:07:34Z</dc:date>
    </item>
    <item>
      <title>Re: TCP/IP stack for MCF5222x family</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/TCP-IP-stack-for-MCF5222x-family/m-p/134487#M1463</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;Hi lntsenthil&lt;BR /&gt;&lt;BR /&gt;The MCF5222x has USB on-the-go but no Ethernet interface. Therefore it is not normally used together with a TCP/IP stack.&lt;BR /&gt;&lt;BR /&gt;The MCF5223X family with integrated EMAC and EPHY allow single chip embedded IP applications.&lt;BR /&gt;&lt;BR /&gt;Look at the uTasker operating system with integrated TCP/IP stack (www.uTasker.com) which is free (including support) for non-commercial use. There is a demo online at &lt;A href="http://212.254.22.36" target="test_blank"&gt;http://212.254.22.36&lt;/A&gt; requiring about 50k code, 12k SRAM and 32K File system as reference.&lt;BR /&gt;&lt;BR /&gt;Regards&lt;BR /&gt;&lt;BR /&gt;Mark Butcher&lt;BR /&gt;&lt;BR /&gt;&lt;A href="https://community.nxp.com/www.mjbc.ch" target="test_blank"&gt;www.mjbc.ch&lt;/A&gt; / &lt;A href="https://community.nxp.com/www.uTasker.com" target="test_blank"&gt;www.uTasker.com&lt;/A&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 28 Oct 2006 06:04:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/TCP-IP-stack-for-MCF5222x-family/m-p/134487#M1463</guid>
      <dc:creator>mjbcswitzerland</dc:creator>
      <dc:date>2006-10-28T06:04:58Z</dc:date>
    </item>
  </channel>
</rss>