<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>ColdFire/68K Microcontrollers and Processors中的主题 Commandline compiler for Coldfire?</title>
    <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/Commandline-compiler-for-Coldfire/m-p/1794477#M14491</link>
    <description>&lt;P&gt;All of our source code projects except the Coldfire projects, are built via piplines in gitlab through gitlab-runners.&lt;/P&gt;&lt;P&gt;Today we have to build the coldfire projects through the IDE (CodeWarrior for MCU 10.6) and that requires human interaction which is not good.&lt;/P&gt;&lt;P&gt;Is it possible to build the coldfire projects (MCF52233/MFC52236) through a commandline compiler so we can add the coldfire project to the gitlab piplines as well?&lt;/P&gt;</description>
    <pubDate>Wed, 24 Jan 2024 08:27:34 GMT</pubDate>
    <dc:creator>Numinel</dc:creator>
    <dc:date>2024-01-24T08:27:34Z</dc:date>
    <item>
      <title>Commandline compiler for Coldfire?</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/Commandline-compiler-for-Coldfire/m-p/1794477#M14491</link>
      <description>&lt;P&gt;All of our source code projects except the Coldfire projects, are built via piplines in gitlab through gitlab-runners.&lt;/P&gt;&lt;P&gt;Today we have to build the coldfire projects through the IDE (CodeWarrior for MCU 10.6) and that requires human interaction which is not good.&lt;/P&gt;&lt;P&gt;Is it possible to build the coldfire projects (MCF52233/MFC52236) through a commandline compiler so we can add the coldfire project to the gitlab piplines as well?&lt;/P&gt;</description>
      <pubDate>Wed, 24 Jan 2024 08:27:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/Commandline-compiler-for-Coldfire/m-p/1794477#M14491</guid>
      <dc:creator>Numinel</dc:creator>
      <dc:date>2024-01-24T08:27:34Z</dc:date>
    </item>
    <item>
      <title>Re: Commandline compiler for Coldfire?</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/Commandline-compiler-for-Coldfire/m-p/1794710#M14492</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;
&lt;P&gt;Please follow up this link.&lt;/P&gt;
&lt;P&gt;&lt;A href="https://community.nxp.com/t5/CodeWarrior-Development-Tools/CodeWarrior-10-Command-Line-Interface-usage-and-examples/ta-p/1124253" target="_blank"&gt;https://community.nxp.com/t5/CodeWarrior-Development-Tools/CodeWarrior-10-Command-Line-Interface-usage-and-examples/ta-p/1124253&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Regards&lt;/P&gt;</description>
      <pubDate>Wed, 24 Jan 2024 14:46:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/Commandline-compiler-for-Coldfire/m-p/1794710#M14492</guid>
      <dc:creator>Bio_TICFSL</dc:creator>
      <dc:date>2024-01-24T14:46:16Z</dc:date>
    </item>
  </channel>
</rss>