<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>ColdFire/68K Microcontrollers and Processors中的主题 Re: Introduction: MCF52259</title>
    <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/Introduction-MCF52259/m-p/1622676#M14355</link>
    <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;Do you have any technical question about MCF52259 product? Or.&lt;/P&gt;
&lt;P&gt;Mike&lt;/P&gt;</description>
    <pubDate>Mon, 27 Mar 2023 14:28:17 GMT</pubDate>
    <dc:creator>Hui_Ma</dc:creator>
    <dc:date>2023-03-27T14:28:17Z</dc:date>
    <item>
      <title>Introduction: MCF52259</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/Introduction-MCF52259/m-p/1622298#M14354</link>
      <description>&lt;P&gt;The MCF52259 is a member of the ColdFire® family of Reduced Instruction Set Computing (RISC) microprocessors.&lt;BR /&gt;This document provides an overview of the 32-bit MCF52259 microcontroller, focusing on its high integration and diverse feature set.&lt;BR /&gt;This 32-bit device is based on a version 2 ColdFire core operating at up to 80 MHz for performance and low power consumption.&lt;BR /&gt;On-chip memory is tightly coupled to the processor core, including 512 KB of flash memory and 64 KB of static random-access memory (SRAM).&lt;BR /&gt;On-chip modules include: • V2 ColdFire core delivering 76 MIPS (Dhrystone 2.1) 80 MHz, running from internal flash with enhanced multiply-accumulate (MAC) unit and hardware divider, divider&lt;BR /&gt;• Crypto Acceleration Unit (CAU)&lt;BR /&gt;• Fast Ethernet Controller (FEC)&lt;BR /&gt;• Micro FlexBus external bus interface available in 144-pin package&lt;BR /&gt;• Universal Serial Bus on the Go (USBOTG)&lt;BR /&gt;• USB transceiver&lt;BR /&gt;• FlexCAN Controller Area Network (CAN) module&lt;BR /&gt;• Three universal asynchronous/synchronous receivers/transmitters&lt;BR /&gt;• Two Inter-Integrated Circuit (I2C™) bus interface modules&lt;BR /&gt;• Queued Serial Peripheral Interface (QSPI) module&lt;BR /&gt;• Eight-channel 12-bit fast analog-to-digital converter (ADC), simultaneous sampling&lt;BR /&gt;• Quad Channel Direct Memory Access (DMA) Controller&lt;BR /&gt;• Four 32-bit input capture/output compare timers with DMA support (DTIM)&lt;BR /&gt;• Four-channel general purpose timer (GPT) capable of input capture/output compare, pulse width modulation (PWM) and pulse accumulation&lt;BR /&gt;• Octal/Quad Channel, 8-bit/16-bit PWM Timer Two 16-bit Periodic Interrupt Timers (PIT)&lt;BR /&gt;• Real Time Clock (RTC) module with 32 kHz crystal&lt;BR /&gt;• Programmable software watchdog timer&lt;BR /&gt;• Auxiliary watchdog timer with independent clock&lt;BR /&gt;• Interrupt controller capable of handling 57 sources&lt;BR /&gt;• Clock module with 8 MHz on-chip relaxation oscillator and integrated phase-locked loop (PLL)&lt;BR /&gt;• Test access/debug ports (JTAG, BDM)&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="JaydenCai_0-1679899841300.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/216316i5AA738A79992E381/image-size/medium?v=v2&amp;amp;px=400" role="button" title="JaydenCai_0-1679899841300.png" alt="JaydenCai_0-1679899841300.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;Editor:&lt;A title="Perceptive-IC" href="https://www.perceptive-ic.com/" target="_blank" rel="noopener"&gt;Perceptive-IC&lt;/A&gt;&lt;/P&gt;</description>
      <pubDate>Mon, 27 Mar 2023 06:54:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/Introduction-MCF52259/m-p/1622298#M14354</guid>
      <dc:creator>CarrieDuoduo</dc:creator>
      <dc:date>2023-03-27T06:54:38Z</dc:date>
    </item>
    <item>
      <title>Re: Introduction: MCF52259</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/Introduction-MCF52259/m-p/1622676#M14355</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;Do you have any technical question about MCF52259 product? Or.&lt;/P&gt;
&lt;P&gt;Mike&lt;/P&gt;</description>
      <pubDate>Mon, 27 Mar 2023 14:28:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/Introduction-MCF52259/m-p/1622676#M14355</guid>
      <dc:creator>Hui_Ma</dc:creator>
      <dc:date>2023-03-27T14:28:17Z</dc:date>
    </item>
  </channel>
</rss>