<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>ColdFire/68K Microcontrollers and Processors中的主题 Re: Process Expert UART Multidrop parity setup</title>
    <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/Process-Expert-UART-Multidrop-parity-setup/m-p/1589371#M14337</link>
    <description>&lt;P&gt;Hi Mike,&lt;/P&gt;&lt;P&gt;Thanks for legacy UART sample code for evaluation MCF5213 board. Importer classic (legacy) *.mcp project code never is working in CodeWarrior 11.1 (not seeing tooling), therefore I am always create from scratch new project using header and source files (and forget here Processor Expert components' ideas&lt;SPAN&gt;).&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;Hope using sample I can finally establish communication with node network devices, which using multidrop parities.&amp;nbsp;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Marceli&lt;/P&gt;</description>
    <pubDate>Mon, 30 Jan 2023 00:36:54 GMT</pubDate>
    <dc:creator>Marceli2022</dc:creator>
    <dc:date>2023-01-30T00:36:54Z</dc:date>
    <item>
      <title>Process Expert UART Multidrop parity setup</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/Process-Expert-UART-Multidrop-parity-setup/m-p/1587422#M14333</link>
      <description>&lt;P&gt;Dear Sir,&lt;/P&gt;&lt;P&gt;Processor Expert generates different registry addresses, as it was done before for UART having&lt;/P&gt;&lt;P&gt;#define MCF_UART_UMR_PM_MULTI_ADDR (0x1C).&amp;nbsp;I need setup it for using RS485.&lt;/P&gt;&lt;P&gt;PEx creates me for UART with even parity&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Marceli2022_0-1674612104637.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/208281i8BBDDE621455DBE9/image-size/medium?v=v2&amp;amp;px=400" role="button" title="Marceli2022_0-1674612104637.png" alt="Marceli2022_0-1674612104637.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;void AS2_Init(void)&lt;BR /&gt;{&lt;BR /&gt;SerFlag = 0x00; /* Reset flags */&lt;BR /&gt;/* UCR1: ??=0,MISC=3,TC=0,RC=0 */&lt;BR /&gt;setReg8(UCR1, 0x30U); /* Reset UART transmitter */&lt;BR /&gt;/* UCR1: ??=0,MISC=2,TC=0,RC=0 */&lt;BR /&gt;setReg8(UCR1, 0x20U); /* Reset UART receiver */&lt;BR /&gt;/* UMR11: RXRTS=0,RXIRQ=0,ERR=0,PM=0,PT=0,BC=3 */&lt;BR /&gt;setReg8(UMR11, 0x03U); /* Set the UMR1 register */&lt;BR /&gt;/* UMR21: CM=0,TXRTS=0,TXCTS=0,SB=7 */&lt;BR /&gt;setReg8(UMR21, 0x07U); /* Set the UMR2 register */&lt;BR /&gt;/* UCSR1: RCS=0x0D,TCS=0x0D */&lt;BR /&gt;setReg8(UCSR1, 0xDDU);&lt;BR /&gt;/* UBG11: Divider_MSB=0 */&lt;BR /&gt;setReg8(UBG11, 0x00U);&lt;BR /&gt;/* UBG21: Divider_LSB=0xF0 */&lt;BR /&gt;setReg8(UBG21, 0xF0U);&lt;BR /&gt;HWEnDi(); /* Enable/disable device according to status flags */&lt;BR /&gt;}&lt;/P&gt;&lt;P&gt;How to modify UART_UMR_PM registry to make multidrop parity?&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Marceli&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 25 Jan 2023 02:03:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/Process-Expert-UART-Multidrop-parity-setup/m-p/1587422#M14333</guid>
      <dc:creator>Marceli2022</dc:creator>
      <dc:date>2023-01-25T02:03:46Z</dc:date>
    </item>
    <item>
      <title>Re: Process Expert UART Multidrop parity setup</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/Process-Expert-UART-Multidrop-parity-setup/m-p/1587450#M14334</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;
&lt;P&gt;Which ColdFire product you are using? Please provide the part number.&lt;/P&gt;
&lt;P&gt;best regards,&lt;/P&gt;
&lt;P&gt;Mike&lt;/P&gt;</description>
      <pubDate>Wed, 25 Jan 2023 05:09:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/Process-Expert-UART-Multidrop-parity-setup/m-p/1587450#M14334</guid>
      <dc:creator>Hui_Ma</dc:creator>
      <dc:date>2023-01-25T05:09:48Z</dc:date>
    </item>
    <item>
      <title>Re: Process Expert UART Multidrop parity setup</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/Process-Expert-UART-Multidrop-parity-setup/m-p/1587453#M14335</link>
      <description>&lt;P&gt;Hi Mike,&lt;/P&gt;&lt;P&gt;I am using MCF5213ACF80.&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Marceli&lt;/P&gt;</description>
      <pubDate>Wed, 25 Jan 2023 05:35:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/Process-Expert-UART-Multidrop-parity-setup/m-p/1587453#M14335</guid>
      <dc:creator>Marceli2022</dc:creator>
      <dc:date>2023-01-25T05:35:06Z</dc:date>
    </item>
    <item>
      <title>Re: Process Expert UART Multidrop parity setup</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/Process-Expert-UART-Multidrop-parity-setup/m-p/1589293#M14336</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;First of all, sorry for the later reply.&lt;/P&gt;
&lt;P&gt;I could find below support record info about ColdFire(MCF5282) UART multidrop mode.&amp;nbsp; Hope below info could be helpful:&lt;BR /&gt;MCF5282 is using the same UART module with MCF5213.&lt;/P&gt;
&lt;PRE&gt;&lt;STRONG&gt;Question:&lt;/STRONG&gt;&lt;BR /&gt;As part of my recent development effort I’m trying to configure one of the UARTs of MCF5282 in multi-drop mode. The ISR is working fine in address detection mode but only once; then onward I’m not getting the interrupts. These are the set of operations that I’m performing on the UART2 module. 

Initialization() {
 Reset RX and TX;
  // Reset Mode register so it points to UMR1
  Aux-&amp;gt;AuxRegs-&amp;gt;CommandReg-&amp;gt;Register =AUX_RESET_MODE_PTR;
  Aux-&amp;gt;AuxRegs-&amp;gt;Mode1Reg-&amp;gt;Register = (BYTE)0|(CFAUX_PARITY_MULTIDROP_ADDR|Aux-&amp;gt;Line.DataBits);
  // Disable the receiver so that it wake up when we get the next address character
 Aux-&amp;gt;AuxRegs-&amp;gt;CommandReg-&amp;gt;Register =AUX_RX_DISABLE;
 Do rest of the UART initialization;
}

UART2ISR() {
  if (RxReady)  {
    while ((RxReady)||(FIFOFull)) {
     Do the necessary processing; 
     // Must read the Rx byte to clear the interrupt.
     // This also advances/clears the statReg bits to the values for the next queued byte.
   RxByte = Aux-&amp;gt;AuxRegs-&amp;gt;RxBufReg-&amp;gt;RxByte;
   // Check if it is my own address or broadcast address
   if ((MY_ADDRESS == RxByte) || (BCAST_ADDRESS == RxByte)) {
     // Data recording mode
     // Reset mode register pointer before access...
     Aux-&amp;gt;AuxRegs-&amp;gt;CommandReg-&amp;gt;Register =AUX_RESET_MODE_PTR;
    Aux-&amp;gt;AuxRegs-&amp;gt;Mode1Reg-&amp;gt;Register = (BYTE) 0 | (CFAUX_PARITY_MULTIDROP_DATA| Aux-&amp;gt;Line.DataBits);
    Aux-&amp;gt;AuxRegs-&amp;gt;CommandReg-&amp;gt;Register = AUX_RX_ENABLE;
   }
   else if (MESSAGE_TERMINATOR){
   // Address detection Mode
   ParityReg = CFAUX_PARITY_MULTIDROP_ADDR;
   // Reset mode register pointer before access...
   Aux-&amp;gt;AuxRegs-&amp;gt;CommandReg-&amp;gt;Register =AUX_RESET_MODE_PTR;
Aux-&amp;gt;AuxRegs-&amp;gt;Mode1Reg-&amp;gt;Register = (BYTE) 0 | (CFAUX_PARITY_MULTIDROP_ADDR | Aux-&amp;gt;Line.DataBits);
 Aux-&amp;gt;AuxRegs-&amp;gt;CommandReg-&amp;gt;Register =AUX_RX_DISABLE;
}
Address: Bit9 = Set; Bit8 to Bit1 = address
Data: Bit9 = Clear; Bit8 to Bit1 = Data
Terminator: Bit9 = Set; Bit8 to Bit1 = 0xFF
Can you please help me with this.&lt;/PRE&gt;
&lt;PRE&gt;&lt;STRONG&gt;Answer&lt;/STRONG&gt;&lt;BR /&gt;Regarding your inquiry, I am not sure if you have configured UART2 to work in interrupt mode, to do this in user_config.h you need to enable ITTYC = 1. 

The MCF5282 only supports 5–8 data bits plus parity. The &lt;FONT class="&amp;amp;quothighlight&amp;quot;"&gt;&lt;STRONG&gt;parity&lt;/STRONG&gt;&lt;/FONT&gt; bit could be used as the 9th bit.
There are the UMR1n[PM; PT] bits which it is in position to set up either for Force parity, or for &lt;FONT class="&amp;amp;quothighlight&amp;quot;"&gt;&lt;STRONG&gt;Multidrop&lt;/STRONG&gt;&lt;/FONT&gt; mode. In &lt;FONT class="&amp;amp;quothighlight&amp;quot;"&gt;&lt;STRONG&gt;multidrop&lt;/STRONG&gt;&lt;/FONT&gt; mode, the address character has the 9th bit==1 and data character has the 9th bit==0 (8bit character is assumed).

Any way, this will require a change in the UMR1n mode register before a character is pushed to the transmit buffer. A change in UMR1n needs to perform RESET MODE REGISTER POINTER and RESET TRANSMITTER/RECEIVER commands (UCRn command register) in advance.
&lt;/PRE&gt;
&lt;P&gt;About UART UMR register setting, there with below info for your reference:&lt;/P&gt;
&lt;P&gt;&lt;STRONG&gt;Qustion:&lt;/STRONG&gt; There are two registers _UMR1 and _UMR2. But the have the same ipsbar-offset!!! How should this work?&lt;BR /&gt;&lt;STRONG&gt;Answer:&lt;/STRONG&gt; There is one pointer to UMR1n and UMR2n registers.&lt;BR /&gt;The UMR1n can be read or written when the mode register pointer points to it&lt;BR /&gt;&amp;gt; After Reset of CPU&lt;BR /&gt;&amp;gt; After RESET MODE REGISTER POINTER command using UCRn[MISC].&lt;BR /&gt;After UMR1n is read or written , pointer points to UMR2n and can UMR2n can be accessed .&lt;BR /&gt;UMR2n access doesn't update the pointer !&lt;/P&gt;
&lt;P&gt;I attached related code for your reference.&lt;/P&gt;
&lt;P&gt;Wish it helps.&lt;/P&gt;
&lt;P&gt;Mike&lt;/P&gt;</description>
      <pubDate>Sun, 29 Jan 2023 08:03:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/Process-Expert-UART-Multidrop-parity-setup/m-p/1589293#M14336</guid>
      <dc:creator>Hui_Ma</dc:creator>
      <dc:date>2023-01-29T08:03:58Z</dc:date>
    </item>
    <item>
      <title>Re: Process Expert UART Multidrop parity setup</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/Process-Expert-UART-Multidrop-parity-setup/m-p/1589371#M14337</link>
      <description>&lt;P&gt;Hi Mike,&lt;/P&gt;&lt;P&gt;Thanks for legacy UART sample code for evaluation MCF5213 board. Importer classic (legacy) *.mcp project code never is working in CodeWarrior 11.1 (not seeing tooling), therefore I am always create from scratch new project using header and source files (and forget here Processor Expert components' ideas&lt;SPAN&gt;).&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;Hope using sample I can finally establish communication with node network devices, which using multidrop parities.&amp;nbsp;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Marceli&lt;/P&gt;</description>
      <pubDate>Mon, 30 Jan 2023 00:36:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/Process-Expert-UART-Multidrop-parity-setup/m-p/1589371#M14337</guid>
      <dc:creator>Marceli2022</dc:creator>
      <dc:date>2023-01-30T00:36:54Z</dc:date>
    </item>
    <item>
      <title>Re: Process Expert UART Multidrop parity setup</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/Process-Expert-UART-Multidrop-parity-setup/m-p/1589436#M14338</link>
      <description>&lt;P&gt;Hi Mike,&lt;/P&gt;&lt;P&gt;To avoid complexity, Init_UART component consist multidrop parity settings. Therefore it seems convenient to replace one line with:&lt;/P&gt;&lt;P&gt;setReg8(UIMR1, 0x00U);&lt;BR /&gt;/* UMR11: RXRTS=0,RXIRQ=0,ERR=0,PM=3,PT=1,BC=3 multidrop addressable*/&lt;/P&gt;&lt;P&gt;,which consist PM and PT bits. I believe it need be only done initially. After I can use other UART_Serial component parts. It could be good to components update. If it works it should be straight applicable to MCF5282 chip as well.&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Marceli&lt;/P&gt;</description>
      <pubDate>Mon, 30 Jan 2023 03:14:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/Process-Expert-UART-Multidrop-parity-setup/m-p/1589436#M14338</guid>
      <dc:creator>Marceli2022</dc:creator>
      <dc:date>2023-01-30T03:14:37Z</dc:date>
    </item>
    <item>
      <title>Re: Process Expert UART Multidrop parity setup</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/Process-Expert-UART-Multidrop-parity-setup/m-p/1590230#M14340</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;SPAN&gt;Marceli,&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;Thank you for the feedback and let us know the result.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;best regards,&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;Mike&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Tue, 31 Jan 2023 03:21:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/Process-Expert-UART-Multidrop-parity-setup/m-p/1590230#M14340</guid>
      <dc:creator>Hui_Ma</dc:creator>
      <dc:date>2023-01-31T03:21:32Z</dc:date>
    </item>
    <item>
      <title>Re: Process Expert UART Multidrop parity setup</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/Process-Expert-UART-Multidrop-parity-setup/m-p/1591040#M14341</link>
      <description>&lt;P&gt;What are the other RS485 devices do you have on the bus? Are they all Freescale CPUs? I ask because "Multidrop" means a lot more than just that "parity setting". That just allows the parity bit" to be used to discriminate address and data in one (of many) possible multidrop protocols. You also need careful control of receiving, transmitting and the transmit-enable pin on the RS485 Transceiver chip for it to all work. Together with whatever "higher level protocol" is in use. Good luck.&lt;/P&gt;&lt;P&gt;Tom&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 01 Feb 2023 06:49:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/Process-Expert-UART-Multidrop-parity-setup/m-p/1591040#M14341</guid>
      <dc:creator>TomE</dc:creator>
      <dc:date>2023-02-01T06:49:17Z</dc:date>
    </item>
    <item>
      <title>Re: Process Expert UART Multidrop parity setup</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/Process-Expert-UART-Multidrop-parity-setup/m-p/1600706#M14344</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;Here, I working with RS485 to communicate with Microchip&amp;nbsp;PIC18F6720. In the chip RM datasheet (Table 21-3) description is Multidrop parity Address character or Data character type, which can be selected by PEx for use UART initial component. Does switching between both for address byte and data bytes need be done, or need to switch into Low parity type?&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Marceli2022_0-1676588519735.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/211275i7786EFBE35B53C66/image-size/medium?v=v2&amp;amp;px=400" role="button" title="Marceli2022_0-1676588519735.png" alt="Marceli2022_0-1676588519735.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;Marceli&lt;/P&gt;</description>
      <pubDate>Thu, 16 Feb 2023 23:02:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/Process-Expert-UART-Multidrop-parity-setup/m-p/1600706#M14344</guid>
      <dc:creator>Marceli2022</dc:creator>
      <dc:date>2023-02-16T23:02:39Z</dc:date>
    </item>
    <item>
      <title>Re: Process Expert UART Multidrop parity setup</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/Process-Expert-UART-Multidrop-parity-setup/m-p/1604338#M14346</link>
      <description>&lt;P&gt;I don't know how it works.&lt;/P&gt;&lt;P&gt;Read Section "23.4.4 Multidrop Mode" of the User Manual. It gives a pretty good description of how you're meant to use the hardware the achieve the transmission and reception.&lt;/P&gt;&lt;P&gt;I suggest you also download the PIC18F6720 Data Sheet and read the USART section, specifically "18.2.3 Setting up 9-Bit Mode With Address Detect".&lt;/P&gt;&lt;P&gt;Reading both of those together (as they're the opposite ends of the same comms link) should give you enough information to work out how to use it.&lt;/P&gt;&lt;P&gt;It looks like your software does have to receive the "Address Byte" (in an interrupt routine), determine if "this device is addressed" and then switch to receiving the data if so. The whole protocol is an "efficiency hack" so that all devices don't have to spend time (and maybe battery power) receiving all data bytes. You could probably receive all data bytes and handle the protocol in software if you wanted.&lt;/P&gt;&lt;P&gt;Tom&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 23 Feb 2023 06:42:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/Process-Expert-UART-Multidrop-parity-setup/m-p/1604338#M14346</guid>
      <dc:creator>TomE</dc:creator>
      <dc:date>2023-02-23T06:42:43Z</dc:date>
    </item>
  </channel>
</rss>