<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>ColdFire/68K Microcontrollers and Processors中的主题 Re: SDRAM configuration in Coldfire MCF54415</title>
    <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/SDRAM-configuration-in-Coldfire-MCF54415/m-p/1337309#M14140</link>
    <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;I would recommend customer to refer related thread at &lt;A href="https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/MCF54415-External-Flash/m-p/1330466#M14129" target="_self"&gt;here&lt;/A&gt;.&lt;/P&gt;
&lt;P&gt;Customer could refer MCF5441x validation code about DDR2 controller module initialization code with [DDR2] project.&lt;/P&gt;
&lt;P&gt;Related code located at &amp;lt;modelo_ddr2.c&amp;gt; file with [configure_ddr_memory] function and [ddr2_mem_configuration] function.&lt;/P&gt;
&lt;P&gt;About copy Flash data to DDR2 memory, customer could refer example code at &amp;lt;startup.c&amp;gt; with [startup] function (Move initialized data from ROM to RAM. ).&lt;/P&gt;
&lt;P&gt;Wish it helps.&lt;/P&gt;
&lt;P&gt;Mike&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Thu, 09 Sep 2021 02:28:51 GMT</pubDate>
    <dc:creator>Hui_Ma</dc:creator>
    <dc:date>2021-09-09T02:28:51Z</dc:date>
    <item>
      <title>SDRAM configuration in Coldfire MCF54415</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/SDRAM-configuration-in-Coldfire-MCF54415/m-p/1337054#M14138</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I have DDR2 SDRAM 64Mx8 chip interfaced with the MCF5441X Coldfire processor. I am trying to find an example that configures DDR2 SDRAM controller in a coldfire processor and also copy memory from FLASH to SDRAM. Any help/ suggestion is much appreciated.&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Sai K.&lt;/P&gt;</description>
      <pubDate>Wed, 08 Sep 2021 17:42:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/SDRAM-configuration-in-Coldfire-MCF54415/m-p/1337054#M14138</guid>
      <dc:creator>Skankanala</dc:creator>
      <dc:date>2021-09-08T17:42:19Z</dc:date>
    </item>
    <item>
      <title>Re: SDRAM configuration in Coldfire MCF54415</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/SDRAM-configuration-in-Coldfire-MCF54415/m-p/1337309#M14140</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;I would recommend customer to refer related thread at &lt;A href="https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/MCF54415-External-Flash/m-p/1330466#M14129" target="_self"&gt;here&lt;/A&gt;.&lt;/P&gt;
&lt;P&gt;Customer could refer MCF5441x validation code about DDR2 controller module initialization code with [DDR2] project.&lt;/P&gt;
&lt;P&gt;Related code located at &amp;lt;modelo_ddr2.c&amp;gt; file with [configure_ddr_memory] function and [ddr2_mem_configuration] function.&lt;/P&gt;
&lt;P&gt;About copy Flash data to DDR2 memory, customer could refer example code at &amp;lt;startup.c&amp;gt; with [startup] function (Move initialized data from ROM to RAM. ).&lt;/P&gt;
&lt;P&gt;Wish it helps.&lt;/P&gt;
&lt;P&gt;Mike&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 09 Sep 2021 02:28:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/SDRAM-configuration-in-Coldfire-MCF54415/m-p/1337309#M14140</guid>
      <dc:creator>Hui_Ma</dc:creator>
      <dc:date>2021-09-09T02:28:51Z</dc:date>
    </item>
  </channel>
</rss>