<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>ColdFire/68K Microcontrollers and Processors中的主题 Crystal selection</title>
    <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/Crystal-selection/m-p/1236544#M14042</link>
    <description>&lt;P&gt;Hi, We are working with the&amp;nbsp;MCF51QM128VLH 32bit MCU. Currently, We are using&amp;nbsp;&lt;SPAN&gt;ECS-080-18-23A-JGN-TR crystal with no load capacitance. Now we are planning to define ECS-80-18-30-JGN-TR as alternate crystal whose ESR is 100ohm instead of 80ohms of ECS-080-18-23A-JGN-TR. Generally the&amp;nbsp; RNEG(negative resistance) of the amplifier should be grater than or equal to 5*ESR.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;So please let us know RNEG(Negative resistance) of the amplifier the MCU can provide to the crystal. If the MCU can provide the RNEG &amp;gt;= 500ohms&amp;nbsp; or not?&amp;nbsp;&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Would you suggest ECS-80-18-30-JGN-TR as an alternate crystal ?&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Thu, 25 Feb 2021 10:32:17 GMT</pubDate>
    <dc:creator>sanket_patadiya</dc:creator>
    <dc:date>2021-02-25T10:32:17Z</dc:date>
    <item>
      <title>Crystal selection</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/Crystal-selection/m-p/1236544#M14042</link>
      <description>&lt;P&gt;Hi, We are working with the&amp;nbsp;MCF51QM128VLH 32bit MCU. Currently, We are using&amp;nbsp;&lt;SPAN&gt;ECS-080-18-23A-JGN-TR crystal with no load capacitance. Now we are planning to define ECS-80-18-30-JGN-TR as alternate crystal whose ESR is 100ohm instead of 80ohms of ECS-080-18-23A-JGN-TR. Generally the&amp;nbsp; RNEG(negative resistance) of the amplifier should be grater than or equal to 5*ESR.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;So please let us know RNEG(Negative resistance) of the amplifier the MCU can provide to the crystal. If the MCU can provide the RNEG &amp;gt;= 500ohms&amp;nbsp; or not?&amp;nbsp;&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Would you suggest ECS-80-18-30-JGN-TR as an alternate crystal ?&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 25 Feb 2021 10:32:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/Crystal-selection/m-p/1236544#M14042</guid>
      <dc:creator>sanket_patadiya</dc:creator>
      <dc:date>2021-02-25T10:32:17Z</dc:date>
    </item>
    <item>
      <title>Re: Crystal selection</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/Crystal-selection/m-p/1522353#M14270</link>
      <description>&lt;P&gt;I don't have an answer,&lt;/P&gt;&lt;P&gt;I have the same question, but for a different processor&lt;/P&gt;&lt;P&gt;need to know what the absolute negative resistance value (Rs) for&amp;nbsp;DSP56F803?&lt;/P&gt;&lt;P&gt;Need this value to select an alternative&amp;nbsp; 8Mhz crystal oscillator, ESR=100, without load caps.&lt;/P&gt;&lt;P&gt;need to verify Rs is at least 500 ohms&lt;/P&gt;&lt;P&gt;The Driver circuit inside the processor is what determines the negative resistance not the crystal supplier.&lt;/P&gt;&lt;P&gt;The NXT/Freescale Semi datasheets and manuals for this part to not mention or show this value.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="MikeC1_0-1663197956050.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/193693i6820E456E2B1EEEE/image-size/medium?v=v2&amp;amp;px=400" role="button" title="MikeC1_0-1663197956050.png" alt="MikeC1_0-1663197956050.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;Can anyone help with this?&lt;/P&gt;</description>
      <pubDate>Wed, 14 Sep 2022 23:27:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/Crystal-selection/m-p/1522353#M14270</guid>
      <dc:creator>MikeC1</dc:creator>
      <dc:date>2022-09-14T23:27:55Z</dc:date>
    </item>
    <item>
      <title>Re: Crystal selection</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/Crystal-selection/m-p/1523878#M14272</link>
      <description>&lt;P&gt;Searching this site for Application Notes:&lt;/P&gt;&lt;P&gt;&lt;A href="https://www.nxp.com/docs/en/application-note/AN1706.pdf" target="_blank"&gt;https://www.nxp.com/docs/en/application-note/AN1706.pdf&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="https://www.nxp.com/docs/en/application-note/AN1783.pdf" target="_blank"&gt;https://www.nxp.com/docs/en/application-note/AN1783.pdf&lt;/A&gt;&lt;/P&gt;&lt;P&gt;They're a bit hard-core. Here's the simple way to verify the oscillator margin:&lt;/P&gt;&lt;P&gt;&lt;A href="https://www.murata.com/en-sg/products/timingdevice/crystalu/overview/basic/margin" target="_blank"&gt;https://www.murata.com/en-sg/products/timingdevice/crystalu/overview/basic/margin&lt;/A&gt;&lt;/P&gt;&lt;P&gt;The latter is very simple. Take the crystal ESR. Multiply by 5. Pick a resistor of that value. Solder that in series with the crystal. Does it oscillate? If it does you have a margin of "5". For the advanced case, put the device in an environmental chamber and make sure it keeps working over the full temperature range.&lt;/P&gt;&lt;P&gt;Tom&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Sun, 18 Sep 2022 23:29:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/Crystal-selection/m-p/1523878#M14272</guid>
      <dc:creator>TomE</dc:creator>
      <dc:date>2022-09-18T23:29:42Z</dc:date>
    </item>
  </channel>
</rss>