<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>ColdFire/68K Microcontrollers and ProcessorsのトピックRe: AppTRK.elf file missing in MCF5282 pre installed Ulinux</title>
    <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/AppTRK-elf-file-missing-in-MCF5282-pre-installed-Ulinux/m-p/1036746#M13934</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi ,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks for the update.&lt;/P&gt;&lt;P&gt;Please let us know what we can do for you when there still with compile error. Thanks.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;best regards,&lt;/P&gt;&lt;P&gt;Mike&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 29 Nov 2019 01:34:40 GMT</pubDate>
    <dc:creator>Hui_Ma</dc:creator>
    <dc:date>2019-11-29T01:34:40Z</dc:date>
    <item>
      <title>AppTRK.elf file missing in MCF5282 pre installed Ulinux</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/AppTRK-elf-file-missing-in-MCF5282-pre-installed-Ulinux/m-p/1036743#M13931</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I am working on DNP/EVA6(REV 1.2 board) with coldfire MCF5282CVM66. When I read the documentation, it was mentioned that I have to start the AppTRK agent(Apptrk.elf) to have a communication between the evaluation board and codewarrior IDE.&lt;/P&gt;&lt;P&gt;But when I searched for the apptrk.elf file, it was missing. Please ignore my ignorance. How to add the apptrk.elf manually or should I flash a new linux image on to the DNP/EVA6 board. If thats the case, could you please suggest me how to do it&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 26 Nov 2019 13:39:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/AppTRK-elf-file-missing-in-MCF5282-pre-installed-Ulinux/m-p/1036743#M13931</guid>
      <dc:creator>sp2</dc:creator>
      <dc:date>2019-11-26T13:39:06Z</dc:date>
    </item>
    <item>
      <title>Re: AppTRK.elf file missing in MCF5282 pre installed Ulinux</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/AppTRK-elf-file-missing-in-MCF5282-pre-installed-Ulinux/m-p/1036744#M13932</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Which board you are using?&lt;/P&gt;&lt;P&gt;Please help to provide the part number.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Mike&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt; Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 28 Nov 2019 07:11:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/AppTRK-elf-file-missing-in-MCF5282-pre-installed-Ulinux/m-p/1036744#M13932</guid>
      <dc:creator>Hui_Ma</dc:creator>
      <dc:date>2019-11-28T07:11:09Z</dc:date>
    </item>
    <item>
      <title>Re: AppTRK.elf file missing in MCF5282 pre installed Ulinux</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/AppTRK-elf-file-missing-in-MCF5282-pre-installed-Ulinux/m-p/1036745#M13933</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Hui_Ma,&lt;/P&gt;&lt;P&gt;Thanks for the reply. I am using DNP/EVA6 kit (with DNP5282 board). I have been now able to start the apptrk.elf port from the board through which Freescale codewarrior IDE can open the connection. But since its a version 2 coldfire core, there is no proper toolchain support for the IDE.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;When I trz to compile the files in codewarrior IDE, it is throwing some error. I have to check on that&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 28 Nov 2019 12:54:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/AppTRK-elf-file-missing-in-MCF5282-pre-installed-Ulinux/m-p/1036745#M13933</guid>
      <dc:creator>sp2</dc:creator>
      <dc:date>2019-11-28T12:54:49Z</dc:date>
    </item>
    <item>
      <title>Re: AppTRK.elf file missing in MCF5282 pre installed Ulinux</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/AppTRK-elf-file-missing-in-MCF5282-pre-installed-Ulinux/m-p/1036746#M13934</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi ,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks for the update.&lt;/P&gt;&lt;P&gt;Please let us know what we can do for you when there still with compile error. Thanks.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;best regards,&lt;/P&gt;&lt;P&gt;Mike&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 29 Nov 2019 01:34:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/AppTRK-elf-file-missing-in-MCF5282-pre-installed-Ulinux/m-p/1036746#M13934</guid>
      <dc:creator>Hui_Ma</dc:creator>
      <dc:date>2019-11-29T01:34:40Z</dc:date>
    </item>
  </channel>
</rss>