<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>ColdFire/68K Microcontrollers and ProcessorsのトピックRe: MCF5485 Flexbus lines level at start up?</title>
    <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/MCF5485-Flexbus-lines-level-at-start-up/m-p/986218#M13864</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Since it is easy to do, I would test this. Jam the chip in Reset and see if the pins read high with a resistive load on them. The 1M/10M resistance of an oscilloscope probe would be enough for an initial measure. Then remove Reset and see if they change.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Otherwise, if you have signals where it is important that they don't float at reset, add pull resistors to the hardware design.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;There might be a difference between "State During Reset" and "State After Reset". With some chips, even dedicated output pins are tri-state when the reset pin is asserted. If this is important to you it is worth checking on the bench.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If you read the RM Errata, Table 2.1 has been updated 9 times, although changing the reset state isn't listed as a change. That may explain why it is correct.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Tom&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 19 Nov 2019 22:37:54 GMT</pubDate>
    <dc:creator>TomE</dc:creator>
    <dc:date>2019-11-19T22:37:54Z</dc:date>
    <item>
      <title>MCF5485 Flexbus lines level at start up?</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/MCF5485-Flexbus-lines-level-at-start-up/m-p/986215#M13861</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hey! I have a question as to what level the Flexbus lines come up as on the MCF5485.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The Table 2-1 of the RM shows FBCS[5:0] and BE come up as high.&lt;/P&gt;&lt;P&gt;However, table 17-1 shows they come up as Hi-Z&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="flexbus1.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/92314i3BD48E709BAECCC2/image-size/large?v=v2&amp;amp;px=999" role="button" title="flexbus1.png" alt="flexbus1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="flexbus2.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/92366i22007059603D46C6/image-size/large?v=v2&amp;amp;px=999" role="button" title="flexbus2.png" alt="flexbus2.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="flexbus3.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/92392iD182719E62C8B7E8/image-size/large?v=v2&amp;amp;px=999" role="button" title="flexbus3.png" alt="flexbus3.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 13 Nov 2019 19:38:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/MCF5485-Flexbus-lines-level-at-start-up/m-p/986215#M13861</guid>
      <dc:creator>zwilcox</dc:creator>
      <dc:date>2019-11-13T19:38:34Z</dc:date>
    </item>
    <item>
      <title>Re: MCF5485 Flexbus lines level at start up?</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/MCF5485-Flexbus-lines-level-at-start-up/m-p/986216#M13862</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The&amp;nbsp;&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;Table 2-1 of the RM shows FBCS[5:0] and BE come up as high is correct.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;best regards，&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;Mike&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 15 Nov 2019 09:37:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/MCF5485-Flexbus-lines-level-at-start-up/m-p/986216#M13862</guid>
      <dc:creator>Hui_Ma</dc:creator>
      <dc:date>2019-11-15T09:37:02Z</dc:date>
    </item>
    <item>
      <title>Re: MCF5485 Flexbus lines level at start up?</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/MCF5485-Flexbus-lines-level-at-start-up/m-p/986217#M13863</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks :smileyhappy:&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 15 Nov 2019 17:48:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/MCF5485-Flexbus-lines-level-at-start-up/m-p/986217#M13863</guid>
      <dc:creator>zwilcox</dc:creator>
      <dc:date>2019-11-15T17:48:06Z</dc:date>
    </item>
    <item>
      <title>Re: MCF5485 Flexbus lines level at start up?</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/MCF5485-Flexbus-lines-level-at-start-up/m-p/986218#M13864</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Since it is easy to do, I would test this. Jam the chip in Reset and see if the pins read high with a resistive load on them. The 1M/10M resistance of an oscilloscope probe would be enough for an initial measure. Then remove Reset and see if they change.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Otherwise, if you have signals where it is important that they don't float at reset, add pull resistors to the hardware design.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;There might be a difference between "State During Reset" and "State After Reset". With some chips, even dedicated output pins are tri-state when the reset pin is asserted. If this is important to you it is worth checking on the bench.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If you read the RM Errata, Table 2.1 has been updated 9 times, although changing the reset state isn't listed as a change. That may explain why it is correct.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Tom&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 19 Nov 2019 22:37:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/MCF5485-Flexbus-lines-level-at-start-up/m-p/986218#M13864</guid>
      <dc:creator>TomE</dc:creator>
      <dc:date>2019-11-19T22:37:54Z</dc:date>
    </item>
  </channel>
</rss>