<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic What is the dif between MCF5253 and MCF5251? in ColdFire/68K Microcontrollers and Processors</title>
    <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/What-is-the-dif-between-MCF5253-and-MCF5251/m-p/964876#M13843</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;What is the dif between MCF5253 and MCF5251? If we have been using the 5253 can we switch to the 5251?&lt;/P&gt;&lt;P&gt;Thank you&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 07 Aug 2019 19:49:37 GMT</pubDate>
    <dc:creator>tkrajewski</dc:creator>
    <dc:date>2019-08-07T19:49:37Z</dc:date>
    <item>
      <title>What is the dif between MCF5253 and MCF5251?</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/What-is-the-dif-between-MCF5253-and-MCF5251/m-p/964876#M13843</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;What is the dif between MCF5253 and MCF5251? If we have been using the 5253 can we switch to the 5251?&lt;/P&gt;&lt;P&gt;Thank you&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 07 Aug 2019 19:49:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/What-is-the-dif-between-MCF5253-and-MCF5251/m-p/964876#M13843</guid>
      <dc:creator>tkrajewski</dc:creator>
      <dc:date>2019-08-07T19:49:37Z</dc:date>
    </item>
    <item>
      <title>Re: What is the dif between MCF5253 and MCF5251?</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/What-is-the-dif-between-MCF5253-and-MCF5251/m-p/964877#M13844</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;MCF5253 has the same modules with MCF5251. &lt;BR /&gt;The differences between two chips is that: &lt;BR /&gt;The MCF5251 which comes with license access to a variety of MP3 encode and decoders and the MCF5253 which is a cheaper version that doesn't come with audio software licenses.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;MCF5253 is pin to pin compatible with MCF5251.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;best regards,&lt;/P&gt;&lt;P&gt;Mike&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 08 Aug 2019 08:20:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/What-is-the-dif-between-MCF5253-and-MCF5251/m-p/964877#M13844</guid>
      <dc:creator>Hui_Ma</dc:creator>
      <dc:date>2019-08-08T08:20:16Z</dc:date>
    </item>
  </channel>
</rss>