<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: use static library created on codewarried IDE 5.6 in 10.7 for MCF5208 controller  in ColdFire/68K Microcontrollers and Processors</title>
    <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/use-static-library-created-on-codewarried-IDE-5-6-in-10-7-for/m-p/895439#M13750</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Migrating from versions prior to 7.2 to those later takes a lot of work. That can't be avoided.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;it is unlikely your "static library" will work because the ABI between the two compilers is different. One passes parameters on the stack and the other passes in registers. You can't code around that fundamental difference.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;You're far better off recompiling your code under the new compiler. If there's anything obviously wrong, the new compiler should tell you. You'll only have problems if you have inline assembly or assembly source files, because they explicitly code the ABI (which is the bit that changed). Also note in various App Notes that libraries have changed as well, so if you're relying on old libraries you may have to port the code to new ones.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I should be able to point you to the links in this article. The links used to work.They of course point to "community.freescale.com" and not "community.nxp.com", but should redirect, or the article numbers should work, but they don't.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A _jive_internal="true" class="link-titled" href="https://community.nxp.com/thread/478562?commentID=1028460#comment" title="https://community.nxp.com/message/1028460?commentID=1028460#comment-1028460"&gt;https://community.nxp.com/message/1028460?commentID=1028460#comment-1028460&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;See which ones of them you can still locate.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Read this one. Search for "REG_ABI" in the Search-thing and see what you can find.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A _jive_internal="true" class="link-titled" href="https://community.nxp.com/message/401840?commentID=401840#comment-401840" title="https://community.nxp.com/message/401840?commentID=401840#comment-401840"&gt;https://community.nxp.com/message/401840?commentID=401840#comment-401840&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Tom&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 20 May 2019 04:09:11 GMT</pubDate>
    <dc:creator>TomE</dc:creator>
    <dc:date>2019-05-20T04:09:11Z</dc:date>
    <item>
      <title>use static library created on codewarried IDE 5.6 in 10.7 for MCF5208 controller</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/use-static-library-created-on-codewarried-IDE-5-6-in-10-7-for/m-p/895437#M13748</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;The IDE which I use is quite old (&lt;SPAN style="color: #000000; background-color: #ffffff; font-weight: 200; font-size: 12.96px;"&gt;IDE version 5.7.0 build 2264)&lt;/SPAN&gt; and it works only on WinXp machine. I wanted to migrate this IDE to latest one&amp;nbsp; CodeWarrior for MCU&amp;nbsp;Version: 10.7 Build Id:160721 it does support MCF5208 but uses GNU library. To avoid bigger risk in recompile complete code on new compiler instead I want to create a static library of exiting code&amp;nbsp; base from old version of IDE&amp;nbsp;then include in&amp;nbsp;latest version of IDE as a static library and in future development can continue on latest version of IDE.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 May 2019 21:56:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/use-static-library-created-on-codewarried-IDE-5-6-in-10-7-for/m-p/895437#M13748</guid>
      <dc:creator>pawan_modi</dc:creator>
      <dc:date>2019-05-15T21:56:21Z</dc:date>
    </item>
    <item>
      <title>Re: use static library created on codewarried IDE 5.6 in 10.7 for MCF5208 controller</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/use-static-library-created-on-codewarried-IDE-5-6-in-10-7-for/m-p/895438#M13749</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi，&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;There are two application note about porting classic ColdFire project to CodeWarrior for MCU V10.x version.&lt;/P&gt;&lt;P&gt;Please check below link for the detailed info.&lt;/P&gt;&lt;P&gt;&lt;A href="https://www.nxp.com/docs/en/application-note/AN4727.pdf"&gt;AN4727 &lt;/A&gt;&amp;amp; &lt;A href="https://www.nxp.com/docs/en/application-note/AN4104.pdf"&gt;AN4104&lt;/A&gt;.&lt;/P&gt;&lt;P&gt;About create a static library, please refer &lt;A href="https://www.nxp.com/webapp/Download?colCode=CWMCUDBGUG&amp;amp;location=null"&gt;CWMCUDBGUG &lt;/A&gt;document:&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/81649i9DFF650EDFA75118/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;Wish it helps.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Mike&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt; Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 20 May 2019 02:51:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/use-static-library-created-on-codewarried-IDE-5-6-in-10-7-for/m-p/895438#M13749</guid>
      <dc:creator>Hui_Ma</dc:creator>
      <dc:date>2019-05-20T02:51:44Z</dc:date>
    </item>
    <item>
      <title>Re: use static library created on codewarried IDE 5.6 in 10.7 for MCF5208 controller</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/use-static-library-created-on-codewarried-IDE-5-6-in-10-7-for/m-p/895439#M13750</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Migrating from versions prior to 7.2 to those later takes a lot of work. That can't be avoided.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;it is unlikely your "static library" will work because the ABI between the two compilers is different. One passes parameters on the stack and the other passes in registers. You can't code around that fundamental difference.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;You're far better off recompiling your code under the new compiler. If there's anything obviously wrong, the new compiler should tell you. You'll only have problems if you have inline assembly or assembly source files, because they explicitly code the ABI (which is the bit that changed). Also note in various App Notes that libraries have changed as well, so if you're relying on old libraries you may have to port the code to new ones.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I should be able to point you to the links in this article. The links used to work.They of course point to "community.freescale.com" and not "community.nxp.com", but should redirect, or the article numbers should work, but they don't.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A _jive_internal="true" class="link-titled" href="https://community.nxp.com/thread/478562?commentID=1028460#comment" title="https://community.nxp.com/message/1028460?commentID=1028460#comment-1028460"&gt;https://community.nxp.com/message/1028460?commentID=1028460#comment-1028460&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;See which ones of them you can still locate.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Read this one. Search for "REG_ABI" in the Search-thing and see what you can find.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A _jive_internal="true" class="link-titled" href="https://community.nxp.com/message/401840?commentID=401840#comment-401840" title="https://community.nxp.com/message/401840?commentID=401840#comment-401840"&gt;https://community.nxp.com/message/401840?commentID=401840#comment-401840&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Tom&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 20 May 2019 04:09:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/use-static-library-created-on-codewarried-IDE-5-6-in-10-7-for/m-p/895439#M13750</guid>
      <dc:creator>TomE</dc:creator>
      <dc:date>2019-05-20T04:09:11Z</dc:date>
    </item>
  </channel>
</rss>