<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>ColdFire/68K Microcontrollers and Processors中的主题 Re: MCF54417 RMII</title>
    <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/MCF54417-RMII/m-p/883799#M13706</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Well, from the hardware schematic, I do not think that the pull-up/pull-down is a issue. Actually as mentioned by the datasheet of KSZ8081RNA that:&lt;/P&gt;&lt;P&gt;"The PHYAD[1:0] strap-in pin is latched at the de-assertion of reset. In some systems, the RMII MAC receive input pins may drive high/low during power-up or reset, and consequently cause the PHYAD[1:0] strap-in pin, a shared pin with the RMII CRS_DV signal, to be latched to the unintended high/low state. In this case an external pull-up (4.7 kΩ) or pulldown (1.0 kΩ) should be added on the PHYAD[1:0] strap-in pin to ensure that the intended value is strapped-in correctly."&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;So my query is for software driver, do you config the PHY driver correctly? We only provide the DP83849I driver with TWR-MCF5441X.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 14 Feb 2019 06:21:05 GMT</pubDate>
    <dc:creator>miduo</dc:creator>
    <dc:date>2019-02-14T06:21:05Z</dc:date>
    <item>
      <title>MCF54417 RMII</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/MCF54417-RMII/m-p/883798#M13705</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Processor:&amp;nbsp; MCF54417&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am tasked with troubleshooting someone else's MCF54417 RMII design.&amp;nbsp; We seem to be losing connectivity intermittently.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Attached is the layout.&amp;nbsp; I am wondering the pull-up and pull-down resistors on RMII_CRS_DV are correct?&amp;nbsp; There is a pull-up on RMII0 and a pull-down on RMII1?&amp;nbsp; Any other external components missing?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Please advise.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 04 Feb 2019 19:28:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/MCF54417-RMII/m-p/883798#M13705</guid>
      <dc:creator>bplatt</dc:creator>
      <dc:date>2019-02-04T19:28:04Z</dc:date>
    </item>
    <item>
      <title>Re: MCF54417 RMII</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/MCF54417-RMII/m-p/883799#M13706</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Well, from the hardware schematic, I do not think that the pull-up/pull-down is a issue. Actually as mentioned by the datasheet of KSZ8081RNA that:&lt;/P&gt;&lt;P&gt;"The PHYAD[1:0] strap-in pin is latched at the de-assertion of reset. In some systems, the RMII MAC receive input pins may drive high/low during power-up or reset, and consequently cause the PHYAD[1:0] strap-in pin, a shared pin with the RMII CRS_DV signal, to be latched to the unintended high/low state. In this case an external pull-up (4.7 kΩ) or pulldown (1.0 kΩ) should be added on the PHYAD[1:0] strap-in pin to ensure that the intended value is strapped-in correctly."&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;So my query is for software driver, do you config the PHY driver correctly? We only provide the DP83849I driver with TWR-MCF5441X.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 14 Feb 2019 06:21:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/MCF54417-RMII/m-p/883799#M13706</guid>
      <dc:creator>miduo</dc:creator>
      <dc:date>2019-02-14T06:21:05Z</dc:date>
    </item>
  </channel>
</rss>