<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>ColdFire/68K Microcontrollers and Processors中的主题 Re: USB receptable type</title>
    <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/USB-receptable-type/m-p/748744#M13373</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&amp;gt; When you connect 2 OTG systems with a micro-USB cable, host must be micro-USB type AB&lt;/P&gt;&lt;P&gt;&amp;gt; and device must be micro-USB type B, isn't it ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Not according to Wikipedia:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="https://en.wikipedia.org/wiki/USB_On-The-Go#OTG_micro_plugs"&gt;https://en.wikipedia.org/wiki/USB_On-The-Go#OTG_micro_plugs&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P style="padding-left: 30px;"&gt;Micro-A adapters allow for connection to standard-A plugs, as used on fixed or standard devices. An OTG product must have a single micro-AB receptacle and no other USB receptacles.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;I don't understand why phone connectors are micro-USB type B and not micro-USB type AB : someone know why ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Maybe because they don't support, and don't want to support OTG. If you want a keyboard or external audio, use Bluetooth.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;With OTG the "magic happens" because of the cable:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P style="padding-left: 30px;"&gt;An OTG cable has a micro-A plug on one end, and a micro-B plug on the other end.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Tom&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 20 Apr 2018 07:40:49 GMT</pubDate>
    <dc:creator>TomE</dc:creator>
    <dc:date>2018-04-20T07:40:49Z</dc:date>
    <item>
      <title>USB receptable type</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/USB-receptable-type/m-p/748743#M13372</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;BR /&gt;&amp;nbsp;&lt;BR /&gt;When you connect 2 OTG systems with a micro-USB cable, host must be micro-USB type AB and device must be micro-USB type B, isn't it ?&lt;BR /&gt;I don't understand why phone connectors are micro-USB type B and not micro-USB type AB : someone know why ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;A phone can be connected to a PC : it would be normal that phone connector is micro-USB type B because VBUS is powered by PC.&lt;BR /&gt;... But a phone can be connected to a phone : it is why, it would be more logic that phone connector is micro-USB type AB.&lt;BR /&gt;Problem is when I check a phone, I see micro-USB connector is type B and not type AB. With micro-USB type B connector, you can't use micro-USB type A cable and with micro-USB type AB connector, you can use all micro-USB cable type : why phone manufacturers doesn't use micro-USB type AB connector to be compatible with all cable type ? I think there is a reason, isn't it ?&lt;BR /&gt;&amp;nbsp;&lt;BR /&gt;I must develop a USB OTG product (not a phone) and I would to know if I must use micro-USB type AB or type B.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 19 Apr 2018 12:31:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/USB-receptable-type/m-p/748743#M13372</guid>
      <dc:creator>cédricmarmonier</dc:creator>
      <dc:date>2018-04-19T12:31:17Z</dc:date>
    </item>
    <item>
      <title>Re: USB receptable type</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/USB-receptable-type/m-p/748744#M13373</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&amp;gt; When you connect 2 OTG systems with a micro-USB cable, host must be micro-USB type AB&lt;/P&gt;&lt;P&gt;&amp;gt; and device must be micro-USB type B, isn't it ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Not according to Wikipedia:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="https://en.wikipedia.org/wiki/USB_On-The-Go#OTG_micro_plugs"&gt;https://en.wikipedia.org/wiki/USB_On-The-Go#OTG_micro_plugs&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P style="padding-left: 30px;"&gt;Micro-A adapters allow for connection to standard-A plugs, as used on fixed or standard devices. An OTG product must have a single micro-AB receptacle and no other USB receptacles.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;I don't understand why phone connectors are micro-USB type B and not micro-USB type AB : someone know why ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Maybe because they don't support, and don't want to support OTG. If you want a keyboard or external audio, use Bluetooth.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;With OTG the "magic happens" because of the cable:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P style="padding-left: 30px;"&gt;An OTG cable has a micro-A plug on one end, and a micro-B plug on the other end.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Tom&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 20 Apr 2018 07:40:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/USB-receptable-type/m-p/748744#M13373</guid>
      <dc:creator>TomE</dc:creator>
      <dc:date>2018-04-20T07:40:49Z</dc:date>
    </item>
    <item>
      <title>Re: USB receptable type</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/USB-receptable-type/m-p/748745#M13374</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;BLOCKQUOTE class="jive_macro_quote jive-quote jive_text_macro"&gt;&lt;P&gt;Not according to Wikipedia:..&lt;/P&gt;&lt;/BLOCKQUOTE&gt;&lt;P&gt;Wikepedia isn't a trusted source of information but I checked Wikipedia information in USB standard. It write in USB official documentation :&lt;/P&gt;&lt;BLOCKQUOTE class="jive_macro_quote jive-quote jive_text_macro"&gt;&lt;P&gt;An OTG device is required to have one, and only one USB connector: a Micro-AB receptacle as defined in [Micro-USB1.01].&lt;/P&gt;&lt;/BLOCKQUOTE&gt;&lt;BLOCKQUOTE class="jive_macro_quote jive-quote jive_text_macro"&gt;&lt;P&gt;The Micro-AB receptacle is only allowed on OTG products. All other uses of the Micro-AB receptacle are&lt;BR /&gt;prohibited. The Micro-AB receptacle accepts either a Micro-A plug or a Micro-B plug.&lt;/P&gt;&lt;/BLOCKQUOTE&gt;&lt;P&gt;=&amp;gt; OTG product must use Micro-AB receptable and no-OTG product must use Micro-B receptable. A product with micro-USB receptable which can supply VBUS must be mandatorily OTG (It must be micro-AB).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;BLOCKQUOTE class="jive_macro_quote jive-quote jive_text_macro"&gt;&lt;P&gt;Maybe because they don't support, and don't want to support OTG. If you want a keyboard or external audio, use Bluetooth.&lt;/P&gt;&lt;/BLOCKQUOTE&gt;&lt;P&gt;Recent phones can supplies VBUS (ie : you can use USB key =&amp;gt; they are OTG). USB standard is defined by a group composed of main manufacturers (&lt;A class="link-titled" href="http://www.usb.org/about" title="http://www.usb.org/about"&gt;USB.org - About USB-IF&lt;/A&gt;), it is shocking that phones which are manufactured by them aren't in confirmity with USB standard : perhaps, there is an amendment for battery powered devices which permitted micro-B receptacle for OTG products (but I don't find this information in USB standard).&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 20 Apr 2018 15:05:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/USB-receptable-type/m-p/748745#M13374</guid>
      <dc:creator>cédricmarmonier</dc:creator>
      <dc:date>2018-04-20T15:05:56Z</dc:date>
    </item>
  </channel>
</rss>