<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>ColdFire/68K Microcontrollers and ProcessorsのトピックUSB Bootloader for MCF51JM128</title>
    <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/USB-Bootloader-for-MCF51JM128/m-p/674700#M13229</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;BR /&gt;Long ago I developed an application with the ColdFire MCF51JM128 and the USB Bootloader (AN3748) on Code Warrior 6.1.&lt;BR /&gt;Now to update my application I used Code Warrior 10.4 always with the same bootloader.&lt;BR /&gt;The problem is that if I upgrade by connecting the PC usb to a card with the old firmware, upgrade is ok, but the ColdFire starts and goes reset, and so on.&lt;BR /&gt;If instead I program the MCU with the new FW through the Cyclone Pro and then I try to upgrade via PC, the MCU will run correctly.&lt;/P&gt;&lt;P&gt;You can help me ?&lt;/P&gt;&lt;P&gt;Thank you&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 27 Jun 2017 16:11:14 GMT</pubDate>
    <dc:creator>francescofalcin</dc:creator>
    <dc:date>2017-06-27T16:11:14Z</dc:date>
    <item>
      <title>USB Bootloader for MCF51JM128</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/USB-Bootloader-for-MCF51JM128/m-p/674700#M13229</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;BR /&gt;Long ago I developed an application with the ColdFire MCF51JM128 and the USB Bootloader (AN3748) on Code Warrior 6.1.&lt;BR /&gt;Now to update my application I used Code Warrior 10.4 always with the same bootloader.&lt;BR /&gt;The problem is that if I upgrade by connecting the PC usb to a card with the old firmware, upgrade is ok, but the ColdFire starts and goes reset, and so on.&lt;BR /&gt;If instead I program the MCU with the new FW through the Cyclone Pro and then I try to upgrade via PC, the MCU will run correctly.&lt;/P&gt;&lt;P&gt;You can help me ?&lt;/P&gt;&lt;P&gt;Thank you&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 27 Jun 2017 16:11:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/USB-Bootloader-for-MCF51JM128/m-p/674700#M13229</guid>
      <dc:creator>francescofalcin</dc:creator>
      <dc:date>2017-06-27T16:11:14Z</dc:date>
    </item>
    <item>
      <title>Re: USB Bootloader for MCF51JM128</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/USB-Bootloader-for-MCF51JM128/m-p/674701#M13230</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;Sorry I am not quite understand what your meaning. What OS are you using for CW and have you update the GUI for the bootloader?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 28 Sep 2017 18:02:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/USB-Bootloader-for-MCF51JM128/m-p/674701#M13230</guid>
      <dc:creator>miduo</dc:creator>
      <dc:date>2017-09-28T18:02:44Z</dc:date>
    </item>
  </channel>
</rss>