<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>ColdFire/68K Microcontrollers and ProcessorsのトピックRe: 5208 SDR SDRAM MOVEM.L Instruction Whacks Stack, otherwise SDRAM works</title>
    <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/5208-SDR-SDRAM-MOVEM-L-Instruction-Whacks-Stack-otherwise-SDRAM/m-p/133753#M1303</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;&lt;/DIV&gt;&lt;P&gt;It looks like your initialization sequence isn't quite right. In particular, for a 32-bit wide memory you should be using a burst length of 4 instead of 8.&lt;/P&gt;&lt;P&gt;Here is the init sequence we are using for one of our 532x boards that has 32-bit wide SDR on it:&lt;/P&gt;&lt;P&gt;writemem.l 0xFC0B8110&amp;nbsp;0x40000018&amp;nbsp; ; SDCS0&lt;/P&gt;&lt;P&gt;writemem.l 0xFC0B8008&amp;nbsp;0x42222600&amp;nbsp; ; SDCFG1&lt;BR /&gt;writemem.l 0xFC0B800C&amp;nbsp;0x54730000&amp;nbsp; ; SDCFG2&lt;/P&gt;&lt;P&gt;; Issue PALL&lt;BR /&gt;writemem.l 0xFC0B8004&amp;nbsp;0xC0130002&amp;nbsp; ; SDCR&lt;/P&gt;&lt;P&gt;; Perform two refresh cycles&lt;BR /&gt;writemem.l 0xFC0B8004&amp;nbsp;0xC0130004&amp;nbsp; ; SDCR&lt;BR /&gt;writemem.l 0xFC0B8004&amp;nbsp;0xC0130004&amp;nbsp; ; SDCR&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;; Write mode register&lt;BR /&gt;writemem.l 0xFC0B8000&amp;nbsp;0x00890000&amp;nbsp; ; SDMR&lt;/P&gt;&lt;P&gt;; Lock SDMR&lt;BR /&gt;writemem.l 0xFC0B8004&amp;nbsp;0x40130000&amp;nbsp; ; SDCR&lt;/P&gt;&lt;P&gt;; Enable refresh&lt;BR /&gt;writemem.l 0xFC0B8004&amp;nbsp;0x50130000&amp;nbsp; ; SDCR&lt;/P&gt;&lt;P&gt;; Wait a bit&lt;BR /&gt;delay 100&lt;BR /&gt;&lt;/P&gt;&lt;P&gt;It's a different product, but it uses the same SDRAMC as the 5208. So you should be able to follow this init sequence. You'll need to modify the mux value for the SDRAM you are using and you might need a few tweaks to the timing values as well, but I think this should be a good starting point for you.&lt;/P&gt;&lt;P&gt;Hope this helps,&lt;/P&gt;&lt;P&gt;Melissa&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 04 May 2006 02:19:59 GMT</pubDate>
    <dc:creator>melissa_hunter</dc:creator>
    <dc:date>2006-05-04T02:19:59Z</dc:date>
    <item>
      <title>5208 SDR SDRAM MOVEM.L Instruction Whacks Stack, otherwise SDRAM works</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/5208-SDR-SDRAM-MOVEM-L-Instruction-Whacks-Stack-otherwise-SDRAM/m-p/133752#M1302</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;I have my 'A71' board which has 5208 cpu, SDRAM, Flash, etc.&lt;BR /&gt;I have 5208 eval pcb, and all works fine there.&lt;BR /&gt;I reconfigured the SDRAm for my pcb, and have a problem&lt;/DIV&gt;&lt;DIV&gt;I have two 'A71' boards, and problem is identical on both.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;movem issues...&lt;/DIV&gt;&lt;DIV&gt;using 32-bit bus SDR SDRAM on 5208&amp;nbsp;&lt;BR /&gt;DRAM is :&amp;nbsp; MT48LC16M16A2TG-7E&amp;nbsp; ( using two parts to get 32-bits wide)&lt;/DIV&gt;&lt;DIV&gt;I have tried various settings for the SDRAM config, no changes by any setting change.&lt;/DIV&gt;&lt;DIV&gt;The memory works to run from (running routines from SDRAM), the stack in SDRAM works,&lt;BR /&gt;however, the movem instruction does incorrect things which results in whacking the&lt;BR /&gt;stack and crashing things...&lt;/DIV&gt;&lt;DIV&gt;The incorrect things which are done are very repeatable, so makes me think it is&lt;BR /&gt;a config thing.&amp;nbsp; I wrote a function which I call while walking through single step&lt;BR /&gt;in the debugger to see what it does exactly.&amp;nbsp; I have a pattern in this memory before&lt;BR /&gt;I do this, so I can see if anything is touched by the instruction.&lt;/DIV&gt;&lt;DIV&gt;- - - - - - -&amp;nbsp; - - - - -&lt;/DIV&gt;&lt;DIV&gt;First, to see what is going where, I set the registers to:&lt;/DIV&gt;&lt;DIV&gt;D3&amp;nbsp;D3D3D3D3&lt;BR /&gt;D4&amp;nbsp;D4D4D4D4&lt;BR /&gt;D5&amp;nbsp;D5D5D5D5&amp;nbsp;&lt;BR /&gt;D6&amp;nbsp;D6D6D6D6&lt;BR /&gt;D7&amp;nbsp;D7D7D7D7&lt;BR /&gt;A3&amp;nbsp;A3A3A3A3&lt;BR /&gt;A4&amp;nbsp;A4A4A4A4&lt;BR /&gt;A5&amp;nbsp;A5A5A5A5&lt;BR /&gt;A6&amp;nbsp;A6A6A6A6&lt;/DIV&gt;&lt;DIV&gt;and do:&lt;/DIV&gt;&lt;DIV&gt;movem.l&amp;nbsp; d3-d7/a3-a6,64(a7)&amp;nbsp;&lt;BR /&gt;&amp;nbsp;&amp;nbsp;(this was in the dBug printf compilation, which&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;was what was crashing )&lt;/DIV&gt;&lt;DIV&gt;&lt;BR /&gt;when stack ptr at 4001ff1C&lt;BR /&gt;results are:&lt;/DIV&gt;&lt;DIV&gt;1ff50&amp;nbsp;&amp;nbsp;UNCHANGED&amp;nbsp;UNCHANGED&amp;nbsp;UNCHANGED&amp;nbsp;D3D3D3D3&lt;BR /&gt;1FF60&amp;nbsp;&amp;nbsp;A6A6A6A6&amp;nbsp;000000000&amp;nbsp;A6A6A6A6&amp;nbsp;00000000&lt;BR /&gt;1FF70&amp;nbsp;&amp;nbsp;A3A3A3A3&amp;nbsp;A4A4A4A4&amp;nbsp;A5A5A5A5&amp;nbsp;A6A6A6A6&lt;/DIV&gt;&lt;DIV&gt;when should be:&lt;/DIV&gt;&lt;DIV&gt;1ff50&amp;nbsp;&amp;nbsp;UNCHANGED&amp;nbsp;UNCHANGED&amp;nbsp;UNCHANGED&amp;nbsp;D3D3D3D3&lt;BR /&gt;1FF60&amp;nbsp;&amp;nbsp;D4D4D4D4&amp;nbsp;D5D5D5D5&amp;nbsp;D6D6D6D6&amp;nbsp;D7D7D7D7&lt;BR /&gt;1FF70&amp;nbsp;&amp;nbsp;A3A3A3A3&amp;nbsp;A4A4A4A4&amp;nbsp;A5A5A5A5&amp;nbsp;A6A6A6A6&lt;/DIV&gt;&lt;DIV&gt;------------------------------------------------------------------------&lt;/DIV&gt;&lt;DIV&gt;when stack ptr at 40001ff20&lt;BR /&gt;registers same values,&lt;/DIV&gt;&lt;DIV&gt;results are:&lt;/DIV&gt;&lt;DIV&gt;1ff60&amp;nbsp;&amp;nbsp;D3D3D3D3&amp;nbsp;A6A6A6A6&amp;nbsp;00000000&amp;nbsp;A6A6A6A6&lt;BR /&gt;1FF70&amp;nbsp;&amp;nbsp;00000000&amp;nbsp;D7D7D7D7&amp;nbsp;A3A3A3A3&amp;nbsp;A4A4A4A4&lt;BR /&gt;1FF80&amp;nbsp;&amp;nbsp;A5A5A5A5&amp;nbsp;A6A6A6A6&amp;nbsp;UNCHANGED&amp;nbsp;UNCHANGED&amp;nbsp;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;when should be:&lt;/DIV&gt;&lt;DIV&gt;1ff60&amp;nbsp;&amp;nbsp;D3D3D3D3&amp;nbsp;D4D4D4D4&amp;nbsp;D5D5D5D5&amp;nbsp;D6D6D6D6&lt;BR /&gt;1FF70&amp;nbsp;&amp;nbsp;D7D7D7D7&amp;nbsp;A3A3A3A3&amp;nbsp;A4A4A4A4&amp;nbsp;A5A5A5A5&amp;nbsp;&lt;BR /&gt;1FF80&amp;nbsp;&amp;nbsp;A6A6A6A6&amp;nbsp;UNCHANGED&amp;nbsp;UNCHANGED&amp;nbsp;UNCHANGED&lt;/DIV&gt;&lt;DIV&gt;-------------------------------------------------------------------------&lt;/DIV&gt;&lt;DIV&gt;When stack ptr at 40001ff24&lt;BR /&gt;registers same values,&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;1ff60&amp;nbsp;&amp;nbsp;UNCHANGED&amp;nbsp;A5A5A5A5&amp;nbsp;00000000&amp;nbsp;A5A5A5A5&lt;BR /&gt;1FF70&amp;nbsp;&amp;nbsp;00000000&amp;nbsp;D6D6D6D6&amp;nbsp;D7D7D7D7&amp;nbsp;A3A3A3A3&lt;BR /&gt;1FF80&amp;nbsp;&amp;nbsp;A4A4A4A4&amp;nbsp;00000000&amp;nbsp;00000000&amp;nbsp;UNCHANGED&lt;/DIV&gt;&lt;DIV&gt;when should be:&lt;/DIV&gt;&lt;DIV&gt;&lt;BR /&gt;1ff60&amp;nbsp;&amp;nbsp;UNCHANGED&amp;nbsp;D3D3D3D3&amp;nbsp;D4D4D4D4&amp;nbsp;D5D5D5D5&lt;BR /&gt;1FF70&amp;nbsp;&amp;nbsp;D6D6D6D6&amp;nbsp;D7D7D7D7&amp;nbsp;A3A3A3A3&amp;nbsp;A4A4A4A4&lt;BR /&gt;1FF80&amp;nbsp;&amp;nbsp;A5A5A5A5&amp;nbsp;A6A6A6A6&amp;nbsp;UNCHANGED&amp;nbsp;UNCHANGED&lt;/DIV&gt;&lt;DIV&gt;-------------------------------------------------------------------------&lt;/DIV&gt;&lt;DIV&gt;When stack ptr at 40001ff28&lt;BR /&gt;registers same values,&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;1ff60&amp;nbsp;&amp;nbsp;UNCHANGED&amp;nbsp;A4A4A4A4&amp;nbsp;00000000&amp;nbsp;A4A4A4A4&lt;BR /&gt;1FF70&amp;nbsp;&amp;nbsp;00000000&amp;nbsp;D5D5D5D5&amp;nbsp;D6D6D6D6&amp;nbsp;D7D7D7D7&lt;BR /&gt;1FF80&amp;nbsp;&amp;nbsp;A3A3A3A3&amp;nbsp;00000000&amp;nbsp;00000000&amp;nbsp;A6A6A6A6&lt;/DIV&gt;&lt;DIV&gt;when should be:&lt;/DIV&gt;&lt;DIV&gt;&lt;BR /&gt;1ff60&amp;nbsp;&amp;nbsp;UNCHANGED&amp;nbsp;UNCHANGED&amp;nbsp;D3D3D3D3&amp;nbsp;D4D4D4D4&amp;nbsp;&lt;BR /&gt;1FF70&amp;nbsp;&amp;nbsp;D5D5D5D5&amp;nbsp;D6D6D6D6&amp;nbsp;D7D7D7D7&amp;nbsp;A3A3A3A3&lt;BR /&gt;1FF80&amp;nbsp;&amp;nbsp;A4A4A4A4&amp;nbsp;A5A5A5A5&amp;nbsp;A6A6A6A6&amp;nbsp;UNCHANGED&lt;/DIV&gt;&lt;DIV&gt;--------------------------------------------------------------------------&lt;/DIV&gt;&lt;DIV&gt;&lt;BR /&gt;My SDRAM config, in dBug in sysinit.c&lt;BR /&gt;values based on recommendations from Freescale by email.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;delay before calling a bit.&lt;/DIV&gt;&lt;DIV&gt;&lt;BR /&gt;0xFC0A8110 =0x40000019;&amp;nbsp;at 0x40000000 size is 64 Megs&lt;BR /&gt;0xFC0A8114 =0x44000019; at 0x44000000 size is 64 Megs&lt;BR /&gt;0xFC0A8008 =0x52211500;&lt;BR /&gt;&amp;nbsp;&lt;BR /&gt;0xFC0A800C =0x98F70000;&lt;BR /&gt;0xFC0A8004 =0xC1080002;&lt;BR /&gt;0xFC0A8000 =0x008D0000;&lt;BR /&gt;0xFC0A8004 =0xC1080002;&lt;/DIV&gt;&lt;DIV&gt;delay a bit here&lt;BR /&gt;&amp;nbsp;&lt;BR /&gt;0xFC0A8004 =0xC1080004;&amp;nbsp;do a refresh 8x&lt;BR /&gt;0xFC0A8004 =0xC1080004;&lt;BR /&gt;0xFC0A8004 =0xC1080004;&lt;BR /&gt;0xFC0A8004 =0xC1080004;&lt;BR /&gt;0xFC0A8004 =0xC1080004;&lt;BR /&gt;0xFC0A8004 =0xC1080004;&lt;BR /&gt;0xFC0A8004 =0xC1080004;&lt;BR /&gt;0xFC0A8004 =0xC1080004;&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;BR /&gt;delay a bit here&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;0xFC0A8000 =0x008D0000;&lt;BR /&gt;0xFC0A8004 =0xC1080000;&lt;BR /&gt;0xFC0A8004 =0x51080000;&lt;BR /&gt;&amp;nbsp;&lt;BR /&gt;delay a bit here&lt;/DIV&gt;&lt;DIV&gt;SDRAM now ready to go.&lt;/DIV&gt;&lt;DIV&gt;I then run a memory test by putting a pattern in and reading it out (which gives me&lt;BR /&gt;my background pattern for the test above, (the memory test always passes).&lt;/DIV&gt;&lt;DIV&gt;I have tried slowing things down by changing values in the setup above, but no changes&lt;BR /&gt;in the results.&lt;/DIV&gt;&lt;DIV&gt;----------------------&lt;/DIV&gt;&lt;DIV&gt;SDRAM is connected as follows:&lt;BR /&gt;(r33 is 33 ohm resistor pack very small)&lt;/DIV&gt;&lt;DIV&gt;&lt;BR /&gt;CPU&amp;nbsp;&amp;nbsp; &amp;nbsp;&amp;nbsp;&amp;nbsp;SDRAM&lt;/DIV&gt;&lt;DIV&gt;A0&amp;nbsp;&amp;nbsp;R33&amp;nbsp;A0&lt;BR /&gt;A1&amp;nbsp;&amp;nbsp;R33&amp;nbsp;A1&lt;BR /&gt;A2&amp;nbsp;&amp;nbsp;R33&amp;nbsp;A2&lt;BR /&gt;A3&amp;nbsp;&amp;nbsp;R33&amp;nbsp;A3&lt;BR /&gt;A4&amp;nbsp;&amp;nbsp;R33&amp;nbsp;A4&lt;BR /&gt;A5&amp;nbsp;&amp;nbsp;R33&amp;nbsp;A5&lt;BR /&gt;A6&amp;nbsp;&amp;nbsp;R33&amp;nbsp;A6&lt;BR /&gt;A7&amp;nbsp;&amp;nbsp;R33&amp;nbsp;A7&lt;BR /&gt;A8&amp;nbsp;&amp;nbsp;R33&amp;nbsp;A8&lt;BR /&gt;A9&amp;nbsp;&amp;nbsp;R33&amp;nbsp;A9&lt;BR /&gt;SD_A10&amp;nbsp;&amp;nbsp;R33&amp;nbsp;A10&lt;BR /&gt;A11&amp;nbsp;&amp;nbsp;R33&amp;nbsp;A11&lt;BR /&gt;A12&amp;nbsp;&amp;nbsp;R33&amp;nbsp;A12&lt;/DIV&gt;&lt;DIV&gt;A14&amp;nbsp;&amp;nbsp;R33&amp;nbsp;BA0&lt;BR /&gt;A15&amp;nbsp;&amp;nbsp;R33&amp;nbsp;BA1&lt;/DIV&gt;&lt;DIV&gt;SD_CKE&amp;nbsp;&amp;nbsp;R33&amp;nbsp;CKE&lt;BR /&gt;SD_CLK&amp;nbsp;&amp;nbsp;R33&amp;nbsp;CLK&lt;BR /&gt;SD_CS0&amp;nbsp;&amp;nbsp;R33&amp;nbsp;CS&lt;BR /&gt;SD_WE&amp;nbsp;&amp;nbsp;R33&amp;nbsp;WE&lt;BR /&gt;SD_CAS&amp;nbsp;&amp;nbsp;R33&amp;nbsp;CAS&lt;BR /&gt;SD_RAS&amp;nbsp;&amp;nbsp;R33&amp;nbsp;RAS&lt;/DIV&gt;&lt;DIV&gt;one SDRAM has&lt;BR /&gt;D16-D31 &amp;nbsp;R33&amp;nbsp;DQ0-DQ15&lt;BR /&gt;SD_DQMN_3&amp;nbsp;R33&amp;nbsp;DQMH&lt;BR /&gt;SD_DQMN_2&amp;nbsp;R33&amp;nbsp;DQML&lt;/DIV&gt;&lt;DIV&gt;and the other has&lt;BR /&gt;D0-D15&amp;nbsp;&amp;nbsp;R33&amp;nbsp;DQ0-DQ15&lt;BR /&gt;SD_DQMN_1&amp;nbsp;R33&amp;nbsp;DQMH&lt;BR /&gt;SD_DQMN_0&amp;nbsp;R33&amp;nbsp;DQML&lt;/DIV&gt;&lt;DIV&gt;then,&lt;BR /&gt;SD_DR_DQS&amp;nbsp;loop to memory and back to SD_DQS2 and SD_DQS3&lt;BR /&gt;------------------------------------------------------------------------------------------&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;&lt;BR /&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;&lt;BR /&gt;&amp;nbsp;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 27 Apr 2006 03:37:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/5208-SDR-SDRAM-MOVEM-L-Instruction-Whacks-Stack-otherwise-SDRAM/m-p/133752#M1302</guid>
      <dc:creator>prenton</dc:creator>
      <dc:date>2006-04-27T03:37:53Z</dc:date>
    </item>
    <item>
      <title>Re: 5208 SDR SDRAM MOVEM.L Instruction Whacks Stack, otherwise SDRAM works</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/5208-SDR-SDRAM-MOVEM-L-Instruction-Whacks-Stack-otherwise-SDRAM/m-p/133753#M1303</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;&lt;/DIV&gt;&lt;P&gt;It looks like your initialization sequence isn't quite right. In particular, for a 32-bit wide memory you should be using a burst length of 4 instead of 8.&lt;/P&gt;&lt;P&gt;Here is the init sequence we are using for one of our 532x boards that has 32-bit wide SDR on it:&lt;/P&gt;&lt;P&gt;writemem.l 0xFC0B8110&amp;nbsp;0x40000018&amp;nbsp; ; SDCS0&lt;/P&gt;&lt;P&gt;writemem.l 0xFC0B8008&amp;nbsp;0x42222600&amp;nbsp; ; SDCFG1&lt;BR /&gt;writemem.l 0xFC0B800C&amp;nbsp;0x54730000&amp;nbsp; ; SDCFG2&lt;/P&gt;&lt;P&gt;; Issue PALL&lt;BR /&gt;writemem.l 0xFC0B8004&amp;nbsp;0xC0130002&amp;nbsp; ; SDCR&lt;/P&gt;&lt;P&gt;; Perform two refresh cycles&lt;BR /&gt;writemem.l 0xFC0B8004&amp;nbsp;0xC0130004&amp;nbsp; ; SDCR&lt;BR /&gt;writemem.l 0xFC0B8004&amp;nbsp;0xC0130004&amp;nbsp; ; SDCR&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;; Write mode register&lt;BR /&gt;writemem.l 0xFC0B8000&amp;nbsp;0x00890000&amp;nbsp; ; SDMR&lt;/P&gt;&lt;P&gt;; Lock SDMR&lt;BR /&gt;writemem.l 0xFC0B8004&amp;nbsp;0x40130000&amp;nbsp; ; SDCR&lt;/P&gt;&lt;P&gt;; Enable refresh&lt;BR /&gt;writemem.l 0xFC0B8004&amp;nbsp;0x50130000&amp;nbsp; ; SDCR&lt;/P&gt;&lt;P&gt;; Wait a bit&lt;BR /&gt;delay 100&lt;BR /&gt;&lt;/P&gt;&lt;P&gt;It's a different product, but it uses the same SDRAMC as the 5208. So you should be able to follow this init sequence. You'll need to modify the mux value for the SDRAM you are using and you might need a few tweaks to the timing values as well, but I think this should be a good starting point for you.&lt;/P&gt;&lt;P&gt;Hope this helps,&lt;/P&gt;&lt;P&gt;Melissa&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 04 May 2006 02:19:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/5208-SDR-SDRAM-MOVEM-L-Instruction-Whacks-Stack-otherwise-SDRAM/m-p/133753#M1303</guid>
      <dc:creator>melissa_hunter</dc:creator>
      <dc:date>2006-05-04T02:19:59Z</dc:date>
    </item>
    <item>
      <title>Re: 5208 SDR SDRAM MOVEM.L Instruction Whacks Stack, otherwise SDRAM works</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/5208-SDR-SDRAM-MOVEM-L-Instruction-Whacks-Stack-otherwise-SDRAM/m-p/133754#M1304</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;&lt;/DIV&gt;&lt;P&gt;yes, I changed it yesterday to 4 and it worked...&lt;/P&gt;&lt;P&gt;Paul&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 04 May 2006 02:24:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/5208-SDR-SDRAM-MOVEM-L-Instruction-Whacks-Stack-otherwise-SDRAM/m-p/133754#M1304</guid>
      <dc:creator>prenton</dc:creator>
      <dc:date>2006-05-04T02:24:48Z</dc:date>
    </item>
    <item>
      <title>Re: 5208 SDR SDRAM MOVEM.L Instruction Whacks Stack, otherwise SDRAM works</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/5208-SDR-SDRAM-MOVEM-L-Instruction-Whacks-Stack-otherwise-SDRAM/m-p/133755#M1305</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;In the last command as as the dqs signals are externally shorted and routed to a DQS as it is shown in the AN2982.pdf for 32 bit SDR-SDRAM, the las should be:&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;; ENABLE SDMR&lt;BR /&gt;writemem.l 0xFC0A8004&amp;nbsp;0x50144000&amp;nbsp; ; SDCR&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;am I correct?&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 16 Jun 2008 23:05:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/5208-SDR-SDRAM-MOVEM-L-Instruction-Whacks-Stack-otherwise-SDRAM/m-p/133755#M1305</guid>
      <dc:creator>adam07</dc:creator>
      <dc:date>2008-06-16T23:05:39Z</dc:date>
    </item>
  </channel>
</rss>