<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>ColdFire/68K Microcontrollers and ProcessorsのトピックRe: MCF5271 uart2 on QFP160</title>
    <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/MCF5271-uart2-on-QFP160/m-p/133730#M1300</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;I think I see the problem.&lt;BR /&gt;&lt;BR /&gt;By setting the pin multiplexing, you can choose which physical pins are used for the UART 2 TX and RX functions. In each case there are two choices, but in your example code you have set things up so that *both* choices of pin are used. For example, for RX you have selected:&lt;BR /&gt;&lt;BR /&gt;(a) PORT_FECI2C: FEC_EMDIO / I2C_SDA / U2RXD / PFECI2C[2]&lt;BR /&gt;&lt;BR /&gt;AND&lt;BR /&gt;&lt;BR /&gt;(b)PORT_UARTH: U2RXD / PUARTH[0]&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;These are physically distinct pins. You need to check which one your serial cable connects to, and only configure the UART2 function on that one.&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;Hope that helps&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;Simon&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 20 Oct 2006 15:44:05 GMT</pubDate>
    <dc:creator>SimonMarsden_de</dc:creator>
    <dc:date>2006-10-20T15:44:05Z</dc:date>
    <item>
      <title>MCF5271 uart2 on QFP160</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/MCF5271-uart2-on-QFP160/m-p/133729#M1299</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;I have probleme to use UART2 with the alternative pins EMDIO &amp;amp; EMDC.&lt;/DIV&gt;&lt;DIV&gt;Tx : ok&lt;/DIV&gt;&lt;DIV&gt;Rx : nothing.&lt;/DIV&gt;&lt;DIV&gt;I think that my driver is ok because it is ok is I use the Loop Back Mode.&lt;/DIV&gt;&lt;DIV&gt;It seems that I don't corrrectly connect the pysical pin EMDIO to the receive UART block.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;My initialisation :&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;MCF_GPIO_PDDR_FECI2C = 0;&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;MCF_GPIO_PAR_FECI2C = MCF_GPIO_PAR_FECI2C_PAR_EMDC_UART2 |&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;MCF_GPIO_PAR_FECI2C_PAR_EMDIO_UART2&amp;nbsp; ;&amp;nbsp;&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;MCF_GPIO_PODR_FECI2C = 0 ;&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;MCF_GPIO_PAR_UART = MCF_GPIO_PAR_UART_PAR_U2RXD&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; |&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;MCF_GPIO_PAR_UART_PAR_U2TXD&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; |&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;MCF_GPIO_PAR_UART_PAR_U1RXD(0x3) |&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;MCF_GPIO_PAR_UART_PAR_U1TXD(0x3) |&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;MCF_GPIO_PAR_UART_PAR_U0RXD&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; |&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;MCF_GPIO_PAR_UART_PAR_U0TXD&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; |&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;MCF_GPIO_PAR_UART_PAR_U0RTS;&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;MCF_GPIO_PDDR_UARTH = 0;&lt;BR /&gt;&lt;/DIV&gt;&lt;DIV&gt;Thanks for your help!&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 20 Oct 2006 15:29:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/MCF5271-uart2-on-QFP160/m-p/133729#M1299</guid>
      <dc:creator>TimeMan</dc:creator>
      <dc:date>2006-10-20T15:29:53Z</dc:date>
    </item>
    <item>
      <title>Re: MCF5271 uart2 on QFP160</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/MCF5271-uart2-on-QFP160/m-p/133730#M1300</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;I think I see the problem.&lt;BR /&gt;&lt;BR /&gt;By setting the pin multiplexing, you can choose which physical pins are used for the UART 2 TX and RX functions. In each case there are two choices, but in your example code you have set things up so that *both* choices of pin are used. For example, for RX you have selected:&lt;BR /&gt;&lt;BR /&gt;(a) PORT_FECI2C: FEC_EMDIO / I2C_SDA / U2RXD / PFECI2C[2]&lt;BR /&gt;&lt;BR /&gt;AND&lt;BR /&gt;&lt;BR /&gt;(b)PORT_UARTH: U2RXD / PUARTH[0]&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;These are physically distinct pins. You need to check which one your serial cable connects to, and only configure the UART2 function on that one.&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;Hope that helps&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;Simon&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 20 Oct 2006 15:44:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/MCF5271-uart2-on-QFP160/m-p/133730#M1300</guid>
      <dc:creator>SimonMarsden_de</dc:creator>
      <dc:date>2006-10-20T15:44:05Z</dc:date>
    </item>
    <item>
      <title>Re: MCF5271 uart2 on QFP160</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/MCF5271-uart2-on-QFP160/m-p/133731#M1301</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;That's run !&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;Thanks a lot.&lt;/DIV&gt;&lt;DIV&gt;&lt;IMG alt=":smileyvery-happy:" class="emoticon emoticon-smileyvery-happy" id="smileyvery-happy" src="http://freescale.i.lithium.com/i/smilies/16x16_smiley-very-happy.gif" title="Smiley Very Happy" /&gt;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 20 Oct 2006 16:18:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/MCF5271-uart2-on-QFP160/m-p/133731#M1301</guid>
      <dc:creator>TimeMan</dc:creator>
      <dc:date>2006-10-20T16:18:27Z</dc:date>
    </item>
  </channel>
</rss>