<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>ColdFire/68K Microcontrollers and ProcessorsのトピックProper EOI sequence for 5213 IRQs</title>
    <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/Proper-EOI-sequence-for-5213-IRQs/m-p/606522#M12975</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I've inherited an old project and adding ISR routines to IRQ1-IRQ7 pins of the 5213.&amp;nbsp; Pretty sure I have the EPORT configured properly since I do enter the ISR but can only enter once. I'm running on an old freescale Evaluation board. (the one with 3 pushbuttons connected to IRQ1, IRQ2 and IRQ3).&amp;nbsp; Old freescale app notes refer to EPORTSoftwareDemo.zip which contains source for ISR examples but that file is no longer around.&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Any help explaining the proper EOI sequence will be appreciated&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 13 Dec 2016 19:16:18 GMT</pubDate>
    <dc:creator>philroth</dc:creator>
    <dc:date>2016-12-13T19:16:18Z</dc:date>
    <item>
      <title>Proper EOI sequence for 5213 IRQs</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/Proper-EOI-sequence-for-5213-IRQs/m-p/606522#M12975</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I've inherited an old project and adding ISR routines to IRQ1-IRQ7 pins of the 5213.&amp;nbsp; Pretty sure I have the EPORT configured properly since I do enter the ISR but can only enter once. I'm running on an old freescale Evaluation board. (the one with 3 pushbuttons connected to IRQ1, IRQ2 and IRQ3).&amp;nbsp; Old freescale app notes refer to EPORTSoftwareDemo.zip which contains source for ISR examples but that file is no longer around.&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Any help explaining the proper EOI sequence will be appreciated&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 13 Dec 2016 19:16:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/Proper-EOI-sequence-for-5213-IRQs/m-p/606522#M12975</guid>
      <dc:creator>philroth</dc:creator>
      <dc:date>2016-12-13T19:16:18Z</dc:date>
    </item>
    <item>
      <title>Re: Proper EOI sequence for 5213 IRQs</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/Proper-EOI-sequence-for-5213-IRQs/m-p/606523#M12976</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I just realized there was low level code already setting up the stack frame before my function so all I needed was a void function(void) call, terminating on an RTS rather than RTE.&amp;nbsp; So I'm good to go now.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 14 Dec 2016 13:15:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/Proper-EOI-sequence-for-5213-IRQs/m-p/606523#M12976</guid>
      <dc:creator>philroth</dc:creator>
      <dc:date>2016-12-14T13:15:46Z</dc:date>
    </item>
  </channel>
</rss>