<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: MCF5213 not running in ColdFire/68K Microcontrollers and Processors</title>
    <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/MCF5213-not-running/m-p/606484#M12973</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, &lt;/P&gt;&lt;P&gt;From the schematic attached, I can not find the BDM connection. You mentioned that pulled the BKPT up to VCC, do you use the 4.7K pull-up?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 13 Mar 2017 06:17:45 GMT</pubDate>
    <dc:creator>miduo</dc:creator>
    <dc:date>2017-03-13T06:17:45Z</dc:date>
    <item>
      <title>MCF5213 not running</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/MCF5213-not-running/m-p/606482#M12971</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Having trouble starting up a MCF5213.&amp;nbsp; I know the code is good because it ran on an eval board and my design is very similar, for now only toggling a LED on a GPIO pin every 500ms using a timer interrupt. Again, code runs on the Eval board so it's the hardware. The only activity I see is the 48MHz on the PSTCLK.&amp;nbsp; Input is an 8MHz oscillator and clkmod = 1:1. Unfortunately clkmod pins are tied to VCC under the chip and can't be easily modified.&amp;nbsp; CPU can be successfully programmed via eZport and verifies so the cpu is allowing the flash to be loaded.&amp;nbsp; Any help is appreciated.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Attached is schematic&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 28 Feb 2017 22:19:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/MCF5213-not-running/m-p/606482#M12971</guid>
      <dc:creator>philroth</dc:creator>
      <dc:date>2017-02-28T22:19:19Z</dc:date>
    </item>
    <item>
      <title>Re: MCF5213 not running</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/MCF5213-not-running/m-p/606483#M12972</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I Left the BKPT# pin floating so CPU halted. Pulled up to VCC and runs like a champ &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 01 Mar 2017 03:24:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/MCF5213-not-running/m-p/606483#M12972</guid>
      <dc:creator>philroth</dc:creator>
      <dc:date>2017-03-01T03:24:41Z</dc:date>
    </item>
    <item>
      <title>Re: MCF5213 not running</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/MCF5213-not-running/m-p/606484#M12973</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, &lt;/P&gt;&lt;P&gt;From the schematic attached, I can not find the BDM connection. You mentioned that pulled the BKPT up to VCC, do you use the 4.7K pull-up?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 13 Mar 2017 06:17:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/MCF5213-not-running/m-p/606484#M12973</guid>
      <dc:creator>miduo</dc:creator>
      <dc:date>2017-03-13T06:17:45Z</dc:date>
    </item>
    <item>
      <title>Re: MCF5213 not running</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/MCF5213-not-running/m-p/606485#M12974</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Put it right to VCC to get me going but have added a 4.7k pullup to the final design.&amp;nbsp; Also had trouble getting Port DD working as GPIO but got that working also after some more reading.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 13 Mar 2017 10:36:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/MCF5213-not-running/m-p/606485#M12974</guid>
      <dc:creator>philroth</dc:creator>
      <dc:date>2017-03-13T10:36:01Z</dc:date>
    </item>
  </channel>
</rss>