<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Memory use of uTasker and SSL in ColdFire/68K Microcontrollers and Processors</title>
    <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/Memory-use-of-uTasker-and-SSL/m-p/541544#M12878</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I have a use for a TCP/IP stack which supports SSL/TLS and wondered if anyone was using the uTasker system and could give some idea of memory use - code and ram etc.&lt;/P&gt;&lt;P&gt;My target is the MCF53014.&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;If anyone has any other recommendations for tcp/ip with tls which will run either without an operating system or come with its own o/s please let me know.&lt;/P&gt;&lt;P&gt;I have limited memory on the target board, basically just the 128K of ram built into the 53014 and 1megabyte of flash so small memory use is a must!&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 19 Aug 2016 07:15:59 GMT</pubDate>
    <dc:creator>paul1962</dc:creator>
    <dc:date>2016-08-19T07:15:59Z</dc:date>
    <item>
      <title>Memory use of uTasker and SSL</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/Memory-use-of-uTasker-and-SSL/m-p/541544#M12878</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I have a use for a TCP/IP stack which supports SSL/TLS and wondered if anyone was using the uTasker system and could give some idea of memory use - code and ram etc.&lt;/P&gt;&lt;P&gt;My target is the MCF53014.&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;If anyone has any other recommendations for tcp/ip with tls which will run either without an operating system or come with its own o/s please let me know.&lt;/P&gt;&lt;P&gt;I have limited memory on the target board, basically just the 128K of ram built into the 53014 and 1megabyte of flash so small memory use is a must!&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 19 Aug 2016 07:15:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/Memory-use-of-uTasker-and-SSL/m-p/541544#M12878</guid>
      <dc:creator>paul1962</dc:creator>
      <dc:date>2016-08-19T07:15:59Z</dc:date>
    </item>
    <item>
      <title>Re: Memory use of uTasker and SSL</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/Memory-use-of-uTasker-and-SSL/m-p/541545#M12879</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Do you mind to put your question on the uTasker forum instead:&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="http://www.utasker.com/forum/" title="http://www.utasker.com/forum/"&gt;µTasker Forum - Index&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 13 Sep 2016 06:51:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/Memory-use-of-uTasker-and-SSL/m-p/541545#M12879</guid>
      <dc:creator>miduo</dc:creator>
      <dc:date>2016-09-13T06:51:13Z</dc:date>
    </item>
  </channel>
</rss>