<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>ColdFire/68K Microcontrollers and Processorsのトピック5282 timer</title>
    <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/5282-timer/m-p/133684#M1286</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;What is the maximum timeout that we can provide using GPT module in 5282.&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 26 Apr 2006 10:59:30 GMT</pubDate>
    <dc:creator>rao</dc:creator>
    <dc:date>2006-04-26T10:59:30Z</dc:date>
    <item>
      <title>5282 timer</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/5282-timer/m-p/133684#M1286</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;What is the maximum timeout that we can provide using GPT module in 5282.&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 26 Apr 2006 10:59:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/5282-timer/m-p/133684#M1286</guid>
      <dc:creator>rao</dc:creator>
      <dc:date>2006-04-26T10:59:30Z</dc:date>
    </item>
    <item>
      <title>Re: 5282 timer</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/5282-timer/m-p/133685#M1287</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;what are you trying to do? if you are looking to periodically interrupt the proc, i think it would be easier to use the PIT timers. however, if you are going to use the GPT, i believe that the maximum timeout is a little under 17 million system clocks (2^24). if you are looking on an external clock, i think it can be much longer. looking at the datasheet, though i'm not 100% sure how to use the module, you can prescale the Pulse Accumulator by up to 65536, then this can be divided by 2^16, or a total time of nearly 4.3 billion clock cycles (2^32). let me know if this helps, or if it is wrong...hehe.&lt;BR /&gt;&lt;BR /&gt;Trevor&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 26 Apr 2006 12:39:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/5282-timer/m-p/133685#M1287</guid>
      <dc:creator>airswit</dc:creator>
      <dc:date>2006-04-26T12:39:51Z</dc:date>
    </item>
  </channel>
</rss>