<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Problem with TeraTerm and scanf() in ColdFire/68K Microcontrollers and Processors</title>
    <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/Problem-with-TeraTerm-and-scanf/m-p/470399#M12689</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;K64F is Kinetis. This is the Coldfire forum.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Between your code and Teraterm you need code equivalent to a "terminal driver".&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;These can get horribly complicated, but at a basic level you expect "hello world\n" to print with a carriage return as well as the line feed. So if you changed your code to "hello world\r\n" it would look more normal. So a normal function of a Terminal Driver is to convert all "\n" on output to "\r\n".&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;It also echoes all input that you type back to the output so you can see what you're entering.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;And for bonus points it should let you EDIT your response, at a minimum allowing you to backspace over what you typed, and only forwarding the edited result to your program when you hot "return".&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The development board may come with software to do that, but you may have bypassed it to call the serial port directly. See if you can find one (and ask on the Kinetis forum). Or you could write one. Or you could write your code to explicitly (or via a function) emit "\r\n" and echo input characters.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Somehow the "scanf()" call is linked up to the serial driver somehow. just not through something standard or smart enough. There may be a project option somewhere.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Tom&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 26 Apr 2016 14:00:51 GMT</pubDate>
    <dc:creator>TomE</dc:creator>
    <dc:date>2016-04-26T14:00:51Z</dc:date>
    <item>
      <title>Problem with TeraTerm and scanf()</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/Problem-with-TeraTerm-and-scanf/m-p/470398#M12688</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I was working on FRDM K64F using KDS&lt;/P&gt;&lt;P&gt;My code is working correctly on teraterm but I cannot see the scanf values I enter. It does the calculation correctly though. Also the teraterm output is spaced. I have attached how my output looks on tera term&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 24 Apr 2016 05:17:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/Problem-with-TeraTerm-and-scanf/m-p/470398#M12688</guid>
      <dc:creator>kirantujare</dc:creator>
      <dc:date>2016-04-24T05:17:16Z</dc:date>
    </item>
    <item>
      <title>Re: Problem with TeraTerm and scanf()</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/Problem-with-TeraTerm-and-scanf/m-p/470399#M12689</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;K64F is Kinetis. This is the Coldfire forum.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Between your code and Teraterm you need code equivalent to a "terminal driver".&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;These can get horribly complicated, but at a basic level you expect "hello world\n" to print with a carriage return as well as the line feed. So if you changed your code to "hello world\r\n" it would look more normal. So a normal function of a Terminal Driver is to convert all "\n" on output to "\r\n".&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;It also echoes all input that you type back to the output so you can see what you're entering.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;And for bonus points it should let you EDIT your response, at a minimum allowing you to backspace over what you typed, and only forwarding the edited result to your program when you hot "return".&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The development board may come with software to do that, but you may have bypassed it to call the serial port directly. See if you can find one (and ask on the Kinetis forum). Or you could write one. Or you could write your code to explicitly (or via a function) emit "\r\n" and echo input characters.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Somehow the "scanf()" call is linked up to the serial driver somehow. just not through something standard or smart enough. There may be a project option somewhere.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Tom&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 26 Apr 2016 14:00:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/Problem-with-TeraTerm-and-scanf/m-p/470399#M12689</guid>
      <dc:creator>TomE</dc:creator>
      <dc:date>2016-04-26T14:00:51Z</dc:date>
    </item>
    <item>
      <title>Re: Problem with TeraTerm and scanf()</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/Problem-with-TeraTerm-and-scanf/m-p/470400#M12690</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thank you! I got it figured out. &lt;BR /&gt;To use scanf(), I had to use debug_scanf and it worked&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 27 Apr 2016 19:03:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/Problem-with-TeraTerm-and-scanf/m-p/470400#M12690</guid>
      <dc:creator>kirantujare</dc:creator>
      <dc:date>2016-04-27T19:03:58Z</dc:date>
    </item>
  </channel>
</rss>