<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>ColdFire/68K Microcontrollers and Processors中的主题 Re: Hi</title>
    <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/Hi/m-p/425231#M12583</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;STRONG&gt;Lo&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;gt; MCF52277x&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I assume you mean MCF5227x.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The MCF52277 is not a good choice if you want network connectivity. It doesn't have an internet Ethernet controller. With a better choice of CPU, all you need for WiFi is a cheap external WiFi hub. Any old obsolete ADSL WiFi box can do that.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Lots of embedded boards claiming do do this as well, like these:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="http://www.alibaba.com/showroom/ethernet-wifi-module.html" title="http://www.alibaba.com/showroom/ethernet-wifi-module.html"&gt;Ethernet Wifi Module, Ethernet Wifi Module Suppliers and Manufacturers at Alibaba.com&lt;/A&gt; &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The MCF52277 does have USB, and USB-to-WiFi adapters are less than $10. But they would only work when plugged into a Windows PC. Some of them may work on Linux. It is unlikely you could get them to work on an embedded system.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Many of the above listed boards are "Serial to WiFi". That means they might be a "WiFi Serial Modem". They may convert a serial port data stream into a Telnet connection to a preconfigured host machine.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;You haven't said what you need the WiFi connectivity for. Is the CPU to be a Server or a Client? General purpose (web and so on) or single purpose? That makes a difference to the possible solutions.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'd recommend you use a different chip, and a different family as well. You shouldn't start a project using ColdFire now - use Kinetis or an ARM-based solution instead.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Tom&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Sat, 03 Oct 2015 14:37:13 GMT</pubDate>
    <dc:creator>TomE</dc:creator>
    <dc:date>2015-10-03T14:37:13Z</dc:date>
    <item>
      <title>Hi</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/Hi/m-p/425230#M12582</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, &lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;This is ravi.&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I am looking for the Low cost Wifi module which can support on Freescale Coldfire. eg: MCF52277x. &lt;/P&gt;&lt;P&gt;Please suggest me the proper solution. &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 30 Sep 2015 15:13:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/Hi/m-p/425230#M12582</guid>
      <dc:creator>ravindranp</dc:creator>
      <dc:date>2015-09-30T15:13:51Z</dc:date>
    </item>
    <item>
      <title>Re: Hi</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/Hi/m-p/425231#M12583</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;STRONG&gt;Lo&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;gt; MCF52277x&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I assume you mean MCF5227x.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The MCF52277 is not a good choice if you want network connectivity. It doesn't have an internet Ethernet controller. With a better choice of CPU, all you need for WiFi is a cheap external WiFi hub. Any old obsolete ADSL WiFi box can do that.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Lots of embedded boards claiming do do this as well, like these:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="http://www.alibaba.com/showroom/ethernet-wifi-module.html" title="http://www.alibaba.com/showroom/ethernet-wifi-module.html"&gt;Ethernet Wifi Module, Ethernet Wifi Module Suppliers and Manufacturers at Alibaba.com&lt;/A&gt; &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The MCF52277 does have USB, and USB-to-WiFi adapters are less than $10. But they would only work when plugged into a Windows PC. Some of them may work on Linux. It is unlikely you could get them to work on an embedded system.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Many of the above listed boards are "Serial to WiFi". That means they might be a "WiFi Serial Modem". They may convert a serial port data stream into a Telnet connection to a preconfigured host machine.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;You haven't said what you need the WiFi connectivity for. Is the CPU to be a Server or a Client? General purpose (web and so on) or single purpose? That makes a difference to the possible solutions.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'd recommend you use a different chip, and a different family as well. You shouldn't start a project using ColdFire now - use Kinetis or an ARM-based solution instead.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Tom&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 03 Oct 2015 14:37:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/Hi/m-p/425231#M12583</guid>
      <dc:creator>TomE</dc:creator>
      <dc:date>2015-10-03T14:37:13Z</dc:date>
    </item>
    <item>
      <title>Re: Hi</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/Hi/m-p/425232#M12584</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Netburner make a WiFi module that has a UART or SPI interface for USD25 in one offs:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/www.netburner.com/products/wireless/nbwifiin-802-11b-g-n" target="test_blank"&gt;www.netburner.com/products/wireless/nbwifiin-802-11b-g-n&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Shaun&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 06 Oct 2015 00:13:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/Hi/m-p/425232#M12584</guid>
      <dc:creator>yibbidy</dc:creator>
      <dc:date>2015-10-06T00:13:28Z</dc:date>
    </item>
  </channel>
</rss>