<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>ColdFire/68K Microcontrollers and ProcessorsのトピックMCF5213 ADC</title>
    <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/MCF5213-ADC/m-p/133419#M1249</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;Hi,&lt;/DIV&gt;&lt;DIV&gt;I want to know about the type of ADC in MCF5213&lt;/DIV&gt;&lt;DIV&gt;Thanks.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 18 Oct 2006 13:09:40 GMT</pubDate>
    <dc:creator>Vijaya</dc:creator>
    <dc:date>2006-10-18T13:09:40Z</dc:date>
    <item>
      <title>MCF5213 ADC</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/MCF5213-ADC/m-p/133419#M1249</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;Hi,&lt;/DIV&gt;&lt;DIV&gt;I want to know about the type of ADC in MCF5213&lt;/DIV&gt;&lt;DIV&gt;Thanks.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 18 Oct 2006 13:09:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/MCF5213-ADC/m-p/133419#M1249</guid>
      <dc:creator>Vijaya</dc:creator>
      <dc:date>2006-10-18T13:09:40Z</dc:date>
    </item>
    <item>
      <title>Re: MCF5213 ADC</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/MCF5213-ADC/m-p/133420#M1250</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;Here are the main features of the AtoD converter on the MCF5213:&lt;BR /&gt;&lt;BR /&gt;The analog-to-digital converter (ADC) consists of two separate and complete ADCs, each with their own&lt;BR /&gt;sample and hold circuits. The converters share a common voltage reference and common digital control&lt;BR /&gt;module.&lt;BR /&gt;&lt;BR /&gt;The ADC’s characteristics include the following:&lt;BR /&gt;• 12-bit resolution&lt;BR /&gt;• Maximum ADC clock frequency of 5.0 MHz, 200ns period&lt;BR /&gt;• Sampling rate up to 1.66 million samples per second1&lt;BR /&gt;• Single conversion time of 8.5 ADC clock cycles (8.5 × 200ns = 1.7µs)&lt;BR /&gt;• Additional conversion time of 6 ADC clock cycles (6 × 200ns = 1.2µs)&lt;BR /&gt;• Eight conversions in 26.5 ADC clocks (26.5×200ns = 5.3µs) using simultaneous mode&lt;BR /&gt;• Ability to simultaneously sample and hold 2 inputs&lt;BR /&gt;• Ability to sequentially scan and store up to 8 measurements&lt;BR /&gt;• Internal multiplex to select two of 8 inputs&lt;BR /&gt;• Power savings modes allow automatic shutdown/startup of all or part of ADC&lt;BR /&gt;• Those inputs not selected tolerate injected/sourced current without affecting ADC performance,&lt;BR /&gt;supporting operation in noisy industrial environments.&lt;BR /&gt;• Optional interrupts at the end of a scan, if an out-of-range limit is exceeded (high or low), or at zero&lt;BR /&gt;crossing&lt;BR /&gt;• Optional sample correction by subtracting a pre-programmed offset value&lt;BR /&gt;• Signed or unsigned result&lt;BR /&gt;• Single ended or differential inputs for all input pins with support for an arbitrary mix of input types&lt;BR /&gt;&lt;BR /&gt;More information on the A/D converter can be found in the MCF5213 user's manual. Here's the link:&lt;BR /&gt;&lt;A href="http://www.freescale.com/files/32bit/doc/ref_manual/MCF5213RM.pdf" target="test_blank"&gt;http://www.freescale.com/files/32bit/doc/ref_manual/MCF5213RM.pdf&lt;/A&gt;&lt;BR /&gt;&lt;BR /&gt;regards,&lt;BR /&gt;mpeters&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 24 Oct 2006 05:40:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/MCF5213-ADC/m-p/133420#M1250</guid>
      <dc:creator>mpeters</dc:creator>
      <dc:date>2006-10-24T05:40:08Z</dc:date>
    </item>
  </channel>
</rss>