<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: MCF5282 Obsolete in ColdFire/68K Microcontrollers and Processors</title>
    <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/MCF5282-Obsolete/m-p/400655#M12483</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Tom,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am going to switch to ARM based MCU and have to re-write all code I have on MCF5282 because I have no other choice.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I will keep eye on Freescale web to see when the last order is coming, hope it never comes...&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Christie&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 11 Nov 2015 14:36:02 GMT</pubDate>
    <dc:creator>a8Chcx</dc:creator>
    <dc:date>2015-11-11T14:36:02Z</dc:date>
    <item>
      <title>MCF5282 Obsolete</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/MCF5282-Obsolete/m-p/400653#M12481</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I am using MCF5282 and becoming obsolete.&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Can anyone tell me where it will stop production?&lt;/P&gt;&lt;P&gt;Is there any alternative that I can use?&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Christie&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 10 Nov 2015 17:03:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/MCF5282-Obsolete/m-p/400653#M12481</guid>
      <dc:creator>a8Chcx</dc:creator>
      <dc:date>2015-11-10T17:03:20Z</dc:date>
    </item>
    <item>
      <title>Re: MCF5282 Obsolete</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/MCF5282-Obsolete/m-p/400654#M12482</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;MCF5282 Device Page:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A class="jive-link-external-small" href="http://www.freescale.com/products/more-processors/32-bit-mcu-and-mpu/coldfire-plus-coldfire-mcus-mpus/coldfire-mcus/v2-mcu/integrated-coldfire-v2-ethernet-can-and-flash-microcontrollers:MCF528X?&amp;amp;cof=0&amp;amp;am=0&amp;amp;tab=Buy_Parametric_Tab&amp;amp;fromSearch=false" rel="nofollow"&gt;http://www.freescale.com/products/more-processors/32-bit-mcu-and-mpu/coldfire-plus-coldfire-mcus-mpus/coldfire-mcus/v2-mcu/integrated-coldfire-v2-ethernet-can-and-flash-microcontrollers:MCF528X?&amp;amp;cof=0&amp;amp;am=0&amp;amp;tab=Buy_Parametric_Tab&amp;amp;fromSearch=false&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;It is marked '&lt;SPAN class="ng-scope"&gt;&lt;SPAN class="ng-scope cellCont"&gt;&lt;SPAN class="ng-binding cellContainer"&gt;Not Recommended for New Design". It is also marked "&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;SPAN class="ng-scope"&gt;&lt;SPAN class="ng-scope cellCont"&gt;&lt;SPAN class="ng-binding cellContainer"&gt;10-YEARS APPLICATION LIFE", but they don't give the start date.&lt;BR /&gt;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="ng-scope"&gt;&lt;SPAN class="ng-scope cellCont"&gt;&lt;SPAN class="ng-binding cellContainer"&gt;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="ng-scope"&gt;&lt;SPAN class="ng-scope cellCont"&gt;&lt;SPAN class="ng-binding cellContainer"&gt;I went through this for another CPU here:&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="ng-scope"&gt;&lt;SPAN class="ng-scope cellCont"&gt;&lt;SPAN class="ng-binding cellContainer"&gt;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="ng-scope"&gt;&lt;SPAN class="ng-scope cellCont"&gt;&lt;SPAN class="ng-binding cellContainer"&gt;&lt;A class="jive-link-message-small" data-containerid="2018" data-containertype="14" data-objectid="537937" data-objecttype="2" href="https://community.freescale.com/message/537937#537937"&gt;https://community.freescale.com/message/537937#537937&lt;/A&gt;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="ng-scope"&gt;&lt;SPAN class="ng-scope cellCont"&gt;&lt;SPAN class="ng-binding cellContainer"&gt;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/SPAN&gt;That shows "Not Recommended for New Designs". &lt;SPAN class="ng-scope"&gt;&lt;SPAN class="ng-scope cellCont"&gt;&lt;SPAN class="ng-binding cellContainer"&gt;It is also marked "&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;SPAN class="ng-scope"&gt;&lt;SPAN class="ng-scope cellCont"&gt;&lt;SPAN class="ng-binding cellContainer"&gt;10-YEARS APPLICATION LIFE", but they don't give the start date. &lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/SPAN&gt;OK, so how long then? Click on "Show Parametrics", then drag "Last Order Date" into the "Show" column and Apply.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;That shows a "Last Ship Date" of &lt;SPAN&gt;&lt;SPAN class="name ng-binding"&gt;11/13/2014. "Last Order Date" of &lt;/SPAN&gt;&lt;/SPAN&gt;&lt;SPAN&gt;&lt;SPAN class="name ng-binding"&gt;2013-11-1, but only for SOME of the packages, types and speed grades.&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;&lt;SPAN class="name ng-binding"&gt;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;&lt;SPAN class="name ng-binding"&gt;Another thing to do is to &lt;/SPAN&gt;&lt;/SPAN&gt;click on the "Overview" tab and then search for "Product Longevity Program". There isn't one, but here's one I prepared earlier&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A class="jive-link-external-small" data-content-finding="Community" href="http://www.freescale.com/webapp/sps/site/overview.jsp?code=PRDCT_LONGEVITY_HM" rel="nofollow"&gt;Product Longevity|Freescale&lt;/A&gt; &lt;/P&gt;&lt;P&gt;&lt;SPAN class="ng-scope"&gt;&lt;SPAN class="ng-scope cellCont"&gt;&lt;SPAN class="ng-binding cellContainer"&gt;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="ng-scope"&gt;&lt;SPAN class="ng-scope cellCont"&gt;&lt;SPAN class="ng-binding cellContainer"&gt;Not there. Click on the "Archived" page:&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="ng-scope"&gt;&lt;SPAN class="ng-scope cellCont"&gt;&lt;SPAN class="ng-binding cellContainer"&gt;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="ng-scope"&gt;&lt;SPAN class="ng-scope cellCont"&gt;&lt;SPAN class="ng-binding cellContainer"&gt;&lt;A class="jive-link-external-small" href="http://www.freescale.com/pages/product-longevity-archived:LONGEVITY-ARCHIVED" rel="nofollow"&gt;http://www.freescale.com/pages/product-longevity-archived:LONGEVITY-ARCHIVED&lt;/A&gt;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="ng-scope"&gt;&lt;SPAN class="ng-scope cellCont"&gt;&lt;SPAN class="ng-binding cellContainer"&gt;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="ng-scope"&gt;&lt;SPAN class="ng-scope cellCont"&gt;&lt;SPAN class="ng-binding cellContainer"&gt;MCF521x (521x and 528x are the same family) is 10 years from September 2005. So that's gone.&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="ng-scope"&gt;&lt;SPAN class="ng-scope cellCont"&gt;&lt;SPAN class="ng-binding cellContainer"&gt;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="ng-scope"&gt;&lt;SPAN class="ng-scope cellCont"&gt;&lt;SPAN class="ng-binding cellContainer"&gt;&amp;gt; &lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/SPAN&gt;Can anyone tell me where it will stop production?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Ask your Distributor. Otherwise keep a monthly eye on the above Product Page.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Remember that "Last Time Buy" is always an option. Buy as many as you'll need for the rest of your production.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;gt; Is there any alternative that I can use?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;You're very unlikely to get anything pin compatible unless you're going from something like the MCF5281 to MCF5282 or to the faster speed grade of the same chip.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;So you need to list all of the features you need in your product that you are using in that chip, and then search for something else with a longer life and the same (or similar) features.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Then you have to do some real work going through the Parametrics Lists and the Data Sheets. This isn't something anyone else can do for you.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I see you've already asked this on the Kinetis list and in relation to the MC56F8367. Going to an ARM based product is a good idea if you can.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Has your code been written to only work on a Coldfire? it is big-endian, ARM is little-endian. Coldfire has multiple interrupt levels, ARM not so much. ColdFire peripherals are different to ARM ones and so on, so there's a LOT of code rewriting if you're not using a standard operating system that comes with working drivers.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If your code isn't portable you may need another Coldfire chip. I know the MCF5329 has a 15 year life from 2007 because I looked it up. You'll have to do the same for all the other chips that might do what you need.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Tom&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 11 Nov 2015 00:09:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/MCF5282-Obsolete/m-p/400654#M12482</guid>
      <dc:creator>TomE</dc:creator>
      <dc:date>2015-11-11T00:09:04Z</dc:date>
    </item>
    <item>
      <title>Re: MCF5282 Obsolete</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/MCF5282-Obsolete/m-p/400655#M12483</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Tom,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am going to switch to ARM based MCU and have to re-write all code I have on MCF5282 because I have no other choice.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I will keep eye on Freescale web to see when the last order is coming, hope it never comes...&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Christie&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 11 Nov 2015 14:36:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/MCF5282-Obsolete/m-p/400655#M12483</guid>
      <dc:creator>a8Chcx</dc:creator>
      <dc:date>2015-11-11T14:36:02Z</dc:date>
    </item>
    <item>
      <title>Re: MCF5282 Obsolete</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/MCF5282-Obsolete/m-p/400656#M12484</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&amp;gt; I have no other choice.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;You have a huge number of choices, unless someone in "management" has issued some sort of edict.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;Wait until you can't buy any, then panic (not a good idea),&lt;/LI&gt;&lt;LI&gt;Last-Time-Buy. Buy enough for 5 to 10 years worth of projected production,&lt;/LI&gt;&lt;LI&gt;Switch to a different ColdFire chip that has the features you need and a longer life (if one exists),&lt;/LI&gt;&lt;LI&gt;Switch to a Kinetis chip that has the features you need (if one exists),&lt;/LI&gt;&lt;LI&gt;Switch to a chip from some other manufacturer,&lt;/LI&gt;&lt;LI&gt;Stop making the product, or replace it with a newer one,&lt;/LI&gt;&lt;LI&gt;Get a job somewhere else and make this "someone else's problem".&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;A quick check of ColdFire chip features shows the MCF5282 has:&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;80MHz ISA_A with "68k emulation exception", and 2k of Cache.&lt;/LI&gt;&lt;LI&gt;64k SRAM and 512k of Flash&lt;/LI&gt;&lt;LI&gt;100MHz Ethernet&lt;/LI&gt;&lt;LI&gt;CAN&lt;/LI&gt;&lt;LI&gt;Three UARTs&lt;/LI&gt;&lt;LI&gt;I2C&lt;/LI&gt;&lt;LI&gt;QSPI&lt;/LI&gt;&lt;LI&gt;QADC with 18 inputs&lt;/LI&gt;&lt;LI&gt;Four PIT, four DMA Timers, two GPT&lt;/LI&gt;&lt;LI&gt;Four channel DMA controller&lt;/LI&gt;&lt;LI&gt;External 32 bit bus interface.&lt;/LI&gt;&lt;LI&gt;Up to 142 GPIO pins&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The MCF5225x has most of the above. 80MHz with 512k Flash, 64k RAM, Ethernet, CAN, DMA, ADC, but only up to 96 GPIOs. It has a 10 year life starting from November 2008.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If you don't need all that you could use the MCF5223x. It has a 10 year life starting from March 2007 (not so good).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If you are using (or can use) external FLASH you could use the MCF5227x.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If you need Ethernet and CAN, and you want a Kinetis part, then you need the K6 or K7 series:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A class="jive-link-external-small" href="http://www.freescale.com/products/arm-processors/kinetis-cortex-m/k-series:KINETIS_K_SERIES?cof=0&amp;amp;am=0" rel="nofollow"&gt;http://www.freescale.com/products/arm-processors/kinetis-cortex-m/k-series:KINETIS_K_SERIES?cof=0&amp;amp;am=0&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;it is all a trade-off between getting a long life (Kinetic K seeries is 10 years from 2011/2014 depending on the model) and the amount of work needed to rewrite the code.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;It would be worth changing your code to use an Operating System that already comes with some hardware drivers. That should be faster, cheaper and would make the next change easier.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Tom&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 12 Nov 2015 04:49:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/MCF5282-Obsolete/m-p/400656#M12484</guid>
      <dc:creator>TomE</dc:creator>
      <dc:date>2015-11-12T04:49:04Z</dc:date>
    </item>
  </channel>
</rss>