<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Flashing a MCF5272  with CFFlasher  CLI in ColdFire/68K Microcontrollers and Processors</title>
    <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/Flashing-a-MCF5272-with-CFFlasher-CLI/m-p/384419#M12440</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks for the answer.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I tried to use the CFFlasher in a script, thats the reason i wanted the CLI. Now im abusing the GUI by simulating keyboard inputs with the win32api. Works quite well.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 11 Sep 2014 10:44:35 GMT</pubDate>
    <dc:creator>meka_tama</dc:creator>
    <dc:date>2014-09-11T10:44:35Z</dc:date>
    <item>
      <title>Flashing a MCF5272  with CFFlasher  CLI</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/Flashing-a-MCF5272-with-CFFlasher-CLI/m-p/384417#M12438</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I am flashing a Coldfire MCF5272 with the CFFlasher 3.1.10 on Windows 7.&lt;/P&gt;&lt;P&gt;If i use the GUI everythings works fine, but when i try to get the same result with the CLI it doesn´t work.&lt;/P&gt;&lt;P&gt;I tried it with:&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; CFFlasher.exe -t TARGET -p FILE -s -bdm PE_USB_ML&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;The programm tried to flash and it seems to work (no errors, just reports that the programm started and finished), but when I verify the result with the CFFlasher the data is just 0xFFFFFFFF.&lt;/P&gt;&lt;P&gt;It seems that only the erase works but not the programming.&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;There is an old discussion (&lt;/SPAN&gt;&lt;A _jive_internal="true" data-containerid="2018" data-containertype="14" data-objectid="21082" data-objecttype="1" href="https://community.nxp.com/thread/21082"&gt;https://community.freescale.com/thread/21082&lt;/A&gt;&lt;SPAN&gt;) with the same problem but there is no answer.&lt;/SPAN&gt;&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;What may be the cause? If this is a problem in the CFFlasher, is there another programm to flash a MCF5272 (except the PROGCFZ)?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 27 Aug 2014 11:01:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/Flashing-a-MCF5272-with-CFFlasher-CLI/m-p/384417#M12438</guid>
      <dc:creator>meka_tama</dc:creator>
      <dc:date>2014-08-27T11:01:23Z</dc:date>
    </item>
    <item>
      <title>Re: Flashing a MCF5272  with CFFlasher  CLI</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/Flashing-a-MCF5272-with-CFFlasher-CLI/m-p/384418#M12439</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Well, the Cfflasher is quite old FSL free Flash Programming tool for FSL evaluation board. There really has problems &amp;amp; bugs with the CLI and for the reason that this tool is EOL now, so we have no resource to update the bug any more. (Anyway, the GUI is the recommend and should work without problem.)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Fang&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 11 Sep 2014 09:26:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/Flashing-a-MCF5272-with-CFFlasher-CLI/m-p/384418#M12439</guid>
      <dc:creator>miduo</dc:creator>
      <dc:date>2014-09-11T09:26:23Z</dc:date>
    </item>
    <item>
      <title>Re: Flashing a MCF5272  with CFFlasher  CLI</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/Flashing-a-MCF5272-with-CFFlasher-CLI/m-p/384419#M12440</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks for the answer.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I tried to use the CFFlasher in a script, thats the reason i wanted the CLI. Now im abusing the GUI by simulating keyboard inputs with the win32api. Works quite well.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 11 Sep 2014 10:44:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/Flashing-a-MCF5272-with-CFFlasher-CLI/m-p/384419#M12440</guid>
      <dc:creator>meka_tama</dc:creator>
      <dc:date>2014-09-11T10:44:35Z</dc:date>
    </item>
  </channel>
</rss>