<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>ColdFire/68K Microcontrollers and ProcessorsのトピックRe: MCF52233 Flash program utility for Windows 64 bit</title>
    <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/MCF52233-Flash-program-utility-for-Windows-64-bit/m-p/332510#M12232</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Using CF Flasher in a Windows 7 virtual machine (like in VMWARE Player) might help. It's what I do to keep using the legacy Codewarrior 7.2.2 which doesn't work in a 64bit environment either.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 29 Jan 2015 11:40:33 GMT</pubDate>
    <dc:creator>vier_kuifjes</dc:creator>
    <dc:date>2015-01-29T11:40:33Z</dc:date>
    <item>
      <title>MCF52233 Flash program utility for Windows 64 bit</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/MCF52233-Flash-program-utility-for-Windows-64-bit/m-p/332507#M12229</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I use the CF flasher (version 3.1.10) to program MCF52233 on Windows 7 ,32 bit which works fine.&lt;/P&gt;&lt;P&gt;The problem is that CF Flasher doesn't work on Windows 7 ,64 bit.&lt;/P&gt;&lt;P&gt;1. Are there any plans porting it for 64 bit ?&lt;/P&gt;&lt;P&gt;2.If the answer is no, I am interested in another simple utility for programming - for production purposes.&lt;/P&gt;&lt;P&gt;I am looking for a free one, since only basic features are needed (without mass production features).&lt;/P&gt;&lt;P&gt;Is there some free utility by Freescale to program/verify/erase the flash memory?&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Gil&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 08 Dec 2014 12:38:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/MCF52233-Flash-program-utility-for-Windows-64-bit/m-p/332507#M12229</guid>
      <dc:creator>gilfine</dc:creator>
      <dc:date>2014-12-08T12:38:22Z</dc:date>
    </item>
    <item>
      <title>Re: MCF52233 Flash program utility for Windows 64 bit</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/MCF52233-Flash-program-utility-for-Windows-64-bit/m-p/332508#M12230</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Two weeks and no response. I don't know anything about this, but it has been too long, so... My turn!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Type "64 bit" and "windows 7" into the Search Box and do some research on how long people have been asking these questions.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I think you have to dedicate a 32-bit computer as the one that has to be used to debug and program these chips. Just think of the whole computer as "a very large programming pod with a screen and keyboard". Then make sure you can clone/mirror it onto other hardware if it dies. You have to keep it/them alive for the duration of your production run and your customer support phase.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Tom&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 22 Dec 2014 06:44:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/MCF52233-Flash-program-utility-for-Windows-64-bit/m-p/332508#M12230</guid>
      <dc:creator>TomE</dc:creator>
      <dc:date>2014-12-22T06:44:08Z</dc:date>
    </item>
    <item>
      <title>Re: MCF52233 Flash program utility for Windows 64 bit</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/MCF52233-Flash-program-utility-for-Windows-64-bit/m-p/332509#M12231</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Henri Laidet (the chap who made the DigiButler project) made an equivalent to CF_Flasher that works with the TBLCF and OSBDM, not sure about the PE Multilink.&amp;nbsp; I haven't used it myself but it might be worth a shot.&amp;nbsp; You can get the source and binary here: &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="http://hlaidet.pagesperso-orange.fr/H_Flasher.htm" title="http://hlaidet.pagesperso-orange.fr/H_Flasher.htm"&gt;H_Flasher&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Shaun&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 23 Dec 2014 22:52:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/MCF52233-Flash-program-utility-for-Windows-64-bit/m-p/332509#M12231</guid>
      <dc:creator>yibbidy</dc:creator>
      <dc:date>2014-12-23T22:52:38Z</dc:date>
    </item>
    <item>
      <title>Re: MCF52233 Flash program utility for Windows 64 bit</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/MCF52233-Flash-program-utility-for-Windows-64-bit/m-p/332510#M12232</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Using CF Flasher in a Windows 7 virtual machine (like in VMWARE Player) might help. It's what I do to keep using the legacy Codewarrior 7.2.2 which doesn't work in a 64bit environment either.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 29 Jan 2015 11:40:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/MCF52233-Flash-program-utility-for-Windows-64-bit/m-p/332510#M12232</guid>
      <dc:creator>vier_kuifjes</dc:creator>
      <dc:date>2015-01-29T11:40:33Z</dc:date>
    </item>
  </channel>
</rss>