<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>ColdFire/68K Microcontrollers and ProcessorsのトピックRe: When using mini-flex bus on MCF52259 - do I need to connect pull-up to D0-D7 ?</title>
    <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/When-using-mini-flex-bus-on-MCF52259-do-I-need-to-connect-pull/m-p/317808#M12169</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Usually pull-ups are required on data bus, to make a legal voltage levels between access to the different devices on the bus.&lt;/P&gt;&lt;P&gt;Unless the devices on the data bus have internal pull-ups.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 12 Jun 2014 07:55:31 GMT</pubDate>
    <dc:creator>ambre</dc:creator>
    <dc:date>2014-06-12T07:55:31Z</dc:date>
    <item>
      <title>When using mini-flex bus on MCF52259 - do I need to connect pull-up to D0-D7 ?</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/When-using-mini-flex-bus-on-MCF52259-do-I-need-to-connect-pull/m-p/317806#M12167</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Usually, pull-ups are needed on data bus, but in the MCF52259EVB schematic - no pull-ups are mentioned.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 12 Jun 2014 07:15:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/When-using-mini-flex-bus-on-MCF52259-do-I-need-to-connect-pull/m-p/317806#M12167</guid>
      <dc:creator>ambre</dc:creator>
      <dc:date>2014-06-12T07:15:58Z</dc:date>
    </item>
    <item>
      <title>Re: When using mini-flex bus on MCF52259 - do I need to connect pull-up to D0-D7 ?</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/When-using-mini-flex-bus-on-MCF52259-do-I-need-to-connect-pull/m-p/317807#M12168</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Why do you think pullups are required on a data bus?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;There are some instances in which this might be useful; I'm interested in your reasons.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Tom&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 12 Jun 2014 07:34:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/When-using-mini-flex-bus-on-MCF52259-do-I-need-to-connect-pull/m-p/317807#M12168</guid>
      <dc:creator>TomE</dc:creator>
      <dc:date>2014-06-12T07:34:34Z</dc:date>
    </item>
    <item>
      <title>Re: When using mini-flex bus on MCF52259 - do I need to connect pull-up to D0-D7 ?</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/When-using-mini-flex-bus-on-MCF52259-do-I-need-to-connect-pull/m-p/317808#M12169</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Usually pull-ups are required on data bus, to make a legal voltage levels between access to the different devices on the bus.&lt;/P&gt;&lt;P&gt;Unless the devices on the data bus have internal pull-ups.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 12 Jun 2014 07:55:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/When-using-mini-flex-bus-on-MCF52259-do-I-need-to-connect-pull/m-p/317808#M12169</guid>
      <dc:creator>ambre</dc:creator>
      <dc:date>2014-06-12T07:55:31Z</dc:date>
    </item>
    <item>
      <title>Re: When using mini-flex bus on MCF52259 - do I need to connect pull-up to D0-D7 ?</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/When-using-mini-flex-bus-on-MCF52259-do-I-need-to-connect-pull/m-p/317809#M12170</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&amp;gt; legal voltage levels between access to the different devices on the bus.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Between accesses, no device cares what the levels are on the bus, so it doesn't really matter.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;You haven't given me your specific reasons for wanting "legal voltage levels" between cycles.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Or why the EVB should be supporting and demonstrating that need or requirement.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Tom&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 12 Jun 2014 23:24:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/When-using-mini-flex-bus-on-MCF52259-do-I-need-to-connect-pull/m-p/317809#M12170</guid>
      <dc:creator>TomE</dc:creator>
      <dc:date>2014-06-12T23:24:44Z</dc:date>
    </item>
    <item>
      <title>Re: When using mini-flex bus on MCF52259 - do I need to connect pull-up to D0-D7 ?</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/When-using-mini-flex-bus-on-MCF52259-do-I-need-to-connect-pull/m-p/317810#M12171</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Typically, since the data lines can be inputs it is best not to have them floating at any time. However, we don't use pullups/downs on the data buses on our ColdFire eval boards. &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 16 Jun 2014 08:28:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/When-using-mini-flex-bus-on-MCF52259-do-I-need-to-connect-pull/m-p/317810#M12171</guid>
      <dc:creator>miduo</dc:creator>
      <dc:date>2014-06-16T08:28:03Z</dc:date>
    </item>
  </channel>
</rss>