<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>ColdFire/68K Microcontrollers and Processorsのトピックppp over serial</title>
    <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/ppp-over-serial/m-p/314640#M12158</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I have already posted this query in many threads&amp;nbsp; but could not get any appropriate solution.&lt;/P&gt;&lt;P&gt;So, I am reposting my query with more details:-&lt;/P&gt;&lt;P&gt;I am using mcf52259 .&lt;/P&gt;&lt;P&gt;I want to connect mcf52259 to modem using serial port .(mcf52259---------------------&amp;gt;Modem)&lt;/P&gt;&lt;P&gt;I took sample code to start ppp in mqx and it works fine when connected to PC.&lt;/P&gt;&lt;P&gt;mcf52259--------serial port---------&amp;gt;PC&lt;/P&gt;&lt;P&gt;Now, i want Mcf52259 to communicate with modem through serial port .&lt;/P&gt;&lt;P&gt;I want to send AT commands from MCF52259 to modem to start ppp &amp;amp; ppp of mqx should syn with modem for further data transfer how to go further with this .&lt;/P&gt;&lt;P&gt;AT command which i am gone send to start PPP in modem is&lt;/P&gt;&lt;P&gt;AT&lt;/P&gt;&lt;P&gt;ATZ&lt;/P&gt;&lt;P&gt;AT+CGDCONT+1,"IP","airtelgprs.com"&lt;/P&gt;&lt;P&gt;ATD*999***1#&lt;/P&gt;&lt;P&gt;The given above AT commands starts ppp in modem.&lt;/P&gt;&lt;P&gt;what changes i need to do n sample code make it works .&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;please do reply&lt;/P&gt;&lt;P&gt;Thanks in advance&lt;/P&gt;&lt;P&gt;Netra &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 05 Jun 2014 05:43:51 GMT</pubDate>
    <dc:creator>netra</dc:creator>
    <dc:date>2014-06-05T05:43:51Z</dc:date>
    <item>
      <title>ppp over serial</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/ppp-over-serial/m-p/314640#M12158</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I have already posted this query in many threads&amp;nbsp; but could not get any appropriate solution.&lt;/P&gt;&lt;P&gt;So, I am reposting my query with more details:-&lt;/P&gt;&lt;P&gt;I am using mcf52259 .&lt;/P&gt;&lt;P&gt;I want to connect mcf52259 to modem using serial port .(mcf52259---------------------&amp;gt;Modem)&lt;/P&gt;&lt;P&gt;I took sample code to start ppp in mqx and it works fine when connected to PC.&lt;/P&gt;&lt;P&gt;mcf52259--------serial port---------&amp;gt;PC&lt;/P&gt;&lt;P&gt;Now, i want Mcf52259 to communicate with modem through serial port .&lt;/P&gt;&lt;P&gt;I want to send AT commands from MCF52259 to modem to start ppp &amp;amp; ppp of mqx should syn with modem for further data transfer how to go further with this .&lt;/P&gt;&lt;P&gt;AT command which i am gone send to start PPP in modem is&lt;/P&gt;&lt;P&gt;AT&lt;/P&gt;&lt;P&gt;ATZ&lt;/P&gt;&lt;P&gt;AT+CGDCONT+1,"IP","airtelgprs.com"&lt;/P&gt;&lt;P&gt;ATD*999***1#&lt;/P&gt;&lt;P&gt;The given above AT commands starts ppp in modem.&lt;/P&gt;&lt;P&gt;what changes i need to do n sample code make it works .&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;please do reply&lt;/P&gt;&lt;P&gt;Thanks in advance&lt;/P&gt;&lt;P&gt;Netra &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 05 Jun 2014 05:43:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/ppp-over-serial/m-p/314640#M12158</guid>
      <dc:creator>netra</dc:creator>
      <dc:date>2014-06-05T05:43:51Z</dc:date>
    </item>
  </channel>
</rss>