<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>ColdFire/68K Microcontrollers and ProcessorsのトピックRe: Intermittent USB Recognition Issue</title>
    <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/Intermittent-USB-Recognition-Issue/m-p/287593#M12029</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Pepe,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks for the info...we have resolved the issue the internal VREG was not being supplied with the correct voltage via VBUS causing a inconsistent signal. &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks...&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 12 Mar 2013 21:05:47 GMT</pubDate>
    <dc:creator>grt951</dc:creator>
    <dc:date>2013-03-12T21:05:47Z</dc:date>
    <item>
      <title>Intermittent USB Recognition Issue</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/Intermittent-USB-Recognition-Issue/m-p/287591#M12027</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am using the freescale USB CDC stack and virtual com port driver for the MCF51JE256 as a device only and have a intermittent issue where windows will not recognize the device. The hardware is to the USB app note (33ohm series resistors and 1.5k pull-up on D+) and the device will recognize roughly 50% of the time. It seems to also be PC dependent which is why I am looking at the hardware...any ideas? &lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Gary &lt;/P&gt;&lt;P&gt;EE &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 07 Mar 2013 16:26:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/Intermittent-USB-Recognition-Issue/m-p/287591#M12027</guid>
      <dc:creator>grt951</dc:creator>
      <dc:date>2013-03-07T16:26:28Z</dc:date>
    </item>
    <item>
      <title>Re: Intermittent USB Recognition Issue</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/Intermittent-USB-Recognition-Issue/m-p/287592#M12028</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Gary,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Are you using an external 1.5K ohm resistor or the internal one?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If you use an external one you are not giving enough time to the MCU to enable properly the internal PLL and all the USB stack. remove the external pull-up resistor. the MCU already has an internal resistor that will be activated in SW.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;try it and let us know if worked.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;regards&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 12 Mar 2013 05:16:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/Intermittent-USB-Recognition-Issue/m-p/287592#M12028</guid>
      <dc:creator>Pepe_Ruiz</dc:creator>
      <dc:date>2013-03-12T05:16:41Z</dc:date>
    </item>
    <item>
      <title>Re: Intermittent USB Recognition Issue</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/Intermittent-USB-Recognition-Issue/m-p/287593#M12029</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Pepe,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks for the info...we have resolved the issue the internal VREG was not being supplied with the correct voltage via VBUS causing a inconsistent signal. &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks...&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 12 Mar 2013 21:05:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/Intermittent-USB-Recognition-Issue/m-p/287593#M12029</guid>
      <dc:creator>grt951</dc:creator>
      <dc:date>2013-03-12T21:05:47Z</dc:date>
    </item>
  </channel>
</rss>