<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>ColdFire/68K Microcontrollers and ProcessorsのトピックRe: 52259 counter</title>
    <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/52259-counter/m-p/284346#M11980</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks Tom for the clarification.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;One more question, I was reading through the documentation MCF52259RM. The formula mentioned in section 26.4.2 about calculating the timeout values is little strange.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;For example in section 26.1.2, the maximum timeout mentioned is 109,951 seconds at 80 MHz (~31 hours).&amp;nbsp; &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;But if I use the formula in section 26.4.2, that is&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Timeout period = (1 ⁄ 80000000) × 16 × (0xFF + 1) × (0xFFFFFFFF + 1) = 219,902.3255552 seconds.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;System Frequency: 80 MHz&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;But if I divide the timeout period by 2, then i will get the mentioned maximum timeout period.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Once again thanks for the help.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 14 Jun 2013 12:33:26 GMT</pubDate>
    <dc:creator>salman83</dc:creator>
    <dc:date>2013-06-14T12:33:26Z</dc:date>
    <item>
      <title>52259 counter</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/52259-counter/m-p/284340#M11974</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I want to measure in milliseconds on mcf52259. I can't use RTC, so I am left with GPT. How do i do it.&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks &amp;amp; Regards.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 10 Jun 2013 14:35:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/52259-counter/m-p/284340#M11974</guid>
      <dc:creator>salman83</dc:creator>
      <dc:date>2013-06-10T14:35:15Z</dc:date>
    </item>
    <item>
      <title>Re: 52259 counter</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/52259-counter/m-p/284341#M11975</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&amp;gt; How do I do it.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Is this homework?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Read the manual. Write some code.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Or search for some sample code and App Notes. Type "GPT sample code" into the "Search" box on this page for starters. Or type register names into Google.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;have you gone to the MCF52259 Product Page and downloaded "&lt;A href="http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=MCF5225X&amp;amp;nodeId=018rH3YTLC00M95448&amp;amp;fpsp=1&amp;amp;tab=Design_Tools_Tab"&gt;MCF5225X_SAMPLE_CODE&lt;/A&gt;:"? It may not help but you should try that first.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;You don't say WHAT you want to measure. If you want to accurately measure an external signal then you want to use "Capture" mode of the GPT. if you want to measure software execution time, or to have a timer you can use from software you're better off programming a DMA Timer to free-run at 1MHz and just read the DMA Counter register to get "the time". Then subtract subsequent samples to get the duration.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Tom&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 11 Jun 2013 04:30:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/52259-counter/m-p/284341#M11975</guid>
      <dc:creator>TomE</dc:creator>
      <dc:date>2013-06-11T04:30:06Z</dc:date>
    </item>
    <item>
      <title>Re: 52259 counter</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/52259-counter/m-p/284342#M11976</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Tom,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks for the reply.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;It is not a homework.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Basically, I want to use some timeouts in my code. It does not require any capture from external signal.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;So you are suggesting me that I should go for DMA timers for measuring time (milliseconds) in the software.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 11 Jun 2013 13:48:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/52259-counter/m-p/284342#M11976</guid>
      <dc:creator>salman83</dc:creator>
      <dc:date>2013-06-11T13:48:32Z</dc:date>
    </item>
    <item>
      <title>Re: 52259 counter</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/52259-counter/m-p/284343#M11977</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&amp;gt; It is not a homework.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I couldn't tell from your post that it wasn't.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;gt; So you are suggesting me&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Yes. They are very easy to program and use for this.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Tom&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 11 Jun 2013 13:56:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/52259-counter/m-p/284343#M11977</guid>
      <dc:creator>TomE</dc:creator>
      <dc:date>2013-06-11T13:56:54Z</dc:date>
    </item>
    <item>
      <title>Re: 52259 counter</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/52259-counter/m-p/284344#M11978</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Tom,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I looked into the DMA Timers. I found that t&lt;SPAN style="font-size: 10pt; line-height: 1.5em;"&gt;here is no overflow flag to tell that the counter has reached its upper limit.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I want a counter which i can use to calculate the start and end time. If the difference is 500 milliseconds, then I execute a certain operation. I do not want any interrupts at all.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks for your help anyway.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 13 Jun 2013 10:50:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/52259-counter/m-p/284344#M11978</guid>
      <dc:creator>salman83</dc:creator>
      <dc:date>2013-06-13T10:50:04Z</dc:date>
    </item>
    <item>
      <title>Re: 52259 counter</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/52259-counter/m-p/284345#M11979</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&amp;gt; I want a counter which i can use to calculate the start and end time&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Which the DMA timers are perfect for. There's no need for overflow interrupts or anything.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;gt; I do not want any interrupts at all.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;What makes you think you even need an interrupt? What broken timers have you used in the past that need this (maybey timers on 8-bitters).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I guess this might be a little "tricky", but I've known about this use of simple binary arithmetic for so long it just seems an utterly obvious way to do this.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;You set up the DMA Timer to free-run instead of resetting at a reference value, so it counts from zero to 0xffffffff AND THEN ROLLS OVER TO ZERO. This is incredibly powerful and simple. To use this, all you have to do is set the timer running and then:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;unsigned long nTime1 = DTCn;&lt;/P&gt;&lt;P&gt;... Do something that you want to time ...&lt;/P&gt;&lt;P&gt;unsigned long nTime2 = DTCn;&lt;/P&gt;&lt;P&gt;unsigned long nElapsedTime = nTimer2 - nTime1;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;THAT'S IT. You're subtracting two 32-bit numbers. No need to worry about rollover or anything. As long as the thing you're timing is less than the roll time (4,294,967,296 microseconds, or 71 minutes, 34 seconds) you end up with an unsigned duration in microseconds.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;But make sure you always SUBTRACT the two values before comparing them to anything. If you write code like "if (nTime2 &amp;gt; nTime1 + 1000)" it won't work when it wraps (once every 71 minutes) and those bugs are very hard to track down.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="mce_paste_marker"&gt;You can have longer times by making the timer run slower, or measure finer times by making it run faster, remembering the maximum duration is now less.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="mce_paste_marker"&gt;&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="mce_paste_marker"&gt;I find that using 1MHz makes coding very easy when everything is in microseconds and there's no need to convert to some weird "tick value".&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="mce_paste_marker"&gt;&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="mce_paste_marker"&gt;Tom&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="mce_paste_marker"&gt;&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 13 Jun 2013 14:39:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/52259-counter/m-p/284345#M11979</guid>
      <dc:creator>TomE</dc:creator>
      <dc:date>2013-06-13T14:39:20Z</dc:date>
    </item>
    <item>
      <title>Re: 52259 counter</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/52259-counter/m-p/284346#M11980</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks Tom for the clarification.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;One more question, I was reading through the documentation MCF52259RM. The formula mentioned in section 26.4.2 about calculating the timeout values is little strange.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;For example in section 26.1.2, the maximum timeout mentioned is 109,951 seconds at 80 MHz (~31 hours).&amp;nbsp; &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;But if I use the formula in section 26.4.2, that is&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Timeout period = (1 ⁄ 80000000) × 16 × (0xFF + 1) × (0xFFFFFFFF + 1) = 219,902.3255552 seconds.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;System Frequency: 80 MHz&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;But if I divide the timeout period by 2, then i will get the mentioned maximum timeout period.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Once again thanks for the help.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 14 Jun 2013 12:33:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/52259-counter/m-p/284346#M11980</guid>
      <dc:creator>salman83</dc:creator>
      <dc:date>2013-06-14T12:33:26Z</dc:date>
    </item>
    <item>
      <title>Re: 52259 counter</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/52259-counter/m-p/284347#M11981</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Congratulations, you've found your very own bug in a manual!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I've just looked at the manual for the chip I work with, and the summary there says:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; Maximum timeout period of 219,902 seconds at 80 MHz (~61 hours)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Here's where you can start on your own Archaeology Expedition. Typing "Maximum timeout period of 109,951 seconds at 80 MHz" into Freescale's Search box finds the MCF52259 manual ONLY. Searching for "219,902" instead finds the MCF5329, 5282, 53017 and 5373 manuals. Cut/copy/paste/edit bug in copying chapters around. There's an Addendum to that manual, but it doesn't mention that one.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;You can get very long timeouts, but to make your code easier I'd recommend you divide by 1, 1 and 80 to get a 1us count. If you want a finer time period, the next useful&amp;nbsp; one is 1, 1 and 8 to get a 100ns clock.&lt;/P&gt;&lt;P&gt;.&lt;/P&gt;&lt;P&gt;Tom&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 14 Jun 2013 13:29:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/52259-counter/m-p/284347#M11981</guid>
      <dc:creator>TomE</dc:creator>
      <dc:date>2013-06-14T13:29:49Z</dc:date>
    </item>
  </channel>
</rss>