<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>ColdFire/68K Microcontrollers and Processors中的主题 Re: MCF51JE</title>
    <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/MCF51JE/m-p/272705#M11808</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Anything is possible. You could add an external Ethernet controller to the Mini-FlexBus. You might be able to find a USB-connected Ethernet adaptor. But you can't get Ethernet on that chip without external hardware. Any "non-standard" solution would make the software a lot harder to get working.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The only MCF51 chip with Ethernet is the MCF51CN128. That has half the FLASH, less than half the RAM and a different mix of peripherals to the one you're using (no USB for instance).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;You may need to step up to an MCF52 series chip.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Then you'll need a lot of extra software to get the network stack (e.g. FNET) unless you're already using something like MQX.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Tom&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Sat, 24 Aug 2013 00:58:19 GMT</pubDate>
    <dc:creator>TomE</dc:creator>
    <dc:date>2013-08-24T00:58:19Z</dc:date>
    <item>
      <title>MCF51JE</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/MCF51JE/m-p/272704#M11807</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I'm working in a project using MCF51JE256. Now i need send data through a ethernet port (RJ-45, socket conection),&amp;nbsp; is it possible do this using this MCU?&lt;/P&gt;&lt;P&gt;Thanks..&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Eduardo&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 23 Aug 2013 17:43:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/MCF51JE/m-p/272704#M11807</guid>
      <dc:creator>Vick</dc:creator>
      <dc:date>2013-08-23T17:43:40Z</dc:date>
    </item>
    <item>
      <title>Re: MCF51JE</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/MCF51JE/m-p/272705#M11808</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Anything is possible. You could add an external Ethernet controller to the Mini-FlexBus. You might be able to find a USB-connected Ethernet adaptor. But you can't get Ethernet on that chip without external hardware. Any "non-standard" solution would make the software a lot harder to get working.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The only MCF51 chip with Ethernet is the MCF51CN128. That has half the FLASH, less than half the RAM and a different mix of peripherals to the one you're using (no USB for instance).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;You may need to step up to an MCF52 series chip.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Then you'll need a lot of extra software to get the network stack (e.g. FNET) unless you're already using something like MQX.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Tom&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 24 Aug 2013 00:58:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/MCF51JE/m-p/272705#M11808</guid>
      <dc:creator>TomE</dc:creator>
      <dc:date>2013-08-24T00:58:19Z</dc:date>
    </item>
    <item>
      <title>Re: MCF51JE</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/MCF51JE/m-p/272706#M11809</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;You can do this with MCF51CN256 , I have implemented SPI to Ethernet bridge in my application using MCF51CN128.&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Chary&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 27 Aug 2013 11:01:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/MCF51JE/m-p/272706#M11809</guid>
      <dc:creator>chary</dc:creator>
      <dc:date>2013-08-27T11:01:24Z</dc:date>
    </item>
  </channel>
</rss>