<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>ColdFire/68K Microcontrollers and ProcessorsのトピックColdfire V4 Embedded Proc MCF5445X system power to headers check</title>
    <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/Coldfire-V4-Embedded-Proc-MCF5445X-system-power-to-headers-check/m-p/272331#M11806</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;SPAN style="font-size: 10pt;"&gt;Good morning. I'm new to this to let me know if there is a better way to go about this, but I am on a deadline so I am jumping in.&amp;nbsp; I am using the Colfire V4 Embedded Processor MCF5445EVB System with MCF54455 32-bit Coldfire uProc.&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 10pt;"&gt;&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 10pt;"&gt;I recently disconnected the power on/of switch to the 3 headers it goes to.&amp;nbsp; Although reconnected, the system is not turning on.&amp;nbsp; I looked through the documentation and have it set up so that:&lt;BR /&gt; &lt;BR /&gt; There are 3 sets of 2 wired each that go to headers.&lt;BR /&gt; &lt;BR /&gt; For the red/white pair (labeled 'HDD LED'): connected to header 9, with the red wire connected to pin 1, and the white wire connected to pin 2.&lt;BR /&gt; &lt;BR /&gt; For the orange/white pair (labeled 'POWER SW'): connected to header 15, with the orange wire connected to pin 1, and the white wire connected to pin 2.&lt;BR /&gt; &lt;BR /&gt; For the green/white pair (labeled '+P LED' and '-P LED' respectively): connected to header 16, with the green wire connected to pin 1, and the white wire connected to pin 2.&lt;BR /&gt; &lt;BR /&gt; Would you please tell me if these are the correct connections?&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 19 Dec 2013 15:57:24 GMT</pubDate>
    <dc:creator>kendanewton</dc:creator>
    <dc:date>2013-12-19T15:57:24Z</dc:date>
    <item>
      <title>Coldfire V4 Embedded Proc MCF5445X system power to headers check</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/Coldfire-V4-Embedded-Proc-MCF5445X-system-power-to-headers-check/m-p/272331#M11806</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;SPAN style="font-size: 10pt;"&gt;Good morning. I'm new to this to let me know if there is a better way to go about this, but I am on a deadline so I am jumping in.&amp;nbsp; I am using the Colfire V4 Embedded Processor MCF5445EVB System with MCF54455 32-bit Coldfire uProc.&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 10pt;"&gt;&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 10pt;"&gt;I recently disconnected the power on/of switch to the 3 headers it goes to.&amp;nbsp; Although reconnected, the system is not turning on.&amp;nbsp; I looked through the documentation and have it set up so that:&lt;BR /&gt; &lt;BR /&gt; There are 3 sets of 2 wired each that go to headers.&lt;BR /&gt; &lt;BR /&gt; For the red/white pair (labeled 'HDD LED'): connected to header 9, with the red wire connected to pin 1, and the white wire connected to pin 2.&lt;BR /&gt; &lt;BR /&gt; For the orange/white pair (labeled 'POWER SW'): connected to header 15, with the orange wire connected to pin 1, and the white wire connected to pin 2.&lt;BR /&gt; &lt;BR /&gt; For the green/white pair (labeled '+P LED' and '-P LED' respectively): connected to header 16, with the green wire connected to pin 1, and the white wire connected to pin 2.&lt;BR /&gt; &lt;BR /&gt; Would you please tell me if these are the correct connections?&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 19 Dec 2013 15:57:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/Coldfire-V4-Embedded-Proc-MCF5445X-system-power-to-headers-check/m-p/272331#M11806</guid>
      <dc:creator>kendanewton</dc:creator>
      <dc:date>2013-12-19T15:57:24Z</dc:date>
    </item>
  </channel>
</rss>