<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: M52235EVB GPT and PWM usage, header missing in ColdFire/68K Microcontrollers and Processors</title>
    <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/M52235EVB-GPT-and-PWM-usage-header-missing/m-p/124513#M118</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;&lt;/DIV&gt;&lt;P&gt;We will correct the missing header.&lt;/P&gt;&lt;P&gt;As long as the port assignment register selects the correct source to drive the pin, using the timers for software TIC counts, etc is fine. The PWM can do this as well but without a pin to control, I see no point.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 14 Aug 2006 23:10:40 GMT</pubDate>
    <dc:creator>DrSeuss</dc:creator>
    <dc:date>2006-08-14T23:10:40Z</dc:date>
    <item>
      <title>M52235EVB GPT and PWM usage, header missing</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/M52235EVB-GPT-and-PWM-usage-header-missing/m-p/124512#M117</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;Is there a reason mcf5223_gpt.h is not included in mcf5223.h?&amp;nbsp; I assumed it should be there, added it, and proceeded to use MCF_GPT_&amp;nbsp; assignments to gain access to GPT0.&amp;nbsp; No Joy.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;Maybe related, I am configuring PMW1 and PMW3 to generate signals.&amp;nbsp; I am getting these signals using MCF_GPIO_ assignmets.&amp;nbsp; A specific concern is the use of PWM (pin&amp;nbsp;99 PWM1,pin 100 PWM3) and Timers (pin 107, GPT0) at the same time.&amp;nbsp; I used the primary function setting for pin assignment.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;MCF_GPIO_PTDPAR = 0&lt;BR /&gt;&amp;nbsp;| MCF_GPIO_PTDPAR_PTDPAR0&lt;BR /&gt;&amp;nbsp;| MCF_GPIO_PTDPAR_PTDPAR1&lt;BR /&gt;&amp;nbsp;| MCF_GPIO_PTDPAR_PTDPAR2&lt;BR /&gt;&amp;nbsp;| MCF_GPIO_PTDPAR_PTDPAR3; //set for primary function&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;Is this proper to use both PWM1, PWM3, and GPT0 ?&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;I appologize in advance since I am totally new to embedded programming.&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 19 Jul 2006 21:08:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/M52235EVB-GPT-and-PWM-usage-header-missing/m-p/124512#M117</guid>
      <dc:creator>paynete</dc:creator>
      <dc:date>2006-07-19T21:08:29Z</dc:date>
    </item>
    <item>
      <title>Re: M52235EVB GPT and PWM usage, header missing</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/M52235EVB-GPT-and-PWM-usage-header-missing/m-p/124513#M118</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;&lt;/DIV&gt;&lt;P&gt;We will correct the missing header.&lt;/P&gt;&lt;P&gt;As long as the port assignment register selects the correct source to drive the pin, using the timers for software TIC counts, etc is fine. The PWM can do this as well but without a pin to control, I see no point.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 14 Aug 2006 23:10:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/M52235EVB-GPT-and-PWM-usage-header-missing/m-p/124513#M118</guid>
      <dc:creator>DrSeuss</dc:creator>
      <dc:date>2006-08-14T23:10:40Z</dc:date>
    </item>
  </channel>
</rss>