<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Having trouble decoding memory on 52277 using CW10.3 in ColdFire/68K Microcontrollers and Processors</title>
    <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/Having-trouble-decoding-memory-on-52277-using-CW10-3/m-p/266788#M11749</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Using the debugger, I cannot correctly decode an external block of memory. When I create my Flash version and run standalone, everything works fine. The Memory Configuration file appears to have correct mapping ranges; however, when I read back "reserved" ranges the data is not 0xbaba as specified, so I'm a little skeptical. This is a stable project imported from CW7.1.&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Update: The memory configuration file I am using was generated from an older version of CW10. I now get the following message when creating Processor Expert code:&lt;/P&gt;&lt;P&gt;&lt;EM&gt;Hint: The debugger file Project_Settings\Debugger\INTERNAL.xml can't be generated because an internal or an external FLASH doesn't exist or isn't configured.&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;Not sure how to rectify this as there are no Flash components available to Processor Expert.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 15 Apr 2013 12:58:14 GMT</pubDate>
    <dc:creator>Ainslie</dc:creator>
    <dc:date>2013-04-15T12:58:14Z</dc:date>
    <item>
      <title>Having trouble decoding memory on 52277 using CW10.3</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/Having-trouble-decoding-memory-on-52277-using-CW10-3/m-p/266788#M11749</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Using the debugger, I cannot correctly decode an external block of memory. When I create my Flash version and run standalone, everything works fine. The Memory Configuration file appears to have correct mapping ranges; however, when I read back "reserved" ranges the data is not 0xbaba as specified, so I'm a little skeptical. This is a stable project imported from CW7.1.&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Update: The memory configuration file I am using was generated from an older version of CW10. I now get the following message when creating Processor Expert code:&lt;/P&gt;&lt;P&gt;&lt;EM&gt;Hint: The debugger file Project_Settings\Debugger\INTERNAL.xml can't be generated because an internal or an external FLASH doesn't exist or isn't configured.&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;Not sure how to rectify this as there are no Flash components available to Processor Expert.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 15 Apr 2013 12:58:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/Having-trouble-decoding-memory-on-52277-using-CW10-3/m-p/266788#M11749</guid>
      <dc:creator>Ainslie</dc:creator>
      <dc:date>2013-04-15T12:58:14Z</dc:date>
    </item>
  </channel>
</rss>