<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>ColdFire/68K Microcontrollers and ProcessorsのトピックUSB Buffer Descriptor</title>
    <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/USB-Buffer-Descriptor/m-p/259318#M11677</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I have a question regarding usb buffer descriptor. I setup one bulk IN endpoint (with max. packet size 64 bytes) on my MCF52259. Now I want to send a stream of data through it. According to USB specs, DATA0/DATA1 are used for synchronization purposes only. Now, if I have set two buffers simultaneously in EVEN and ODD buffer descriptors for better throughput. With even buffer descriptor set to DATA0 and odd buffer descriptor set to DATA1.&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;If an error comes up on DATA0 or I have to send it again, then obviously I need to send it on DATA1. Then my question is that how would I maximize the throughput as I can't send the second buffer as the first one is not completed.&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 10pt; line-height: 1.5em;"&gt;Regards.&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 08 Jul 2013 12:40:06 GMT</pubDate>
    <dc:creator>salman83</dc:creator>
    <dc:date>2013-07-08T12:40:06Z</dc:date>
    <item>
      <title>USB Buffer Descriptor</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/USB-Buffer-Descriptor/m-p/259318#M11677</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I have a question regarding usb buffer descriptor. I setup one bulk IN endpoint (with max. packet size 64 bytes) on my MCF52259. Now I want to send a stream of data through it. According to USB specs, DATA0/DATA1 are used for synchronization purposes only. Now, if I have set two buffers simultaneously in EVEN and ODD buffer descriptors for better throughput. With even buffer descriptor set to DATA0 and odd buffer descriptor set to DATA1.&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;If an error comes up on DATA0 or I have to send it again, then obviously I need to send it on DATA1. Then my question is that how would I maximize the throughput as I can't send the second buffer as the first one is not completed.&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 10pt; line-height: 1.5em;"&gt;Regards.&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 08 Jul 2013 12:40:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/USB-Buffer-Descriptor/m-p/259318#M11677</guid>
      <dc:creator>salman83</dc:creator>
      <dc:date>2013-07-08T12:40:06Z</dc:date>
    </item>
  </channel>
</rss>