<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>ColdFire/68K Microcontrollers and Processorsのトピックan2295 serial boot loader on MCF52259</title>
    <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/an2295-serial-boot-loader-on-MCF52259/m-p/248489#M11545</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Good day, I download app note sw and has folder for MCF52259, but unable to get working. Board is same as MCF52259 demo. Want to use uart0. I have the codewarrior 10.2 and the classic 7.2. Both versions the import is not clean, There are missing MCF52259_Internal_flash.cfg and MCF52259_Internal_flash.mem&lt;/P&gt;&lt;P&gt;I dont know if that the problem. It seems to compile ok.&amp;nbsp; I've tried generating new target and launch configurations in 10.2 but getting lost.&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I know the board works fine because I have an MQX project that runs on it. I want to be able to load up the MQX proj via serial fiber link since bdm port not easily accessible.&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;thx&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 01 Jul 2013 18:55:11 GMT</pubDate>
    <dc:creator>shenlung</dc:creator>
    <dc:date>2013-07-01T18:55:11Z</dc:date>
    <item>
      <title>an2295 serial boot loader on MCF52259</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/an2295-serial-boot-loader-on-MCF52259/m-p/248489#M11545</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Good day, I download app note sw and has folder for MCF52259, but unable to get working. Board is same as MCF52259 demo. Want to use uart0. I have the codewarrior 10.2 and the classic 7.2. Both versions the import is not clean, There are missing MCF52259_Internal_flash.cfg and MCF52259_Internal_flash.mem&lt;/P&gt;&lt;P&gt;I dont know if that the problem. It seems to compile ok.&amp;nbsp; I've tried generating new target and launch configurations in 10.2 but getting lost.&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I know the board works fine because I have an MQX project that runs on it. I want to be able to load up the MQX proj via serial fiber link since bdm port not easily accessible.&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;thx&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 01 Jul 2013 18:55:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/an2295-serial-boot-loader-on-MCF52259/m-p/248489#M11545</guid>
      <dc:creator>shenlung</dc:creator>
      <dc:date>2013-07-01T18:55:11Z</dc:date>
    </item>
  </channel>
</rss>