<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>ColdFire/68K Microcontrollers and Processors中的主题 M52233DEMO UART problem</title>
    <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/M52233DEMO-UART-problem/m-p/247043#M11521</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I'm having a problem with displaying a simple string "Hello World" to the terminal using the M52233DEMO board via serial. The output consists of some gibberish ASCII characters. I tried various baud rates and I'm confused as to why the string is not displayed properly. Any help would be greatly appreciated. Thank you :-)&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Original Attachment has been moved to: &lt;A _jive_internal="true" href="https://community.nxp.com/docs/DOC-337785"&gt;StringTest.zip&lt;/A&gt;&lt;/STRONG&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 30 Oct 2013 13:13:48 GMT</pubDate>
    <dc:creator>admin</dc:creator>
    <dc:date>2013-10-30T13:13:48Z</dc:date>
    <item>
      <title>M52233DEMO UART problem</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/M52233DEMO-UART-problem/m-p/247043#M11521</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I'm having a problem with displaying a simple string "Hello World" to the terminal using the M52233DEMO board via serial. The output consists of some gibberish ASCII characters. I tried various baud rates and I'm confused as to why the string is not displayed properly. Any help would be greatly appreciated. Thank you :-)&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Original Attachment has been moved to: &lt;A _jive_internal="true" href="https://community.nxp.com/docs/DOC-337785"&gt;StringTest.zip&lt;/A&gt;&lt;/STRONG&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 30 Oct 2013 13:13:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/M52233DEMO-UART-problem/m-p/247043#M11521</guid>
      <dc:creator>admin</dc:creator>
      <dc:date>2013-10-30T13:13:48Z</dc:date>
    </item>
    <item>
      <title>Re: M52233DEMO UART problem</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/M52233DEMO-UART-problem/m-p/247044#M11522</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;It is most likely to be the baud rate that is wrong. The most likely cause of that is that the system clock isn't running at the rate you think it is, or you've missed a divider in the chain, or you've got an "off by one" bug where you program a register with "N" to get a division ration of "N+1" or "N-1" and you've missed that.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The standard why-would-you-do-anything-else way of fixing this is to use an oscilloscope on the pin and MEASURE what it is actually doing. That will tell you what factor you're out by, either *2 or /2, or 15/16 and that will lead you to the programming problem.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If you don't have one, then find a friend or school that has and go there.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If you still can't do that, write some code to program a timer to flash a LED at a rate you can count or measure on a stopwatch. That may show you the problem.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Before that you should read all the relevant sections of the CPU Reference Manual and cross-check with all the generated code and work out the timing chain yourself.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Tom&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 31 Oct 2013 22:10:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/M52233DEMO-UART-problem/m-p/247044#M11522</guid>
      <dc:creator>TomE</dc:creator>
      <dc:date>2013-10-31T22:10:40Z</dc:date>
    </item>
    <item>
      <title>Re: M52233DEMO UART problem</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/M52233DEMO-UART-problem/m-p/247045#M11523</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I'm trying to create a project in CW 10.5 eclipse under windows 8 74bit.&lt;/P&gt;&lt;P&gt;I see from the screenshot attached that you use CW eclipse for this board...&lt;/P&gt;&lt;P&gt;Could you please post a basic project for the M52233DEMO board in CW 10.5 or a link where to download a basic sample for this board for CW eclipse?&lt;/P&gt;&lt;P&gt;I received the board only with samples in CW 7.2 which is not suitable for win 64bit.&lt;/P&gt;&lt;P&gt;thank you&lt;/P&gt;&lt;P&gt;Maurice&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 19 Nov 2013 11:04:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/M52233DEMO-UART-problem/m-p/247045#M11523</guid>
      <dc:creator>robit</dc:creator>
      <dc:date>2013-11-19T11:04:07Z</dc:date>
    </item>
  </channel>
</rss>