<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Is the InterNiche’s ColdFire TCP/IP Stack compatibe with the MCF5225X? in ColdFire/68K Microcontrollers and Processors</title>
    <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/Is-the-InterNiche-s-ColdFire-TCP-IP-Stack-compatibe-with-the/m-p/233786#M11340</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I was wondering if the TCP/IP stack is compatible with the Coldfire V2 MCF5225X family because I have the MCF5225X Tower Board and I don't want to use the MQX because it's lack of functionality, particularly regarding peripheral drivers, and I want to use processor expert to develop my projects.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you!!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 22 Jan 2013 22:20:44 GMT</pubDate>
    <dc:creator>m4l490n</dc:creator>
    <dc:date>2013-01-22T22:20:44Z</dc:date>
    <item>
      <title>Is the InterNiche’s ColdFire TCP/IP Stack compatibe with the MCF5225X?</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/Is-the-InterNiche-s-ColdFire-TCP-IP-Stack-compatibe-with-the/m-p/233786#M11340</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I was wondering if the TCP/IP stack is compatible with the Coldfire V2 MCF5225X family because I have the MCF5225X Tower Board and I don't want to use the MQX because it's lack of functionality, particularly regarding peripheral drivers, and I want to use processor expert to develop my projects.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you!!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 22 Jan 2013 22:20:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/Is-the-InterNiche-s-ColdFire-TCP-IP-Stack-compatibe-with-the/m-p/233786#M11340</guid>
      <dc:creator>m4l490n</dc:creator>
      <dc:date>2013-01-22T22:20:44Z</dc:date>
    </item>
    <item>
      <title>Re: Is the InterNiche’s ColdFire TCP/IP Stack compatibe with the MCF5225X?</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/Is-the-InterNiche-s-ColdFire-TCP-IP-Stack-compatibe-with-the/m-p/233787#M11341</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Manuel,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Just in case, if you have an issue with InterNiche &lt;SPAN style="font-family: 'Helvetica Neue', Helvetica, Arial, 'Lucida Grande', sans-serif; background-color: #ffffff;"&gt;"MCF5225X family" support&lt;/SPAN&gt;, you can look at FNET Embedded TCP/IP stack &lt;A href="http://fnet.sourceforge.net/"&gt;http://fnet.sourceforge.net&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;Andrey&lt;/P&gt;&lt;P&gt;&lt;SPAN class="mce_paste_marker"&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 23 Jan 2013 08:44:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/Is-the-InterNiche-s-ColdFire-TCP-IP-Stack-compatibe-with-the/m-p/233787#M11341</guid>
      <dc:creator>butok</dc:creator>
      <dc:date>2013-01-23T08:44:37Z</dc:date>
    </item>
  </channel>
</rss>