<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>ColdFire/68K Microcontrollers and ProcessorsのトピックRe: Determining IRQ Source</title>
    <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/Determining-IRQ-Source/m-p/225404#M11283</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;The standard method for common interrupt service routines (like when you have multiple serial ports using common code) is to have separate service routines with different vectors, but have them load up a register with a unique number (the vector index usually) and then branch to a common service routine. In your case that's where you set the one breakpoint, and then examine the register (or variable where the routine saves the number) to see which one did it. Or you can have the individual routines simply CALL the common function, and when in there you just display a stack-trace to see which service routine called the common one.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Tom&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 15 Jan 2013 22:36:14 GMT</pubDate>
    <dc:creator>TomE</dc:creator>
    <dc:date>2013-01-15T22:36:14Z</dc:date>
    <item>
      <title>Determining IRQ Source</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/Determining-IRQ-Source/m-p/225400#M11279</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;My ColdFire application is jumping into the default ISR.&amp;nbsp; (All "unused" ISRs are mapped to a default ISR.)&amp;nbsp; How do I determine the source of the interrupt/exception?&amp;nbsp; I am using MCF51JM128 and CodeWarrior 10.2.&amp;nbsp; Thanks.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 15 Jan 2013 14:58:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/Determining-IRQ-Source/m-p/225400#M11279</guid>
      <dc:creator>jimfell</dc:creator>
      <dc:date>2013-01-15T14:58:55Z</dc:date>
    </item>
    <item>
      <title>Re: Determining IRQ Source</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/Determining-IRQ-Source/m-p/225401#M11280</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;It is simple. For debugging purposes you can make each vector-N pointing to empty ISR_n.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 15 Jan 2013 18:30:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/Determining-IRQ-Source/m-p/225401#M11280</guid>
      <dc:creator>kef</dc:creator>
      <dc:date>2013-01-15T18:30:17Z</dc:date>
    </item>
    <item>
      <title>Re: Determining IRQ Source</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/Determining-IRQ-Source/m-p/225402#M11281</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I need to know what triggered the ISR, after getting into the ISR.&amp;nbsp; There are not enough breakpoints available to be able to set a breakpoint in every possible ISR.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 15 Jan 2013 18:55:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/Determining-IRQ-Source/m-p/225402#M11281</guid>
      <dc:creator>jimfell</dc:creator>
      <dc:date>2013-01-15T18:55:06Z</dc:date>
    </item>
    <item>
      <title>Re: Determining IRQ Source</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/Determining-IRQ-Source/m-p/225403#M11282</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Then instead of empty ISR's you need ISR with for(;;){} inside. In case watchdog is enabled, make these forewer loops resetting watchdog timer. Then just halt timer to see which ISR is running. LED could be used to signal when ISR is called.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 15 Jan 2013 19:13:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/Determining-IRQ-Source/m-p/225403#M11282</guid>
      <dc:creator>kef</dc:creator>
      <dc:date>2013-01-15T19:13:03Z</dc:date>
    </item>
    <item>
      <title>Re: Determining IRQ Source</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/Determining-IRQ-Source/m-p/225404#M11283</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;The standard method for common interrupt service routines (like when you have multiple serial ports using common code) is to have separate service routines with different vectors, but have them load up a register with a unique number (the vector index usually) and then branch to a common service routine. In your case that's where you set the one breakpoint, and then examine the register (or variable where the routine saves the number) to see which one did it. Or you can have the individual routines simply CALL the common function, and when in there you just display a stack-trace to see which service routine called the common one.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Tom&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 15 Jan 2013 22:36:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/Determining-IRQ-Source/m-p/225404#M11283</guid>
      <dc:creator>TomE</dc:creator>
      <dc:date>2013-01-15T22:36:14Z</dc:date>
    </item>
  </channel>
</rss>