<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>ColdFire/68K Microcontrollers and ProcessorsのトピックCAN interface on MCF51AC256</title>
    <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/CAN-interface-on-MCF51AC256/m-p/218403#M11079</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;hi&lt;/P&gt;&lt;P&gt;is there any Application Note about&amp;nbsp; CAN interface of the MCF51AC256 microcontroller ?&lt;BR /&gt;&lt;BR /&gt;Just to get started about the CAN AREAD interface: i need a piece of code which is able to initialize the can with a proper baud rate, and then i need to be able o send and get messages without using interrupts&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;any good code to be started with ?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 30 Jun 2011 04:02:53 GMT</pubDate>
    <dc:creator>flameman</dc:creator>
    <dc:date>2011-06-30T04:02:53Z</dc:date>
    <item>
      <title>CAN interface on MCF51AC256</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/CAN-interface-on-MCF51AC256/m-p/218403#M11079</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;hi&lt;/P&gt;&lt;P&gt;is there any Application Note about&amp;nbsp; CAN interface of the MCF51AC256 microcontroller ?&lt;BR /&gt;&lt;BR /&gt;Just to get started about the CAN AREAD interface: i need a piece of code which is able to initialize the can with a proper baud rate, and then i need to be able o send and get messages without using interrupts&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;any good code to be started with ?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 30 Jun 2011 04:02:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/CAN-interface-on-MCF51AC256/m-p/218403#M11079</guid>
      <dc:creator>flameman</dc:creator>
      <dc:date>2011-06-30T04:02:53Z</dc:date>
    </item>
    <item>
      <title>Re: CAN interface on MCF51AC256</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/CAN-interface-on-MCF51AC256/m-p/218404#M11080</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;If you go here:&lt;/P&gt;&lt;P&gt;&lt;A href="http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=MCF51AC&amp;amp;fpsp=1&amp;amp;tab=Design_Tools_Tab" rel="nofollow" target="_blank"&gt;MC51AC Tools&lt;/A&gt;&lt;/P&gt;&lt;P&gt;And look under "drivers" there is sample CAN code....&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 30 Jun 2011 04:08:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/CAN-interface-on-MCF51AC256/m-p/218404#M11080</guid>
      <dc:creator>JimDon</dc:creator>
      <dc:date>2011-06-30T04:08:39Z</dc:date>
    </item>
    <item>
      <title>Re: CAN interface on MCF51AC256</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/CAN-interface-on-MCF51AC256/m-p/218405#M11081</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;hi&lt;BR /&gt;i need a bit or more support about compiling the can driver&lt;BR /&gt;i am using codewarrior v 5.8.0&lt;BR /&gt;which is telling me&amp;nbsp; that &amp;lt;MCF51AC256.h&amp;gt; is missing&lt;BR /&gt;&lt;BR /&gt;if i try to use #include &amp;lt;MCF51AC256a.h&amp;gt;&lt;BR /&gt;i have issue with msCANdrv.c because same can registers are not defined&lt;BR /&gt;&lt;BR /&gt;could you help me ?&lt;BR /&gt;﻿&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 01 Jul 2011 16:40:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/CAN-interface-on-MCF51AC256/m-p/218405#M11081</guid>
      <dc:creator>flameman</dc:creator>
      <dc:date>2011-07-01T16:40:53Z</dc:date>
    </item>
    <item>
      <title>Re: CAN interface on MCF51AC256</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/CAN-interface-on-MCF51AC256/m-p/218406#M11082</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;What CAN registers are missing?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;5.8.0 is just IDE version. In IDE about box you should click Installed Products to see what development studio you are using. Latest classic CW for MCUs V6.3 comes with 5.9.0 IDE. Since 51AC are quite new, maybe there was some changes in header files.&amp;nbsp;It should be mentioned in CAN driver what CW version it is compatible with.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 01 Jul 2011 22:39:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/CAN-interface-on-MCF51AC256/m-p/218406#M11082</guid>
      <dc:creator>kef</dc:creator>
      <dc:date>2011-07-01T22:39:48Z</dc:date>
    </item>
  </channel>
</rss>