<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>ColdFire/68K Microcontrollers and ProcessorsのトピックRe: MCF5213 UART</title>
    <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/MCF5213-UART/m-p/132329#M1093</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I didn't find any real good solution, if you can't manage RTS by UART functionality, you can start a timer with the amount of time left for the last byte, or poll the TEMP flags. You can also, (if the driver receiver is always enable in RS485 case) waiting for receiving emitted bytes, it's not a nice solution but it should work.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Emmanuel&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 04 Sep 2009 17:16:49 GMT</pubDate>
    <dc:creator>Nouchi</dc:creator>
    <dc:date>2009-09-04T17:16:49Z</dc:date>
    <item>
      <title>MCF5213 UART</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/MCF5213-UART/m-p/132325#M1089</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt; &lt;/DIV&gt;&lt;SPAN&gt;Hi,&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Why they don't let me choose TX interrupt source between TXEMPTY flag and TXRDY flag?&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;You can choose RXRDY or FIFO full interrupt source for the receiver......&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;I need to disable RS485 driver at the end of frame with a low level, so if I use RTS pin with transmitter, I have to add an inverter gate in my design &lt;/SPAN&gt;&lt;SPAN aria-label="Sad" class="emoticon_sad emoticon-inline" style="height:16px;width:16px;"&gt;&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Emmanuel&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;DIV&gt; &lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 05 Oct 2006 21:06:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/MCF5213-UART/m-p/132325#M1089</guid>
      <dc:creator>Nouchi</dc:creator>
      <dc:date>2006-10-05T21:06:50Z</dc:date>
    </item>
    <item>
      <title>Re: MCF5213 UART</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/MCF5213-UART/m-p/132326#M1090</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;Hi Emmanuel&lt;BR /&gt;&lt;BR /&gt;Did you mamnage to sort out this problem in firmware or did you have to resort to an inverter?&lt;BR /&gt;&lt;BR /&gt;Cheers&lt;BR /&gt;&lt;DIV&gt;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 25 May 2007 18:26:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/MCF5213-UART/m-p/132326#M1090</guid>
      <dc:creator>wyliek</dc:creator>
      <dc:date>2007-05-25T18:26:52Z</dc:date>
    </item>
    <item>
      <title>Re: MCF5213 UART</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/MCF5213-UART/m-p/132327#M1091</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;&lt;/DIV&gt;Hi,&lt;BR /&gt;&lt;BR /&gt;No, after all, I managed RTS by hand in the Firmware (RTS as an IO port &lt;SPAN&gt;&lt;IMG alt=":smileysad:" class="emoticon emoticon-smileysad" id="smileysad" src="http://freescale.i.lithium.com/i/smilies/16x16_smiley-sad.gif" title="Smiley Sad" /&gt;&lt;/SPAN&gt;)&lt;BR /&gt;&lt;DIV&gt;&lt;/DIV&gt;&lt;BR /&gt;&lt;BR /&gt;Emmanuel&lt;BR /&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 28 May 2007 13:10:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/MCF5213-UART/m-p/132327#M1091</guid>
      <dc:creator>Nouchi</dc:creator>
      <dc:date>2007-05-28T13:10:57Z</dc:date>
    </item>
    <item>
      <title>Re: MCF5213 UART</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/MCF5213-UART/m-p/132328#M1092</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello, I am having the same problem. How did you manage it by hand in firmware without an interrupt? Did you have to poll to see when frame was complete?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thank you,&lt;/P&gt;&lt;P&gt;Randy Kelso&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 27 Aug 2009 06:44:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/MCF5213-UART/m-p/132328#M1092</guid>
      <dc:creator>rsk2</dc:creator>
      <dc:date>2009-08-27T06:44:09Z</dc:date>
    </item>
    <item>
      <title>Re: MCF5213 UART</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/MCF5213-UART/m-p/132329#M1093</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I didn't find any real good solution, if you can't manage RTS by UART functionality, you can start a timer with the amount of time left for the last byte, or poll the TEMP flags. You can also, (if the driver receiver is always enable in RS485 case) waiting for receiving emitted bytes, it's not a nice solution but it should work.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Emmanuel&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 04 Sep 2009 17:16:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/MCF5213-UART/m-p/132329#M1093</guid>
      <dc:creator>Nouchi</dc:creator>
      <dc:date>2009-09-04T17:16:49Z</dc:date>
    </item>
  </channel>
</rss>