<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>ColdFire/68K Microcontrollers and Processors中的主题 Re: Finding the right processor</title>
    <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/Finding-the-right-processor/m-p/214512#M10762</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks for that scifi,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;In regards to the limitations to choice if I do not&amp;nbsp;BGA, is the overall direction of higher end 32bit processors going to be BGA?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I did speak to the manufacturer and they indicated a preference towards traditional as the costs are higher and debugging is more difficult.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Does using BGA force the design board to use more than 2 layer? Or is 2 layer design still possible?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;How would you diagnose problems on a BGA design if all the pins are hidden?&lt;/P&gt;&lt;P&gt;My learing curve is steep for sure..&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Jamo&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 27 Jul 2010 06:01:27 GMT</pubDate>
    <dc:creator>Jamo</dc:creator>
    <dc:date>2010-07-27T06:01:27Z</dc:date>
    <item>
      <title>Finding the right processor</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/Finding-the-right-processor/m-p/214510#M10760</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I am still fairly new at hardware design.&amp;nbsp; I have been browsing through the freescale range and getting a bit overwhelmed.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Basically I am looking for the right processor to perform the following basic functions:&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Specs&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;## Dual Ethernet (10/100 is fine) - Looking for somehting that can send a packet between ethernet ports at a speed of at least 1Mbps.&lt;/P&gt;&lt;P&gt;##&amp;nbsp; 2 x Serial Ports&lt;/P&gt;&lt;P&gt;##&amp;nbsp; 1&amp;nbsp;x port to talk to an SD card&lt;/P&gt;&lt;P&gt;##&amp;nbsp; at least 20 General Purpose IO (GPIO). Need to drive around 12LEDS&lt;/P&gt;&lt;P&gt;##&amp;nbsp; Sufficient processing power to perform a specific function. This processing function is to receive a JPG&amp;nbsp;image of around 50KB from one ethernet port, shrink the image to 5KB and send it quicky out the other ethernet port.&lt;/P&gt;&lt;P&gt;## Capacity to add some memory&lt;/P&gt;&lt;P&gt;##&amp;nbsp; Packaging to not be BGA (as manufacturing is more expensive)&lt;/P&gt;&lt;P&gt;## Pricing range for processor is $40USD&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I have plenty of room on the PCB so there is not a space issue&lt;/P&gt;&lt;P&gt;Power is not an issue either&lt;/P&gt;&lt;P&gt;I would be&amp;nbsp;open to a&amp;nbsp;processor at a different price bracket if there were solid benefits.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;My other questions are&lt;/STRONG&gt;:&lt;/P&gt;&lt;P&gt;How can I tell how fast the ethernet ports can work?&amp;nbsp;&lt;/P&gt;&lt;P&gt;Is it dependant on the processor speed of the micro?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;If anyone can steer me in the right direction, it would be much appreciated&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Jamo&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 23 Jul 2010 13:04:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/Finding-the-right-processor/m-p/214510#M10760</guid>
      <dc:creator>Jamo</dc:creator>
      <dc:date>2010-07-23T13:04:07Z</dc:date>
    </item>
    <item>
      <title>Re: Finding the right processor</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/Finding-the-right-processor/m-p/214511#M10761</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Jamo,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I think the requirement to have two Ethernet interfaces and a QFP package will limit your search very quickly. Try searching "dual ethernet" on this site. One of the top results is MCF5301x:&lt;/P&gt;&lt;P&gt;&lt;A href="http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=MCF5301x&amp;amp;fsrch=1" rel="nofollow" target="_self"&gt;MCF5301x&lt;/A&gt;&lt;/P&gt;&lt;P&gt;And I wouldn't worry about the speed of Ethernet ports. 1 Mbps is very slow, you will struggle to find an MCU that cannot support this.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;- mike&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 23 Jul 2010 18:12:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/Finding-the-right-processor/m-p/214511#M10761</guid>
      <dc:creator>scifi</dc:creator>
      <dc:date>2010-07-23T18:12:03Z</dc:date>
    </item>
    <item>
      <title>Re: Finding the right processor</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/Finding-the-right-processor/m-p/214512#M10762</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks for that scifi,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;In regards to the limitations to choice if I do not&amp;nbsp;BGA, is the overall direction of higher end 32bit processors going to be BGA?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I did speak to the manufacturer and they indicated a preference towards traditional as the costs are higher and debugging is more difficult.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Does using BGA force the design board to use more than 2 layer? Or is 2 layer design still possible?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;How would you diagnose problems on a BGA design if all the pins are hidden?&lt;/P&gt;&lt;P&gt;My learing curve is steep for sure..&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Jamo&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 27 Jul 2010 06:01:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/Finding-the-right-processor/m-p/214512#M10762</guid>
      <dc:creator>Jamo</dc:creator>
      <dc:date>2010-07-27T06:01:27Z</dc:date>
    </item>
  </channel>
</rss>