<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>ColdFire/68K Microcontrollers and ProcessorsのトピックRe: Linux Booting Issue in M52277EVB board</title>
    <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/Linux-Booting-Issue-in-M52277EVB-board/m-p/214118#M10702</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;If this truly a temperature problem, then there's something wrong with the board. I'd suggest you get it exchanged.&lt;BR /&gt;&lt;BR /&gt;---Tom&lt;BR /&gt;&lt;BR /&gt;&lt;DIV&gt;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 07 Jan 2009 23:55:36 GMT</pubDate>
    <dc:creator>J2MEJediMaster</dc:creator>
    <dc:date>2009-01-07T23:55:36Z</dc:date>
    <item>
      <title>Linux Booting Issue in M52277EVB board</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/Linux-Booting-Issue-in-M52277EVB-board/m-p/214117#M10701</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt; &lt;/DIV&gt;&lt;DIV&gt;&lt;P&gt;&lt;SPAN style=": ; font-size: 4;"&gt;Hi,&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style=": ; font-size: 4;"&gt;We are working with Freescale Coldfire processor MCF52277 based&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style=": ; font-size: 4;"&gt;evaluation board M52277EVB.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;SPAN style=": ; font-size: 4;"&gt;This board is not booting most of the time. We are using the Freescale&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style=": ; font-size: 4;"&gt;Linux BSPs to load the U-Boot loader and the Linux Kernel.&amp;nbsp; We are using&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style=": ; font-size: 4;"&gt;the same flash partition which comes along with BSP without modifying a&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style=": ; font-size: 4;"&gt;single bit. Even we are not modified the Linux kernel also. This is the&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style=": ; font-size: 4;"&gt;background information.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;SPAN style=": ; font-size: 4;"&gt;Problem:&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;SPAN style=": ; font-size: 4;"&gt;This M52277EVB board will not boot most of the time in the morning time&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style=": ; font-size: 4;"&gt;when we first tried to start.&amp;nbsp; It loads the U-Boot loader and&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style=": ; font-size: 4;"&gt;un-compress the Linux kernel and there it halts.&amp;nbsp; After loading the&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style=": ; font-size: 4;"&gt;U-boot loader, we are able to execute the U-boot commands. We had tried&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style=": ; font-size: 4;"&gt;to boot manually by giving "boot" command also in the U-boot prompt.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style=": ; font-size: 4;"&gt;Then also it will not work.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;SPAN style=": ; font-size: 4;"&gt;After doing around 10-15 times of board reset or so, it boots the Linux&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style=": ; font-size: 4;"&gt;kernel. This repetition of resetting the board we have to do to make&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style=": ; font-size: 4;"&gt;this board warm-up.&amp;nbsp; Once it boots, it won't give any problem&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style=": ; font-size: 4;"&gt;afterwards. This means that we can reset the board at any number of&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style=": ; font-size: 4;"&gt;times during our working day once it starts working and it boots&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style=": ; font-size: 4;"&gt;properly. But in the morning it won't boot in a single reset.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;SPAN style=": ; font-size: 4;"&gt;Please help us to resolve this issue as soon as possible.&lt;/SPAN&gt;&lt;/P&gt;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 07 Jan 2009 21:22:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/Linux-Booting-Issue-in-M52277EVB-board/m-p/214117#M10701</guid>
      <dc:creator>vinaymindteck</dc:creator>
      <dc:date>2009-01-07T21:22:13Z</dc:date>
    </item>
    <item>
      <title>Re: Linux Booting Issue in M52277EVB board</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/Linux-Booting-Issue-in-M52277EVB-board/m-p/214118#M10702</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;If this truly a temperature problem, then there's something wrong with the board. I'd suggest you get it exchanged.&lt;BR /&gt;&lt;BR /&gt;---Tom&lt;BR /&gt;&lt;BR /&gt;&lt;DIV&gt;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 07 Jan 2009 23:55:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/Linux-Booting-Issue-in-M52277EVB-board/m-p/214118#M10702</guid>
      <dc:creator>J2MEJediMaster</dc:creator>
      <dc:date>2009-01-07T23:55:36Z</dc:date>
    </item>
  </channel>
</rss>