<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Eliminate Heap in ColdFire/68K Microcontrollers and Processors</title>
    <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/Eliminate-Heap/m-p/211377#M10296</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Yes this is possible defining a heap_size of 0 bytes should be supported.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;CrasyCat&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 01 Mar 2012 16:07:42 GMT</pubDate>
    <dc:creator>CrasyCat</dc:creator>
    <dc:date>2012-03-01T16:07:42Z</dc:date>
    <item>
      <title>Eliminate Heap</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/Eliminate-Heap/m-p/211376#M10295</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I'm working with MCF51QE128 and CW6.3&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;If I'm not using any dynamic memory allocation, &amp;nbsp;could I eliminate heap? I mean define heap size as 0x0000 so I can gain more RAM&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks in advance!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 29 Feb 2012 19:27:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/Eliminate-Heap/m-p/211376#M10295</guid>
      <dc:creator>sebasira</dc:creator>
      <dc:date>2012-02-29T19:27:14Z</dc:date>
    </item>
    <item>
      <title>Re: Eliminate Heap</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/Eliminate-Heap/m-p/211377#M10296</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Yes this is possible defining a heap_size of 0 bytes should be supported.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;CrasyCat&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 01 Mar 2012 16:07:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/Eliminate-Heap/m-p/211377#M10296</guid>
      <dc:creator>CrasyCat</dc:creator>
      <dc:date>2012-03-01T16:07:42Z</dc:date>
    </item>
    <item>
      <title>Re: Eliminate Heap</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/Eliminate-Heap/m-p/211378#M10297</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks!&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I was near my RAM limit, now I've got 1K more!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 01 Mar 2012 22:02:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/Eliminate-Heap/m-p/211378#M10297</guid>
      <dc:creator>sebasira</dc:creator>
      <dc:date>2012-03-01T22:02:25Z</dc:date>
    </item>
    <item>
      <title>Re: Eliminate Heap</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/Eliminate-Heap/m-p/211379#M10298</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I have a similar question, I don't use malloc() but my heap is defined differently, can I just remove all references to __HEAP* from the .LCF?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;PRE&gt;   ___FLASH        = ADDR(.bootcode);    ___FLASH_SIZE    = 0x00080000;    ___SRAM            = 0x20000400;    ___SRAM_SIZE    = 0x0000FC00;    ___VECTOR_RAM    = 0x20000000;    ___IPSBAR        = ADDR(.ipsbar);    ___SP_SIZE      = 0x2000; # 8k    ___HEAP_START    = .; # Store after sections above (.bss)    ___HEAP_END        = ___SRAM + ___SRAM_SIZE - ___SP_SIZE;    ___SP_END        = ___HEAP_END;    ___SP_INIT        = ___SP_END + ___SP_SIZE;          ___heap_addr     = ___HEAP_START;    ___heap_size     = ___HEAP_END - ___HEAP_START ;    __SP_INIT         = ___SP_INIT;        # &lt;A href="http://forums.freescale.com/freescale/attachments/freescale/CWCFCOMM/3435/1/TN268.pdf" rel="nofollow noopener noreferrer" target="_blank"&gt;http://forums.freescale.com/freescale/attachments/freescale/CWCFCOMM/3435/1/TN268.pdf&lt;/A&gt;    ___mem_limit = ___HEAP_END;    ___stack_safety = 16;&lt;/PRE&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 02 Mar 2012 20:49:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/Eliminate-Heap/m-p/211379#M10298</guid>
      <dc:creator>FridgeFreezer</dc:creator>
      <dc:date>2012-03-02T20:49:28Z</dc:date>
    </item>
  </channel>
</rss>