<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: M5329EVB - framebuffer not working in ColdFire/68K Microcontrollers and Processors</title>
    <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/M5329EVB-framebuffer-not-working/m-p/209947#M10192</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;I have changed my kernel configuration according to above post from mwaddel - the only differences were in the items CONFIG_DISPLAY_SUPPORT and CONFIG_FIRMWARE_EDID. Unfortunately no success yet, instead of the penguin the irregular vertical lines appear when the system is booting, and they stay here - see the attached photo. (The horizontal grey lines are not actually on the display, it is moire from photo processing).&lt;BR /&gt;&lt;BR /&gt;Jan&lt;BR /&gt;&lt;DIV&gt;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 16 Dec 2008 17:38:18 GMT</pubDate>
    <dc:creator>jare</dc:creator>
    <dc:date>2008-12-16T17:38:18Z</dc:date>
    <item>
      <title>M5329EVB - framebuffer not working</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/M5329EVB-framebuffer-not-working/m-p/209943#M10188</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt; &lt;/DIV&gt;&lt;SPAN&gt;Hi all,&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;I have problem getting the framebuffer working in linux (m532xevb-20071102-ltib.iso, updated with m5329-20071102-update-ltib.tar.gz). I have selected microwindows in package selector and enabled framebuffer in the kernel configuration.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Linux is normally running, framebuffer is initialized (see the corresponding part of /var/log/messages in attachment), but the nanox examples don't show anything on the screen. Nevertheless the examples seem to be running: after launching the demo2.sh ps shows running bin/nano-X, bin/nanowm, bin/nxeyes, bin/tux. The /usr/nanox/bib/nxcal also seems to be working (it waits for 4 touches on the display and prints diagnostic messages on the console).&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;The "video-open 6 16" and "draw-test" commands from the LogicLoader show the correct test pattern, so the hardware is probably good. The LCD display is the Logic's LCD-3.5-QVGA-10.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;What am I doing wrong? Can anybody send me his /var/log/messages from functioning system?&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Many thanks&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Jan Rejlek&lt;/SPAN&gt;&lt;DIV&gt; &lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 16 Dec 2008 00:05:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/M5329EVB-framebuffer-not-working/m-p/209943#M10188</guid>
      <dc:creator>jare</dc:creator>
      <dc:date>2008-12-16T00:05:47Z</dc:date>
    </item>
    <item>
      <title>Re: M5329EVB - framebuffer not working</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/M5329EVB-framebuffer-not-working/m-p/209944#M10189</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;Do you see the "tux" image on the screen as the kernel boots?&amp;nbsp; Can you tell&lt;BR /&gt;if the backlight is on?&lt;BR /&gt;&lt;BR /&gt;Best regards,&lt;BR /&gt;Matt&lt;BR /&gt;&lt;DIV&gt;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 16 Dec 2008 01:06:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/M5329EVB-framebuffer-not-working/m-p/209944#M10189</guid>
      <dc:creator>mwaddel</dc:creator>
      <dc:date>2008-12-16T01:06:02Z</dc:date>
    </item>
    <item>
      <title>Re: M5329EVB - framebuffer not working</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/M5329EVB-framebuffer-not-working/m-p/209945#M10190</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;No, there is nothing on the screen at boot time also. The backlight is on.&lt;BR /&gt;&lt;BR /&gt;Best regards,&lt;BR /&gt;&lt;BR /&gt;Jan&lt;BR /&gt;&lt;DIV&gt;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 16 Dec 2008 02:34:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/M5329EVB-framebuffer-not-working/m-p/209945#M10190</guid>
      <dc:creator>jare</dc:creator>
      <dc:date>2008-12-16T02:34:45Z</dc:date>
    </item>
    <item>
      <title>Re: M5329EVB - framebuffer not working</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/M5329EVB-framebuffer-not-working/m-p/209946#M10191</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;You should see the little penguin in the corner of the screen while&lt;BR /&gt;the system is booting.&amp;nbsp;&lt;BR /&gt;&lt;BR /&gt;Besides the frame buffer options you mentioned in your original&lt;BR /&gt;&amp;nbsp;message, what other frame buffer options are enabled in your&lt;BR /&gt;kernel?&amp;nbsp; I have the following enabled in the default configuration:&lt;BR /&gt;&lt;BR /&gt;# Display device support&lt;BR /&gt;#&lt;BR /&gt;# CONFIG_DISPLAY_SUPPORT is not set&lt;BR /&gt;# CONFIG_VGASTATE is not set&lt;BR /&gt;CONFIG_FB=y&lt;BR /&gt;CONFIG_FIRMWARE_EDID=y&lt;BR /&gt;# CONFIG_FB_DDC is not set&lt;BR /&gt;CONFIG_FB_CFB_FILLRECT=y&lt;BR /&gt;CONFIG_FB_CFB_COPYAREA=y&lt;BR /&gt;CONFIG_FB_CFB_IMAGEBLIT=y&lt;BR /&gt;# CONFIG_FB_SYS_FILLRECT is not set&lt;BR /&gt;# CONFIG_FB_SYS_COPYAREA is not set&lt;BR /&gt;# CONFIG_FB_SYS_IMAGEBLIT is not set&lt;BR /&gt;# CONFIG_FB_SYS_FOPS is not set&lt;BR /&gt;CONFIG_FB_DEFERRED_IO=y&lt;BR /&gt;# CONFIG_FB_SVGALIB is not set&lt;BR /&gt;# CONFIG_FB_MACMODES is not set&lt;BR /&gt;# CONFIG_FB_BACKLIGHT is not set&lt;BR /&gt;# CONFIG_FB_MODE_HELPERS is not set&lt;BR /&gt;# CONFIG_FB_TILEBLITTING is not set&lt;BR /&gt;&lt;BR /&gt;#&lt;BR /&gt;# Frame buffer hardware drivers&lt;BR /&gt;#&lt;BR /&gt;# CONFIG_FB_S1D13XXX is not set&lt;BR /&gt;CONFIG_FB_M532x=y&lt;BR /&gt;# CONFIG_LCD_640x480 is not set&lt;BR /&gt;# CONFIG_LCD_800x600 is not set&lt;BR /&gt;CONFIG_LCD_240x320=y&lt;BR /&gt;# CONFIG_FB_VIRTUAL is not set&lt;BR /&gt;&lt;BR /&gt;#&lt;BR /&gt;# Console display driver support&lt;BR /&gt;#&lt;BR /&gt;CONFIG_DUMMY_CONSOLE=y&lt;BR /&gt;CONFIG_FRAMEBUFFER_CONSOLE=y&lt;BR /&gt;# CONFIG_FRAMEBUFFER_CONSOLE_ROTATION is not set&lt;BR /&gt;CONFIG_FONTS=y&lt;BR /&gt;CONFIG_FONT_8x8=y&lt;BR /&gt;CONFIG_FONT_8x16=y&lt;BR /&gt;# CONFIG_FONT_6x11 is not set&lt;BR /&gt;# CONFIG_FONT_7x14 is not set&lt;BR /&gt;# CONFIG_FONT_PEARL_8x8 is not set&lt;BR /&gt;# CONFIG_FONT_ACORN_8x8 is not set&lt;BR /&gt;CONFIG_FONT_MINI_4x6=y&lt;BR /&gt;# CONFIG_FONT_SUN8x16 is not set&lt;BR /&gt;# CONFIG_FONT_SUN12x22 is not set&lt;BR /&gt;# CONFIG_FONT_10x18 is not set&lt;BR /&gt;CONFIG_LOGO=y&lt;BR /&gt;CONFIG_LOGO_LINUX_MONO=y&lt;BR /&gt;CONFIG_LOGO_LINUX_VGA16=y&lt;BR /&gt;CONFIG_LOGO_LINUX_CLUT224=y&lt;BR /&gt;&lt;BR /&gt;You probably don't need all these options, but once you get a&lt;BR /&gt;working frame buffer you can disabling options.&lt;BR /&gt;&lt;BR /&gt;&lt;DIV&gt;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 16 Dec 2008 07:28:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/M5329EVB-framebuffer-not-working/m-p/209946#M10191</guid>
      <dc:creator>mwaddel</dc:creator>
      <dc:date>2008-12-16T07:28:08Z</dc:date>
    </item>
    <item>
      <title>Re: M5329EVB - framebuffer not working</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/M5329EVB-framebuffer-not-working/m-p/209947#M10192</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;I have changed my kernel configuration according to above post from mwaddel - the only differences were in the items CONFIG_DISPLAY_SUPPORT and CONFIG_FIRMWARE_EDID. Unfortunately no success yet, instead of the penguin the irregular vertical lines appear when the system is booting, and they stay here - see the attached photo. (The horizontal grey lines are not actually on the display, it is moire from photo processing).&lt;BR /&gt;&lt;BR /&gt;Jan&lt;BR /&gt;&lt;DIV&gt;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 16 Dec 2008 17:38:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/M5329EVB-framebuffer-not-working/m-p/209947#M10192</guid>
      <dc:creator>jare</dc:creator>
      <dc:date>2008-12-16T17:38:18Z</dc:date>
    </item>
    <item>
      <title>Re: M5329EVB - framebuffer not working</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/M5329EVB-framebuffer-not-working/m-p/209948#M10193</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;Problem is solved!&lt;BR /&gt;The driver linux-2.6.22-uc1.20070808/drivers/video/m532xfb.c seems to not support my Sharp 240x320 TFT panel. I have modified it - the net result of my modifications is:&lt;BR /&gt;&lt;BR /&gt;MCF_LCDC_LPCR = 0xcc2480c9&lt;BR /&gt;and&lt;BR /&gt;MCF_LCDC_LPCCR = 0x00a00510&lt;BR /&gt;&lt;BR /&gt;Thanks to mwaddel - although his posts didn't lead directly to the solution, they helped me in better orientation in the problem.&lt;DIV&gt;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 18 Dec 2008 00:46:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/M5329EVB-framebuffer-not-working/m-p/209948#M10193</guid>
      <dc:creator>jare</dc:creator>
      <dc:date>2008-12-18T00:46:34Z</dc:date>
    </item>
  </channel>
</rss>