<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Flash read/write help with the MCF52233 board in ColdFire/68K Microcontrollers and Processors</title>
    <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/Flash-read-write-help-with-the-MCF52233-board/m-p/209146#M10100</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Motti&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;See: &lt;A href="http://www.utasker.com/docs/uTasker/uTaskerFileSystem_3.PDF" rel="nofollow" target="_self"&gt;http://www.utasker.com/docs/uTasker/uTaskerFileSystem_3.PDF&lt;/A&gt; (section about parameter system).&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Mark&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;A href="http://www.uTasker.com" rel="nofollow" target="_self"&gt;www.uTasker.com&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 25 Jun 2010 22:59:26 GMT</pubDate>
    <dc:creator>mjbcswitzerland</dc:creator>
    <dc:date>2010-06-25T22:59:26Z</dc:date>
    <item>
      <title>Flash read/write help with the MCF52233 board</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/Flash-read-write-help-with-the-MCF52233-board/m-p/209145#M10099</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I've developed a project based off the Coldfire_lite TCP project.&amp;nbsp; I'm using TCP on multiple boards to communicate with a server.&amp;nbsp; The TCP program works well as well as the other tasks I've created on the RTOS.&amp;nbsp; The only thing left is to create a menu option using the console that would allow a user to change the IP address and other network related info so that the boards don't create any conflicts on the LAN.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I am trying to create a function that would take in the new IP from the uart and flash it to a safe place in FLASH memory.&amp;nbsp; I don't fully understand the commands used to both read and write to flash from the embedded software and I don't want to store the address in RAM (I've done that already).&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;If anybody has any experience with this and could guide me where to look I would really appreciate the help.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Motti&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 25 Jun 2010 22:09:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/Flash-read-write-help-with-the-MCF52233-board/m-p/209145#M10099</guid>
      <dc:creator>Motti</dc:creator>
      <dc:date>2010-06-25T22:09:58Z</dc:date>
    </item>
    <item>
      <title>Re: Flash read/write help with the MCF52233 board</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/Flash-read-write-help-with-the-MCF52233-board/m-p/209146#M10100</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Motti&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;See: &lt;A href="http://www.utasker.com/docs/uTasker/uTaskerFileSystem_3.PDF" rel="nofollow" target="_self"&gt;http://www.utasker.com/docs/uTasker/uTaskerFileSystem_3.PDF&lt;/A&gt; (section about parameter system).&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Mark&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;A href="http://www.uTasker.com" rel="nofollow" target="_self"&gt;www.uTasker.com&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 25 Jun 2010 22:59:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/Flash-read-write-help-with-the-MCF52233-board/m-p/209146#M10100</guid>
      <dc:creator>mjbcswitzerland</dc:creator>
      <dc:date>2010-06-25T22:59:26Z</dc:date>
    </item>
    <item>
      <title>Re: Flash read/write help with the MCF52233 board</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/Flash-read-write-help-with-the-MCF52233-board/m-p/209147#M10101</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Mark,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks for the link.&amp;nbsp; It's just what i was looking for.&amp;nbsp; I'll check out the demo code in uTasker.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Motti&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 26 Jun 2010 00:09:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/Flash-read-write-help-with-the-MCF52233-board/m-p/209147#M10101</guid>
      <dc:creator>Motti</dc:creator>
      <dc:date>2010-06-26T00:09:39Z</dc:date>
    </item>
  </channel>
</rss>