<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>ColdFire/68K Microcontrollers and ProcessorsのトピックRe: Migration from Microtec C compiler to CodeWarrior 68k</title>
    <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/Migration-from-Microtec-C-compiler-to-CodeWarrior-68k/m-p/209083#M10098</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I have done this a few times for clients over years on these specific parts. I have moved them to the GNU compiler and it proved effective and cost efficent. I can only speak about GNU gcc because this is what I focus on so using Codewarrior maybe possible but a Codewarrior user would need to speak up.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;The GNU gcc is nice because it has moved over the years with host operating systems, be it Windows, Linux, or MacOS. Sure you may need a new build of GNU gcc for a new host but your appliction source code does not change greatly if at all.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 25 Jun 2010 08:48:55 GMT</pubDate>
    <dc:creator>ChrisJohns</dc:creator>
    <dc:date>2010-06-25T08:48:55Z</dc:date>
    <item>
      <title>Migration from Microtec C compiler to CodeWarrior 68k</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/Migration-from-Microtec-C-compiler-to-CodeWarrior-68k/m-p/209082#M10097</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I need to migrate C and Assembly code for a MC68332 based device to the CodeWarrior 68k system. It was originally compiled using the Microtec C compiler (either ver 1.0 or 2.0).&lt;BR /&gt;It is needed for an older model device that my company has. It is an older 68332 based product that we have the C source code for but no longer have the Microtec C compiler. It's part of a product line that we purchased but to this point never needed to make any modifications to. That has recently changed.&lt;BR /&gt;Unfortunately it was developed using the Microtec compiler according to documentation on the product. I need a compiler/ide to reproduce the 'bin' file output and then start to make changes that customers have been asking for, bug fixes, etc.&lt;/P&gt;&lt;P&gt;Has anyone ever done this migration before and if so can they provide any pointers on how to get started and advise on pitfalls to avoid?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks in advance&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 25 Jun 2010 04:58:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/Migration-from-Microtec-C-compiler-to-CodeWarrior-68k/m-p/209082#M10097</guid>
      <dc:creator>pflannery</dc:creator>
      <dc:date>2010-06-25T04:58:50Z</dc:date>
    </item>
    <item>
      <title>Re: Migration from Microtec C compiler to CodeWarrior 68k</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/Migration-from-Microtec-C-compiler-to-CodeWarrior-68k/m-p/209083#M10098</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I have done this a few times for clients over years on these specific parts. I have moved them to the GNU compiler and it proved effective and cost efficent. I can only speak about GNU gcc because this is what I focus on so using Codewarrior maybe possible but a Codewarrior user would need to speak up.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;The GNU gcc is nice because it has moved over the years with host operating systems, be it Windows, Linux, or MacOS. Sure you may need a new build of GNU gcc for a new host but your appliction source code does not change greatly if at all.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 25 Jun 2010 08:48:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/Migration-from-Microtec-C-compiler-to-CodeWarrior-68k/m-p/209083#M10098</guid>
      <dc:creator>ChrisJohns</dc:creator>
      <dc:date>2010-06-25T08:48:55Z</dc:date>
    </item>
  </channel>
</rss>