<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>OSBDM and TBDML中的主题 Re: CFV1 Flash Programmer Standalone ?</title>
    <link>https://community.nxp.com/t5/OSBDM-and-TBDML/CFV1-Flash-Programmer-Standalone/m-p/158137#M905</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear Joel,&lt;BR /&gt;&lt;BR /&gt;Sorry for the confusion.&lt;BR /&gt;&lt;BR /&gt;I keep a copy of the uploaded files but it seems that I've accidently updated it so it's inconsistent with the posted version (overwritten with V4.7 structure).&lt;BR /&gt;&lt;BR /&gt;For version 4.6a (as posted on sourceforge)&lt;BR /&gt;&lt;BR /&gt;The executable files in &lt;STRONG&gt;USBDM_Win32_4_6a\Win32\Utilities&lt;/STRONG&gt; should run without &lt;STRONG&gt;ANY&lt;/STRONG&gt; changes as all the device files and DLLs are present in that directory (or subdirectories).&lt;BR /&gt;&lt;BR /&gt;For the CFV1 programmer the required files are (from memory - not checked, see below):&lt;BR /&gt;&lt;BR /&gt;Device Files: &lt;STRONG&gt;cfv1_devices.xml, CFV1 (directory)&lt;/STRONG&gt;&lt;BR /&gt;&lt;BR /&gt;Executable: &lt;STRONG&gt;CFV1_FlashProgrammer.exe, libxerces-c-3-1.dll, usbdm.4.dll, usbdmTCL.4.dll, usbdm-arm.4.dll, libusb-1.0.dll, tcl85.dll&lt;/STRONG&gt;&lt;BR /&gt;&lt;BR /&gt;You would also need to install the device drivers.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Tested as follows:&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;Copied entire &lt;STRONG&gt;Utilities&lt;/STRONG&gt; directory &amp;amp; &lt;STRONG&gt;Drivers&lt;/STRONG&gt; directory to a USB Stick.&lt;/LI&gt;&lt;LI&gt;Moved to 'pristine' machine and plugged in USB Stick.&lt;/LI&gt;&lt;LI&gt;Plugged in USBDM &amp;amp; when prompted (WINXP-32),&amp;nbsp; installed the drivers from &lt;STRONG&gt;Drivers&lt;/STRONG&gt; directory (on stick).&lt;/LI&gt;&lt;LI&gt;Run CFV1_Programmer from Utilties directory (on stick) .&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;bye﻿&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 31 Aug 2011 14:00:56 GMT</pubDate>
    <dc:creator>pgo</dc:creator>
    <dc:date>2011-08-31T14:00:56Z</dc:date>
    <item>
      <title>CFV1 Flash Programmer Standalone ?</title>
      <link>https://community.nxp.com/t5/OSBDM-and-TBDML/CFV1-Flash-Programmer-Standalone/m-p/158128#M896</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi all, and particularly PGO if you see this message,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I'm working with CFV1 Flash Programmer on my computer to load program in Coldfire V1 devices (MCF51JM128). It works fine on my own computer, but I would like to install it on another one. I simply copied the "Utilities" directory provided by PGO on the second computer, but it doesn't work at all.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;CodeWarrior and CodeSourcery are installed on the first machine, but not on the other one. I conclude that some files in the CodeWarrior or CodeSourcery directories are required to get CFV1 Flash Programmer running, right ?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Is it possible to get a standalone CFV1 Flash Programmer ? Which files are required to do it ?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thank you very much for your help.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Joel&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 11 Aug 2011 22:16:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/OSBDM-and-TBDML/CFV1-Flash-Programmer-Standalone/m-p/158128#M896</guid>
      <dc:creator>Joel69003</dc:creator>
      <dc:date>2011-08-11T22:16:07Z</dc:date>
    </item>
    <item>
      <title>Re: CFV1 Flash Programmer Standalone ?</title>
      <link>https://community.nxp.com/t5/OSBDM-and-TBDML/CFV1-Flash-Programmer-Standalone/m-p/158129#M897</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear Joel,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;the programmers don't need anything from Codewarrior but they do need the device files to be installed to %APPDATA%/usbdm.&amp;nbsp; The installation batch file ﻿does this.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Unfortunately the installation batch file assumes codewarrior is installed and gives an error message if not.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Attached is an installation file that should install the required files (it still gives an error about not finding Codewarrior).&lt;/P&gt;&lt;P&gt;Replace the existing file in the installation directory.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;bye&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 13 Aug 2011 22:13:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/OSBDM-and-TBDML/CFV1-Flash-Programmer-Standalone/m-p/158129#M897</guid>
      <dc:creator>pgo</dc:creator>
      <dc:date>2011-08-13T22:13:50Z</dc:date>
    </item>
    <item>
      <title>Re: CFV1 Flash Programmer Standalone ?</title>
      <link>https://community.nxp.com/t5/OSBDM-and-TBDML/CFV1-Flash-Programmer-Standalone/m-p/158130#M898</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi PGO,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks for your reply. I noticed that there were files in the AppData directory, but maybe I miss something when I have tried to copy those files. I wil ltry again soon and tell you the result, but it should be OK !&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Just for my personnal information : why those files are in the AppData directory ? Why not with the CFV1 Flash Programmer application ? Is it to get the possibility to have different files for the different users (really useful ?) ?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Joel&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 14 Aug 2011 00:21:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/OSBDM-and-TBDML/CFV1-Flash-Programmer-Standalone/m-p/158130#M898</guid>
      <dc:creator>Joel69003</dc:creator>
      <dc:date>2011-08-14T00:21:12Z</dc:date>
    </item>
    <item>
      <title>Re: CFV1 Flash Programmer Standalone ?</title>
      <link>https://community.nxp.com/t5/OSBDM-and-TBDML/CFV1-Flash-Programmer-Standalone/m-p/158131#M899</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear Joel,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;The directory is used to store the per-user last used settings for the programmers etc.&lt;/P&gt;&lt;P&gt;It also is a central location to keep the device files which are used by various programs and DLLs.&amp;nbsp; It would be undesirable to have a copy in each location.&amp;nbsp; The later could be system wide but it would not be a big advantage unless there are multiple users.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;The utilities used to operate stand-alone (they look for the device files in the executable directory as well)&amp;nbsp; but this was broken with the re-arranged installation folder.&amp;nbsp; You can try copying the &lt;STRONG&gt;device_data&lt;/STRONG&gt; folder contents (including sub-directories) into the utilties folder and the device files should be found without the need to install.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;bye&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 15 Aug 2011 07:08:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/OSBDM-and-TBDML/CFV1-Flash-Programmer-Standalone/m-p/158131#M899</guid>
      <dc:creator>pgo</dc:creator>
      <dc:date>2011-08-15T07:08:24Z</dc:date>
    </item>
    <item>
      <title>Re: CFV1 Flash Programmer Standalone ?</title>
      <link>https://community.nxp.com/t5/OSBDM-and-TBDML/CFV1-Flash-Programmer-Standalone/m-p/158132#M900</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi PGO,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I tried to run CFV1 Flash Programmer copying the files in the AppData directory, but it doesn't work...&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Here is the situation :&lt;/P&gt;&lt;P&gt;- In "C:\Documents and Settings\Joël\Application Data﻿\usbdm", I have files : "cfv1_devices﻿.xml", "hcs08_devices.xml﻿", "hcs12_devices﻿.xml", "JTAG_Devices.cfg﻿", "rs08_devices﻿.xml" and "usbdmDeviceSchema﻿.dtd".&lt;/P&gt;&lt;P&gt;- In a folder in Program Files directory (or any other place in fact), I copied files "CFV1_FlashProgrammer﻿.exe", "libusb-1.0.dll﻿", "libxerces-c-3-1.dll﻿" and "usbdm.4.dll﻿".&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;When I run CFV1 Flash Programmer application, it is launched (I can see it in the Task Manager), but with no window, and after some few seconds, the application ends. I sometimes have an error message saying that the application crashed.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I forget to give my configuration : Windows XP SP2.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Any ideas ? Is there special requirements to run the flasher ? .NET Framework ?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thank a lot for your help and for the job you have done on the USBDM !&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Joel&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 17 Aug 2011 22:58:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/OSBDM-and-TBDML/CFV1-Flash-Programmer-Standalone/m-p/158132#M900</guid>
      <dc:creator>Joel69003</dc:creator>
      <dc:date>2011-08-17T22:58:13Z</dc:date>
    </item>
    <item>
      <title>Re: CFV1 Flash Programmer Standalone ?</title>
      <link>https://community.nxp.com/t5/OSBDM-and-TBDML/CFV1-Flash-Programmer-Standalone/m-p/158133#M901</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;EDIT:&lt;BR /&gt;&lt;BR /&gt;In "C:\Documents and Settings\Joël\Application Data﻿\usbdm", I have files : "arm_devices.xml", "cfv1_devices﻿.xml", "cfvx_devices﻿.xml", "hcs08_devices.xml﻿", "hcs12_devices﻿.xml", "JTAG_Devices.cfg﻿", "rs08_devices﻿.xml" and "usbdmDeviceSchema﻿.dtd". I have also directories: "Arm", "CFV1", "CFVx".&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;I copied those files by hand because your batch file to not work ("device_data" is not known...).&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I wondered if it was not because of special characters in the path (for example "ë"), So I copied all those files on another computer (Windows 2003 Server) in "C:\Documents and Settings\Administrateur\Application Data﻿\usbdm", but I get the same result: the flasher is launched in the task manager but with no window, and it ends after some few seconds.﻿&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks for your help.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Joel&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 25 Aug 2011 19:51:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/OSBDM-and-TBDML/CFV1-Flash-Programmer-Standalone/m-p/158133#M901</guid>
      <dc:creator>Joel69003</dc:creator>
      <dc:date>2011-08-25T19:51:27Z</dc:date>
    </item>
    <item>
      <title>Re: CFV1 Flash Programmer Standalone ?</title>
      <link>https://community.nxp.com/t5/OSBDM-and-TBDML/CFV1-Flash-Programmer-Standalone/m-p/158134#M902</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Edit again:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I tried on other computers, and I can see exactly the same : CFV1 Flash Programmer is launched and closed after some few seconds in the task manager, but no window displayed.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I had a look to the events recorded by Windows, and I get two errors about the CFV1 Flash Programmer application :&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;- Error 1000 (application error) : an error occured in the DLL "C:\Win32\Utilities\libxerces-c-3-1.dll﻿﻿". The error code is 1D.&lt;/P&gt;&lt;P&gt;- Error 1005 (application error), immediatly after the first one, indicating that an error occured with the application CFV1 Flash Programmer. I suppose it is due to the first error.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Does somebody allready get something like that ? PGO, what do you think about this error ? Is is possible to debug something ?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thank you very much for any information and help.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Joel&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 28 Aug 2011 19:33:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/OSBDM-and-TBDML/CFV1-Flash-Programmer-Standalone/m-p/158134#M902</guid>
      <dc:creator>Joel69003</dc:creator>
      <dc:date>2011-08-28T19:33:04Z</dc:date>
    </item>
    <item>
      <title>Re: CFV1 Flash Programmer Standalone ?</title>
      <link>https://community.nxp.com/t5/OSBDM-and-TBDML/CFV1-Flash-Programmer-Standalone/m-p/158135#M903</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear Joel,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;The XML parser DLL (xerces) throws exceptions on ANY XML parsing error.&amp;nbsp; Unfortunately MinGW-GCC doesn't handle catching C++ exceptions across DLL (or at least I can't make it do so).&amp;nbsp; This means that if the XML parsing fails for any reason you get a silent crash as you have seen.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;The cause of the above is that the XML files are not found.&amp;nbsp; In particular the files referenced from the XML are not found since missing top-level files are checked for by the programmer before parsing.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;You should be able to use the programmer stand-alone by following the directions outlined earlier:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;You can try copying the &lt;STRONG&gt;device_data&lt;/STRONG&gt; folder contents (including sub-directories) into the &lt;STRONG&gt;Utilties&lt;/STRONG&gt; folder and the device files should be found without the need to install.﻿&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I tried this on a couple of machines at it seemed to work OK.&amp;nbsp; I'm unsure why this isn't working for you. Could you check that you have the subdirectories &lt;STRONG&gt;ARM, CFV1, CFVx&lt;/STRONG&gt; and the &lt;STRONG&gt;xxxx_devices.xml&lt;/STRONG&gt; files in the same directory as the executables?&amp;nbsp; Note the folders NOT the folder contents as the structure is important.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;In any case, I'll modify the next release so that they execute from the Utility directory without any changes but this won't be released for a while.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;bye&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 29 Aug 2011 08:49:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/OSBDM-and-TBDML/CFV1-Flash-Programmer-Standalone/m-p/158135#M903</guid>
      <dc:creator>pgo</dc:creator>
      <dc:date>2011-08-29T08:49:10Z</dc:date>
    </item>
    <item>
      <title>Re: CFV1 Flash Programmer Standalone ?</title>
      <link>https://community.nxp.com/t5/OSBDM-and-TBDML/CFV1-Flash-Programmer-Standalone/m-p/158136#M904</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi PGO,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks for your reply. I understand now why it is crashing like that.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;In order to not introduce some other problems, ﻿I kept the folder structure you give on SourceForge. The CFV1 Flash Programmer application is in the Utilities folder, and there are the XML files in the same directory. I haven't modify anything in the files.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I understand that I can copy the folder "device_data" and its content in the utility folder, but where is the "device_data" folder ? I haven't found it .... is it on SourceForge in one of the available archive ? Which files I should found in this folder ?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Again, thank you very much for your help.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Joel&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 30 Aug 2011 01:43:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/OSBDM-and-TBDML/CFV1-Flash-Programmer-Standalone/m-p/158136#M904</guid>
      <dc:creator>Joel69003</dc:creator>
      <dc:date>2011-08-30T01:43:44Z</dc:date>
    </item>
    <item>
      <title>Re: CFV1 Flash Programmer Standalone ?</title>
      <link>https://community.nxp.com/t5/OSBDM-and-TBDML/CFV1-Flash-Programmer-Standalone/m-p/158137#M905</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear Joel,&lt;BR /&gt;&lt;BR /&gt;Sorry for the confusion.&lt;BR /&gt;&lt;BR /&gt;I keep a copy of the uploaded files but it seems that I've accidently updated it so it's inconsistent with the posted version (overwritten with V4.7 structure).&lt;BR /&gt;&lt;BR /&gt;For version 4.6a (as posted on sourceforge)&lt;BR /&gt;&lt;BR /&gt;The executable files in &lt;STRONG&gt;USBDM_Win32_4_6a\Win32\Utilities&lt;/STRONG&gt; should run without &lt;STRONG&gt;ANY&lt;/STRONG&gt; changes as all the device files and DLLs are present in that directory (or subdirectories).&lt;BR /&gt;&lt;BR /&gt;For the CFV1 programmer the required files are (from memory - not checked, see below):&lt;BR /&gt;&lt;BR /&gt;Device Files: &lt;STRONG&gt;cfv1_devices.xml, CFV1 (directory)&lt;/STRONG&gt;&lt;BR /&gt;&lt;BR /&gt;Executable: &lt;STRONG&gt;CFV1_FlashProgrammer.exe, libxerces-c-3-1.dll, usbdm.4.dll, usbdmTCL.4.dll, usbdm-arm.4.dll, libusb-1.0.dll, tcl85.dll&lt;/STRONG&gt;&lt;BR /&gt;&lt;BR /&gt;You would also need to install the device drivers.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Tested as follows:&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;Copied entire &lt;STRONG&gt;Utilities&lt;/STRONG&gt; directory &amp;amp; &lt;STRONG&gt;Drivers&lt;/STRONG&gt; directory to a USB Stick.&lt;/LI&gt;&lt;LI&gt;Moved to 'pristine' machine and plugged in USB Stick.&lt;/LI&gt;&lt;LI&gt;Plugged in USBDM &amp;amp; when prompted (WINXP-32),&amp;nbsp; installed the drivers from &lt;STRONG&gt;Drivers&lt;/STRONG&gt; directory (on stick).&lt;/LI&gt;&lt;LI&gt;Run CFV1_Programmer from Utilties directory (on stick) .&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;bye﻿&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 31 Aug 2011 14:00:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/OSBDM-and-TBDML/CFV1-Flash-Programmer-Standalone/m-p/158137#M905</guid>
      <dc:creator>pgo</dc:creator>
      <dc:date>2011-08-31T14:00:56Z</dc:date>
    </item>
    <item>
      <title>Re: CFV1 Flash Programmer Standalone ?</title>
      <link>https://community.nxp.com/t5/OSBDM-and-TBDML/CFV1-Flash-Programmer-Standalone/m-p/158138#M906</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi PGO,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks for your reply. I tried again, I have run CFV1 Flash Programmer from the Utilities directory without any modification (I downloaded again the archive file from Sourceforge to be sure), but it still fails. I get the same error.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I tried on several computers, and the only one on which CFV1 Flash Programmer is running is the one on which I have CodeSourcery and CodeWarrior installed.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Compatiblity issue ?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I can wait for version 4.7, maybe its better.....&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Joel&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 04 Sep 2011 05:00:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/OSBDM-and-TBDML/CFV1-Flash-Programmer-Standalone/m-p/158138#M906</guid>
      <dc:creator>Joel69003</dc:creator>
      <dc:date>2011-09-04T05:00:55Z</dc:date>
    </item>
  </channel>
</rss>