<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic It's a bit of a struggle to make sure USBDM works correctly when programming the MC9S08AC128 in OSBDM and TBDML</title>
    <link>https://community.nxp.com/t5/OSBDM-and-TBDML/It-s-a-bit-of-a-struggle-to-make-sure-USBDM-works-correctly-when/m-p/1868379#M3885</link>
    <description>&lt;P&gt;I'm trying to program MC9S08AC128, but it keeps giving me an error, I'm trying to use another MC9S08AW60, now everything is ok, problem. If MC9S08AC128, you are reading flash, now there is a problem and recording the reading, everything will be fine, but when you write a new file is shown, then what is needed, recording in s19 format continues until then, the camera does not respond to the test&lt;/P&gt;</description>
    <pubDate>Sat, 18 May 2024 08:51:38 GMT</pubDate>
    <dc:creator>janis_senc</dc:creator>
    <dc:date>2024-05-18T08:51:38Z</dc:date>
    <item>
      <title>It's a bit of a struggle to make sure USBDM works correctly when programming the MC9S08AC128</title>
      <link>https://community.nxp.com/t5/OSBDM-and-TBDML/It-s-a-bit-of-a-struggle-to-make-sure-USBDM-works-correctly-when/m-p/1868379#M3885</link>
      <description>&lt;P&gt;I'm trying to program MC9S08AC128, but it keeps giving me an error, I'm trying to use another MC9S08AW60, now everything is ok, problem. If MC9S08AC128, you are reading flash, now there is a problem and recording the reading, everything will be fine, but when you write a new file is shown, then what is needed, recording in s19 format continues until then, the camera does not respond to the test&lt;/P&gt;</description>
      <pubDate>Sat, 18 May 2024 08:51:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/OSBDM-and-TBDML/It-s-a-bit-of-a-struggle-to-make-sure-USBDM-works-correctly-when/m-p/1868379#M3885</guid>
      <dc:creator>janis_senc</dc:creator>
      <dc:date>2024-05-18T08:51:38Z</dc:date>
    </item>
  </channel>
</rss>