<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>OSBDM and TBDMLのトピックUSBDM identification</title>
    <link>https://community.nxp.com/t5/OSBDM-and-TBDML/USBDM-identification/m-p/1197414#M3633</link>
    <description>&lt;P&gt;In 2017 I asked for help in identifying my USBDM, but got no replies so I am trying again before I throw them in the bin.&lt;/P&gt;&lt;P&gt;Both items are labelled "freescale".&lt;/P&gt;&lt;P&gt;One PC board is labelled USBDM_CF.PCB V3.1. It has a Coldfire connector, an ARM JTAG connector, a HC8x CF V1 connector and a DSC/ONCE connector. it also has a 4-pin SIL header that may be a serial interface.&lt;/P&gt;&lt;P&gt;The other PC boards labelled USBDM_JS V1.0. It has a 6-pin DIL header for HF8x, a 10-pin DIL header and a 4-pin SIL header, none of which is labelled.&lt;/P&gt;&lt;P&gt;Unless I can identify them I don't know what software and drivers to use.&lt;/P&gt;&lt;P&gt;I would like to be able to use them, otherwise they are just taking up space in the cupboard.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Thu, 10 Dec 2020 12:57:19 GMT</pubDate>
    <dc:creator>juliancox</dc:creator>
    <dc:date>2020-12-10T12:57:19Z</dc:date>
    <item>
      <title>USBDM identification</title>
      <link>https://community.nxp.com/t5/OSBDM-and-TBDML/USBDM-identification/m-p/1197414#M3633</link>
      <description>&lt;P&gt;In 2017 I asked for help in identifying my USBDM, but got no replies so I am trying again before I throw them in the bin.&lt;/P&gt;&lt;P&gt;Both items are labelled "freescale".&lt;/P&gt;&lt;P&gt;One PC board is labelled USBDM_CF.PCB V3.1. It has a Coldfire connector, an ARM JTAG connector, a HC8x CF V1 connector and a DSC/ONCE connector. it also has a 4-pin SIL header that may be a serial interface.&lt;/P&gt;&lt;P&gt;The other PC boards labelled USBDM_JS V1.0. It has a 6-pin DIL header for HF8x, a 10-pin DIL header and a 4-pin SIL header, none of which is labelled.&lt;/P&gt;&lt;P&gt;Unless I can identify them I don't know what software and drivers to use.&lt;/P&gt;&lt;P&gt;I would like to be able to use them, otherwise they are just taking up space in the cupboard.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 10 Dec 2020 12:57:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/OSBDM-and-TBDML/USBDM-identification/m-p/1197414#M3633</guid>
      <dc:creator>juliancox</dc:creator>
      <dc:date>2020-12-10T12:57:19Z</dc:date>
    </item>
    <item>
      <title>Re: USBDM identification</title>
      <link>https://community.nxp.com/t5/OSBDM-and-TBDML/USBDM-identification/m-p/1335054#M3656</link>
      <description>&lt;P&gt;Maybe you should post some picts?&lt;/P&gt;</description>
      <pubDate>Sun, 05 Sep 2021 13:09:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/OSBDM-and-TBDML/USBDM-identification/m-p/1335054#M3656</guid>
      <dc:creator>Mindblaster</dc:creator>
      <dc:date>2021-09-05T13:09:15Z</dc:date>
    </item>
  </channel>
</rss>